Power & Energy
  • Technologies
  • More
Power & Energy
Forum 120v led lamp
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 19 replies
  • Answers 2 answers
  • Subscribers 284 subscribers
  • Views 3311 views
  • Users 0 members are here
Related

120v led lamp

moelleux
moelleux over 11 years ago

Hi,

Ive just started hacking electronics lately, thanks to Jeremy Blum book and tutorials!

 

My desk lamp fluorescent bulb gave up on me and i wanted to replace the bulb with some white LEDs.  So i took appart the lamp and found a circuit board and im not sure what it is for. The fluorescent bulb is rated 120V and i tought it was directly hooked to AC? is this board an AC to DC converter?

Heres some pictures (The side with the fuse is the 120v AC in) :

20141030083725 - HostingPics.net - Hébergement d'images gratuit

20141030083741 - HostingPics.net - Hébergement d'images gratuit

20141030083754 - HostingPics.net - Hébergement d'images gratuit

20141030083813 - HostingPics.net - Hébergement d'images gratuit

 

So my plan is to enclose a AC to DC converter to a potentiometer that would feed current to around 20 white LEDs(maybe those MCL034SWC-YH1MCL034SWC-YH1. This is my main light source in that room so i would like it to be very bright, but dimmable.
Thanks!

Feel free to recommend me stuff!

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago in reply to supper_slash +2
    Hi Lupe, Not sure that circuit will work, unless there is something I don't understand about the 555 (quite likely). Anyway, there is a great resource here, with plenty of 555 circuits - including PWM…
  • jw0752
    jw0752 over 11 years ago in reply to moelleux +1
    Hi William, I also wanted to make sure you used 100 nF caps where indicated. These are also labeled 0.1 uF. If we get the capacitance too high we lower the frequency of the 555 which would allow you to…
  • moelleux
    moelleux over 10 years ago +1
    It's been a while, but i thought i would share it anyway. I've been using it for almost a year now and it's great lighting. Especially for phone repair and precision stuff. I made 2 versions of the board…
  • supper_slash
    0 supper_slash over 11 years ago

    Electronic Ballasts: The electronic ballasts use semiconductors to limit power to a fluorescent lamp. First the ballast rectifies the AC power, then it chops it to make a high frequency for improved efficiency. The ballast can more precisely control power than a magnetic ballast but does have a number of problems.

    That is the circuit you have there.

     

    You can use a simpler diode- resistor combo to cut the voltage down for the led's, but its not efficient, and in my opinion dangerous, Because of the fact that it would be direct mains connection. I don't like this type of setup, i like isolation between any of my circuitry, and the mains, but that's just me.

     

    I would look to PMW to drive the led's, but that may be too much for your project.

    If you want a simple diagram, here is one using a Transformer, it may need some customizing for your led's, but it should be a starter.

    The transformer in the diagram isolates the mains for me in this circuit.

     

    Let me know exactly what your looking for.

    Someone else may be able to chime in if your looking for a switching power supply.As I am not too familiar with them.

    If you can maybe calculate the led stats, so we could know the Amperes, and voltage limitations for your circuit.

    That would be helpful.

    image







    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • moelleux
    0 moelleux over 11 years ago in reply to supper_slash

    Ok thanks, that helps a lot. in that case i wont be using the ballast!

     

     

    for the leds, the forward voltage is  3.4v and they use 20mA. I think i could have 10 rows of 3 in parallel at 12v with 90ohm resistance. so around 200mA Total. Maybe ill throw more led in, they are rated a 3.7cd each.

     

    For the power supply, is it cheaper to build on like you showed there? Would a transformer like that would do?

    http://canada.newark.com/myrra/44087/transformer-12v-1-5va/dp/50P9099


    btw i might use PWM for this project, but is there any other advantage other than setting better range on the potentiometer?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • supper_slash
    0 supper_slash over 11 years ago in reply to moelleux

    Looks OK, but, in my circuit, the transformer wont work for 12v.

    You see you will loose some in the rectifier bridge, and the 7812 will not be able to hold the 12v output.

    1. You can drop the 7812 down to 9v version, supplying 9v to the led's.
    2. Or find a transformer around 14+ volts.

    As for the PWM, I think it is more efficient. Less loss on the supply

    Everything else looks good.

    NOTE: you can buy a "wall wart" type power supply ready made, that should work, than u just need to do the PWM. But there would be no fun in that.

    I like building stuff myself, but it is an option.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • moelleux
    0 moelleux over 11 years ago in reply to supper_slash

    Ok cool, I really like the idea of building my own circuit for this project and im catching up on the knowledge as we speak, but for PWM, i know how it work on a microcontroller, but what you're talking about is a chip like this ?
    UC3845BNG ON SEMICONDUCTOR PWM Controllers | 88H5157 | Newark element14 Canada

    This particular one seem to have a well written datasheet that ill read during the weekend, but the example don't seem to apply to what im doing. Would you have an idea or a little example? Thanks!

     

    Here's the pins

    1 Compensation

    2 Voltage Feedback

    3 Current Sense

    4 RT/CT

    5 Vref

    6 VCC

    7 Output

    8 GND

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • supper_slash
    0 supper_slash over 11 years ago in reply to moelleux

    You can use that chip, i have used a "mic502yn" before.

    There is the 555 timer, you can use, or i prefer going old school, and using an op amp.

    Or, rather four.

    But your space is limited so mabe a mic502ym with a transistor or fet would be fine

    I have a schematic of the op-amp PWM circuit if you would like.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • moelleux
    0 moelleux over 11 years ago in reply to supper_slash

    Thanks but opAmps seem pretty advanced for me for that project.  Seem like the 555 timer could be a simple/cheap solution. With that a i should be able to make the final design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • supper_slash
    0 supper_slash over 11 years ago in reply to moelleux

    Ok, well, breadboard this, and see what you think.

    it should get you on track.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to supper_slash

    Hi Lupe,

     

    Not sure that circuit will work, unless there is something I don't understand about the 555 (quite likely).

    Anyway, there is a great resource here, with plenty of 555 circuits - including PWM ones. Just hit Ctrl-F

    and type PWM to find them there.

    That particular website has good circuits in general - some websites have poor or faulty circuits.

     

    For known working 555 circuits, I would consult that website first.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to shabaz

    Hi Shabaz, What a great site and recommendation. I always find some good sound ideas and advice in your posts.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to jw0752

    Hi John,

     

    Thanks! That site also has links off to 100 transistor circuits, and another 100 more. They seem to be pretty good!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>