Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 286 subscribers
  • Views 14535 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • mpulliam
    0 mpulliam over 5 years ago

    7812 voltage regulator test results:

    w/ Power off and writing facing me

    Black lead on the center pin, read lead on the left pin = 1.2mV and it trickled down to 0

    Black lead on the center pin, read lead on the right pin = .5mV and it trickled down to a negative number

     

    w/ Power On and writing facing me

    Black lead on the center pin, read lead on the left pin = 30V

    Black lead on the center pin, read lead on the right pin = 12.04v

     

    I re-tested the D313 for continuity (after the unit has been turned on and off)

    There is NO continuity between the base and the emitter or collector

    There IS continuity between the emitter and the collector

     

    I retested the corroded diode and it is ok.  The corrosion was giving me a bad reading previously but I scraped it off and the diode shows a voltage reading of .519v in one direction and nothing in the other.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    All sounds good and normal except the D313. We need to test that one out of circuit and verify if it is good or bad.

     

    At some point I mistyped Read when I meant to type Red. I mention it so that we don't start a new convention for what is the correct nomenclature.  Sorry about that. I always try to proofread but at 1:30 AM I may miss things.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

     

    Good job on replacing the D313. Even though that wasn't the problem you at least have one more thing checked off the list. When you test the output transistors I believe they will be 2N3055. An NTE equivalent is an NTE130NTE130.

    Here is a picture of the pin out and the voltage I would expect from a diode check. On these it might also be good to check continuity especially between the Emitter and Collector. The resistance should be high in both polarities. Notice that the Emitter and Base is off center. With the Emitter and Base closer to the bottom of the picture the leads are identified as in the picture.

     

    image

     

    Based on how the unit is acting I am doubtful that these are going to be the problem but we must be sure. I am also a little at loss as to what to focus on next. Without a schematic I am not sure how the circuit is designed and my usual procedure for testing beyond the basics that we have done usually relies on tracing circuits and reverse engineering. These will be next to impossible to do remotely using only pictures. I will be thinking and you can let me know when you have tested the 2N3055s.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    Yep, correct on the Power Transistor. Hopefully I won't have to disconnect the blue and yellow wires.  If so, I'm not sure how to reconnect without disassembling the entire back end of the unit.

    imageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to mpulliam

    there is no continuity between the base, collector, or emitter.

     

    Diode check

    It is showing .015 Volts between the collector and the yellow wire (which I believe is the base in your picture, although I'm not sure if I'm looking at the front or back side)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to mpulliam

    The data sheet for the 2N3055 NPN power transistors specifies

     

    2N3055 Equivalents

    2N6673, 2N6675, complementary pair- MJ2955

     

    Is there something special about complementary pairs vs two NTE130s?

     

    Thanks,

    Matt

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to mpulliam

    Discovery, by following the wires I figured out there are actually a total of (4) 2N3055 power transistors (not 2) hidden in all the heat sinks.... the blue and yellow wires are soldered to the transistor leads so removing them completely will be a chore. 

     

    Here a pic of the transistor tucked away behind a set of heat sinks...  the picture is actually upside down so I could read the description.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    I believe that the transistors are not soldered in but rather plugged into sockets. Once you have taken the screws out I believe that the transistors will unplug. At least I hope this is the case. If the wires are indeed soldered to the pins then you will have no choice except to unsolder them. The reason that they use matched pairs is so the transistors, which all vary slightly from one another, work together and share the load equally. If the transistors are badly mismatched the burden of the work will fall on the weaker of the two devices and it will fail more quickly. Keep in mind that unless there is a short between the Emitter and the Collector these transistors are not likely to be the cause of the problem with the power supply.  I am still trying to figure out what the next step is.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt;

    I think your best bet for continuing will be to see if you can find, locally, an old retired radio TV service technician to look over your shoulder and help trouble shoot the unit. I really can't think of any way to direct you to the next steps remotely. When you finally crack this puzzle please come back and post about it as my curiosity is killing me.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    The are definitely soldered and it would be a major pain to take it all apart to completely isolate the transistors from the unit in order to test them.

     

    There are also the rectifier diodes, which I didn't know what they were at first because they tested like capacitors while on the board.

     

    I can desolder one end of each diode and test them before I completely remove the transistors

     

    image

    Solder joints on one of the transistors.  Hardly any wiggle room to work with and the back end of the unit would have to be dissembled in order to reconnect everything.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

     

    As long as there isn't continuity between the yellow and the metal case of the transistor they are probably good and I would not unsolder them. The diodes that you show should be able to be tested in the circuit using your diode test. I would expect about 0.5 Volts on each of them in one polarity only.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    The rectifier diodes test at .403 V with the black lead on anode side. When I reverse the leads, I get a reading of about .5V and it starts going up to 1V where I'll get a .0L reading (overload)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    The rectifier diodes test at .403 V with the black lead on anode side. When I reverse the leads, I get a reading of about .5V and it starts going up to 1V where I'll get a .0L reading (overload)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    The 0.403 Volts would be normal for a Schottky Diode. Can you read the numbers on the diode? We can look it up to verify this. The voltage you are seeing on the reverse polarity is likely just seeing the capacitors charging and sounds normal for in circuit measuring.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    I can make out N5402 with an NB below it. Maybe there's a 1 before the N, but I'm not certain.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Yes that would be a 1N5402 which has a 3 Amp current capacity and can tolerate 200 Volts. The some of the ones in your power supply are probably being used in parallel to accommodate the higher current of the power supply. If you were to take them out of the circuit I would expect the diode test to be closer to 0.55 Volts as these are not Schottky diodes. Your test however has convinced me that they are not the problem.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    I sent an email to MG Electronics asking for a schematic, but I doubt they will respond as they have been unresponsive so far.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    A schematic could make all the difference.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    I also got in the analog multimeter like you have.  I still need to test the capacitors....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    That is excellent news. The first thing that I want you to do once you get it set up is to put it on the Ohms RX1 scale. Next take your digital meter set to volts and read the voltage across the probes from the analog meter. Note which of the two analog probes your red digital meter probe is on when it indicates a positive voltage. We are determining the polarity of the voltage that is being used by the analog meter. It may not correspond to the colors of the leads. For example on my analog meter the black lead actually has the positive polarity. Let me know if the black or the red lead of the analog meter has the positive voltage so  are testing with the analog meter I can better understand what is going on. Use the analog meter to go back and test the 1N5402 Diodes. You should find that the meter needle will deflect towards zero when the positive lead of the analog meter is on the side of the diode that is away from the marker line and it will not deflect when the probes are reversed. This is the indication of a good diode.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    I'll be able to get to that on Monday.

     

    I just heard back from the CEO of https://www.professormotor.com/  where I purchased the unit.  They said that MG Electronics had refused to honor returns and warranties on over 100 hundred units that they had purchased.  He has no details on the schematic but said 'most power supplies of this type fail by the output transistor or the rectifiers going bad.'  He will scour the shop and look for potential parts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to mpulliam

    Well this didn't take too long.  I have to cross the leads to get positive voltage (black/negative digital MM to red/positive analog MM and red/positive digital mm to black/negative analog MM)

     

    My first test I was the top left diode and it deflected immediately and then went back to zero and stayed there. It repeated tested at zero as did the rest of the diodes.

     

    image

     

    All diodes tested the same.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    That looks good. The leads of the meter have a positive voltage on the Black and a negative voltage on the Red. The meter allows you to apply a 3 volt voltage to any component and the meter tells you whether a current is flowing or not. If you test a large uncharged capacitor and you put the Red lead on the side with the line (negative) and the Black on the positive lead of the capacitor the meter will deflect and then gradually return to zero. This is the effect of the capacitor charging. When it is empty it draws a lot of current and as it fills the current flow lessens, You can also test transistors with the meter . Put the black on the base and move the Red to the collector and emitter. If it is an NPN transistor you will see a nearly equal deflection. Now reverse the leads with the Red on the base and you should see no deflection. There may be a little deflection between the Emitter and Collector depending on the polarity. If the meter deflects all the way this is indication of a short and may indicate a failed transistor. Any full deflection on diodes in both polarities will be a likely bad diode. You can check the smaller capacitors as well. On the smaller capacitors you may need to got to the RX10 or RX100 scales in order to see a small momentary deflection. For testing most components the RX1 scale is the best. If the meter deflects all the way to zero while testing any of the components except an inductor it is a sign of a potential problem. Sometimes it is necessary to take a component out of the circuit but most of the time you can get a pretty good test result right in the circuit.  Do some experimenting and testing of components. Always look at the component in both polarities. Sometimes other components in the circuit will affect your reading in one polarity more than the other. Good luck and ask questions as needed. If I had to go on a service call and I could take only one instrument with me it would be the little analog meter.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer