Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14793 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • mpulliam
    0 mpulliam over 6 years ago

    7812 voltage regulator test results:

    w/ Power off and writing facing me

    Black lead on the center pin, read lead on the left pin = 1.2mV and it trickled down to 0

    Black lead on the center pin, read lead on the right pin = .5mV and it trickled down to a negative number

     

    w/ Power On and writing facing me

    Black lead on the center pin, read lead on the left pin = 30V

    Black lead on the center pin, read lead on the right pin = 12.04v

     

    I re-tested the D313 for continuity (after the unit has been turned on and off)

    There is NO continuity between the base and the emitter or collector

    There IS continuity between the emitter and the collector

     

    I retested the corroded diode and it is ok.  The corrosion was giving me a bad reading previously but I scraped it off and the diode shows a voltage reading of .519v in one direction and nothing in the other.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    All sounds good and normal except the D313. We need to test that one out of circuit and verify if it is good or bad.

     

    At some point I mistyped Read when I meant to type Red. I mention it so that we don't start a new convention for what is the correct nomenclature.  Sorry about that. I always try to proofread but at 1:30 AM I may miss things.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    I'll be able to get to that on Monday.

     

    I just heard back from the CEO of https://www.professormotor.com/  where I purchased the unit.  They said that MG Electronics had refused to honor returns and warranties on over 100 hundred units that they had purchased.  He has no details on the schematic but said 'most power supplies of this type fail by the output transistor or the rectifiers going bad.'  He will scour the shop and look for potential parts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to mpulliam

    Well this didn't take too long.  I have to cross the leads to get positive voltage (black/negative digital MM to red/positive analog MM and red/positive digital mm to black/negative analog MM)

     

    My first test I was the top left diode and it deflected immediately and then went back to zero and stayed there. It repeated tested at zero as did the rest of the diodes.

     

    image

     

    All diodes tested the same.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    That looks good. The leads of the meter have a positive voltage on the Black and a negative voltage on the Red. The meter allows you to apply a 3 volt voltage to any component and the meter tells you whether a current is flowing or not. If you test a large uncharged capacitor and you put the Red lead on the side with the line (negative) and the Black on the positive lead of the capacitor the meter will deflect and then gradually return to zero. This is the effect of the capacitor charging. When it is empty it draws a lot of current and as it fills the current flow lessens, You can also test transistors with the meter . Put the black on the base and move the Red to the collector and emitter. If it is an NPN transistor you will see a nearly equal deflection. Now reverse the leads with the Red on the base and you should see no deflection. There may be a little deflection between the Emitter and Collector depending on the polarity. If the meter deflects all the way this is indication of a short and may indicate a failed transistor. Any full deflection on diodes in both polarities will be a likely bad diode. You can check the smaller capacitors as well. On the smaller capacitors you may need to got to the RX10 or RX100 scales in order to see a small momentary deflection. For testing most components the RX1 scale is the best. If the meter deflects all the way to zero while testing any of the components except an inductor it is a sign of a potential problem. Sometimes it is necessary to take a component out of the circuit but most of the time you can get a pretty good test result right in the circuit.  Do some experimenting and testing of components. Always look at the component in both polarities. Sometimes other components in the circuit will affect your reading in one polarity more than the other. Good luck and ask questions as needed. If I had to go on a service call and I could take only one instrument with me it would be the little analog meter.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    Everything I've tested looks good, but I haven't gone through and tested procedurally, so must have missed something or I'm testing incorrectly. 

     

    I got in touch with MG Electronics.  They just buy these as black boxes from China and resell - no schematic available. Service guy said he's never opened one up.  He suggested to follow the voltage from the outlet to the front of the unit and vice-versa.   Maybe it could be the front terminals and to test for voltage from the inside, and to test the potentiometer on the output.  Other than that, could be just some small component that went out somewhere down the line...

     

    M

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    Hi Matt,

     

    I would like to have you test the potentiometer on the front. With the power turned off, use the resistance setting on the digital meter and test the resistance from the two outside terminals. Next put one probe on an outside and middle terminal and slowly turn the control from one end to the other. You should see a gradual change from zero to the reading that you got on the two outside terminals.

     

    Next let's measure voltages on the LM741 integrated circuits. Turn on the unit. Turn the potentiometer of the unit fully CCW. Put your digital meter on volts. Place the black probe on pin 4 Take voltage readings on each of the other pins 1,2,3,5,6,7,8 and write them down. Now turn the potentiometer fully CW and repeat the taking of voltages. Do this for each of the two LM 741 ICs.

     

    Let me know what the voltages are and I will try to interpret them. Remember the numbering of the IC pins as described in a previous post.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    One more thing to check. There are a lot of brown disk capacitors on the main board. Use the GMT analog meter set on RX1 and test across each of the capacitors when the power is off. You may see some needle movement. We are looking for situation when the needle deflects all the way to zero ohms.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    Here are the diode tests. Notice I set the R value to X10

     

    imageimageimageimageimageimageimageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to mpulliam

    Here are the brown capacitor tests at X1

     

    imageimageimageimageimageimageimageimageimageimageimageimage

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    I tried to test the resistance on the outside terminals with my digital multimeter.  The ohms keep increasing until it gets to 0L.

     

    My guess is that is charging a capacitor that is connected to inside terminals....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to mpulliam

    Yes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to mpulliam

    Yes.