Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14698 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • mpulliam
    0 mpulliam over 6 years ago

    7812 voltage regulator test results:

    w/ Power off and writing facing me

    Black lead on the center pin, read lead on the left pin = 1.2mV and it trickled down to 0

    Black lead on the center pin, read lead on the right pin = .5mV and it trickled down to a negative number

     

    w/ Power On and writing facing me

    Black lead on the center pin, read lead on the left pin = 30V

    Black lead on the center pin, read lead on the right pin = 12.04v

     

    I re-tested the D313 for continuity (after the unit has been turned on and off)

    There is NO continuity between the base and the emitter or collector

    There IS continuity between the emitter and the collector

     

    I retested the corroded diode and it is ok.  The corrosion was giving me a bad reading previously but I scraped it off and the diode shows a voltage reading of .519v in one direction and nothing in the other.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    All sounds good and normal except the D313. We need to test that one out of circuit and verify if it is good or bad.

     

    At some point I mistyped Read when I meant to type Red. I mention it so that we don't start a new convention for what is the correct nomenclature.  Sorry about that. I always try to proofread but at 1:30 AM I may miss things.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    If I'm measuring Resistance, then it's 15 Ohms between Yellow (base) wire on different transistors in both polarities (at X1)

    Between Red to Reds it's also 15 Ohms

    Between Blue to Blues it's also 15 Ohms

    Between Red to Blues there is no reading

     

    Affirmative continuity between negative on both big capacitors and negative banana plug

     

    The continuity between the big capacitors and the LM741 is screwy.  It seems to change...

    Negative continuity between negative on both big capacitors and #4 pin on each of the LM741 ICs, except that there was continuity for a second

     

    Positive continuity between negative on both big capacitors and #2 pin on each of the LM741 ICs, and then there was no continuity

    Intermittent continuity between the positive on both capacitors and some of the pins of each of the LM741 ICs

     

    Positive continuity between the top row of rectifier diodes on the non-line side and the #2 pin on each of the LM741 ICs, then negative continuity

    Negative continuity between the bottom row of rectifier diodes on either side of diode and the #2 pin on each of the LM741 ICs

     

     

    Positive continuity between each of the blue wires on the power transistors and the Red Banana Jack

    Negative continuity between each of the yellow wires on the power transistors and the Red Banana Jack

     

    16.5V between Red wire of power transistor and black banana plug, then turning the front range selector

    26.14V

    36.9V

     

    Black banana plug to yellow transistor wire (all were the same)

    36.7V

     

    Black banana plug to blue transistor wire (all were the same)

    .6V

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    I wanted to thank you for your patience and thoughtful explanations!   I really appreciate it!! 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

    The voltages that you provided tell me that the Output transistors are likely failed open. I just need to confirm that the voltage on the blue wire was 0.6 Volts?

     

    I recommend that you bite the bullet and remove one of the output transistors so we can test it and verify that it is bad. Don't order replacements without talking to me first. Once it is out use the analog meter to run the same test we just ran on them when they were in the circuit.

     

    With 36 volts on the collector and 36 volts on the base the emitter should also be at approx 36 volts not 0.6 volts as this is an NPN transistor.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    Confirm, I'm reading .6V between the blue wires and the negative banana plug

    36V between Red and the negative banana plug

    36V between Yellow and the negative banana plug

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to mpulliam

    Actually, it's -.6V

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

     

    Here are some thoughts on the Output Transistors. If the wires are long enough you might try pulling the wires through the holes in the heat sink and then desoldering them or just clip them off and make new connections to the new transistors. I believe that the coils of wire on the circuit board are emitter resistors. One blue wire should run to one end of each coil and the other ends of the coils should be connected to the red banana jack on the front panel. Confirm to me that this is the case. Otherwise we may need to install our own emitter resistors to help the outputs avoid thermal runaway. When you remount the new output transistors you should either use a teflon insulator or if you are going to use the original mica insulators silicone heat sink compound needs to be used. We want the heat from the 2N3055s to easily transfer to the heat sinks. I saw that Newark has some reasonably priced 2N3055s

     

    https://www.newark.com/multicomp/2n3055h/bipolar-transistor-npn-60v/dp/78M7081?st=2n3055

     

    Get yourself at least one extra just in case. Also you should be able to find the teflon heat sink insulators on Newark. I still want to see the results of your out of circuit test of the 2N3055 before we go ahead but I had some time so I jumped ahead to these ideas on replacing the 2N3055s.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    Hi John,

     

    The wires are not very long and there is no slack. It would be a delicate operation without much room for error to desolder and solder.  I would probably need surgical tools.

    The blue wires go to the bottom of the circuit board then up to I believe the curly q resistance coils (I don't what they are called) then on to the resistor next to it.  From there it's a maze.

     

    Working from the red banana jack back, it's tied to the front Amp Meter and then back to the circuit board (it's the thick red cable coming out of the middle of the board)

     

    In my research, bad power supplies seem to have usual suspects:

     

    If not blown fuses, loose wires, corrosion, broken traces, or cold solder joints then -

     

    Typically goes out:

    Transistors

    Electrolytic Capacitors

    Integrated Circuits

    Diodes

     

    Sometimes goes out:

    Mechanical switches and potentiometers

    Resistors

    Non-polarized capacitors

     

    Usually never goes out:

    Transformers

    Variable capacitors

    Inductors

     

    Also testing components in circuit could yield bad readings.

     

    So I'm willing to order replacements for the ICs, transistors not yet replaced, the power transistors and whatever else you'd recommend.  The parts are cheap but shipping adds up.  I'll give replacing the components a go and if it works great, if not, I'm not sure the unit is worth any more trouble. 

    Thanks,

    Matt

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

    At this point based on your voltage readings the Output transistors are definitely a problem. I would start by replacing them. If that doesn't solve the problem we can go back and look at secondary causes. There are two wires on each output transistor that need to be replaced. The collector is connected through the screws that mount the transistor. You could even cut the pins off the old transistors and then solder on a short piece of wire and seal the connection with heat shrink. This would give extra wire to come through the heat sink and solder on to the new transistor. This extra wire could then be pushed back through the heat sink when the transistor is remounted to the sink. Hold off on replacing anything else until we have done the outputs. If you want to take more detailed pictures of the difficulty replacing the outputs I will see if I can come up with more ideas to make it easier.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    Hi John,

     

    I have a thought.  If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between the blue terminal and the red banana jack could be bad, (and not the output transistor) thus creating the low voltage?

     

    For example, the blue terminal on the output transistors tested positive for continuity with pin 2 on one of the LM741 IC (the lower right one) but gave a weird electronic sound when testing for continuity with pin 2 on the top left LM741 IC.  If the LM741's function is the same on this linear power supply as the ICs on switching power supplies, as detailed HERE in the 6th paragraph down, (which regulates the output voltage of the transistors) then a bad IC could result in low voltage.

     

    Thoughts?

    Matt

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

     

    Sorry but due to the physics of a functional transistor the voltages that you have measured are not possible. Therefore we must conclude that these are not functional transistors. there is an energy barrier of about 0.7 Volts between the Base and the Emitter. Any time that energy barrier is exceeded current flow in the BE circuit. This also causes the CE current to flow. I think the BE junction can handle a few volts for a short period of time but anything more than that would cause it to burn out. Your measurements indicate that there is over 36 volts across this junction and therefore it is apparently already burned out. Until these transistor are replaced and functional we can't further trouble shoot the circuit easily.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

     

    Sorry but due to the physics of a functional transistor the voltages that you have measured are not possible. Therefore we must conclude that these are not functional transistors. there is an energy barrier of about 0.7 Volts between the Base and the Emitter. Any time that energy barrier is exceeded current flow in the BE circuit. This also causes the CE current to flow. I think the BE junction can handle a few volts for a short period of time but anything more than that would cause it to burn out. Your measurements indicate that there is over 36 volts across this junction and therefore it is apparently already burned out. Until these transistor are replaced and functional we can't further trouble shoot the circuit easily.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    Hi John

    So what do I need to order?

    NTE130 or 2N3055H

    Do I need thermal paste?

     

    What type of LM741CN IC?  This one?  If so, it's backordered, is there a suitable replacement you'd recommend?

    Ceramic capacitors? Diodes?  Resistors?

     

    It cost $9.99 to ship a .10 cent component.   I'm already in for about $35 with the analog multimeter and the transistor.  I could buy a new unit with free shipping for $83.

    It doesn't make sense to buy one component at time to see if it's a fix.

     

    Thanks,
    Matt

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to mpulliam

    mpulliam  wrote:

    ...

    It cost $9.99 to ship a .10 cent component.

    ...

    For companies that have free delivery above an amount, I add consumables like solder, flux, wick, spare cutter blades ...

    Your repair will never be economical. If you do it for the fun of learning, you'll have a good time. Even if it fails.

    But it 'll never be worth it in $$.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

     

    I would get the 2N3055 as opposed to the NTE 130s if I had the choice.

     

    https://www.newark.com/multicomp/2n3055h/bipolar-transistor-npn-60v/dp/78M7081?st=2n3055

     

    You will also need to get some of these:

     

    https://www.newark.com/nte-electronics/tp0001/thermal-insulators-thermo-pad/dp/79M5626?st=to-3%20insulator

     

    Which can be used without thermal paste. If you want to reuse the current mica insulators, if they are in good condition, you will need to put a thin layer of thermal paste on the contacting surfaces. Be sure to install the insulators before soldering the wires to the pins..

     

    If you want to save on shipping you might check to see what your electronic store resources are in your city. I would be surprised if you couldn't find a local store that would have these two items though what you save in shipping might be offset by higher component prices.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to jw0752

    jw0752  wrote:

     

    H...

     

    If you want to save on shipping you might check to see what your electronic store resources are in your city. I would be surprised if you couldn't find a local store that would have these two items though what you save in shipping might be offset by higher component prices.

     

    John

    I do that here. In Brussels there's a shop called Elak. They have loads in stock. And I can order anything from element14 / Farnell.

    Because they order from there, my components are a tiny part of their order.

    They have a markup. For most orders lower than what I'd pay for shipping.

    And I prefer to spend the extra money there rather than on FedEx/UPS - who try to make my life miserable whenever they spot the opportunity.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy

     

    and...

     

    imageimage

     

    Success!!!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to mpulliam

    BTW

    I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055.  There is no continuity between any of the terminals

    But when I run a diode test, a new 2N3055 tests at .486 volts with negative on the emitter, and the positive on the base.  .OL in any other test configuration.

    The old 2N3055's test at .OL in every test configuration.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fmilburn
    0 fmilburn over 5 years ago in reply to mpulliam

    Hi Matt,

    Hurray!  Well done.  I am curious what the theory is on why these failed.  If I remember correctly it was working one day for you and the next time you turned it on it wasn't working.  Maybe John has a thought.

    Frank

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Congratulations Matt,

     

    You stuck with it and you won the battle. Your diligence in taking good measurements and notes as well as useful pictures made all the difference. I hope you stick around the forum and continue your adventure in electronics. Don't hesitate to share your projects. The next time someone needs one of these fixed you are the go to expert.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    John, thank you very much for your knowledge and ability to communicate it!

     

    Matt

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to fmilburn

    Hi Frank,

     

    I think that the problem comes from the paralleling of the (4) 2N3055 output transistors. When the unit is used at High current and low voltage the 4 transistors have the challenge of getting rid of the extra power that is not being used. In a perfectly balanced system they would each carry 1/4th of the load and all might be well. Unfortunately they are not perfectly balanced and the one transistor that insists on taking more of the load gets hotter and hotter until it fails. In this case it seems that they fail open Base Emitter which takes the most ambitious transistor off line and transfers the load to the remaining three. One by One they fail until we are left with the situation that Matt had. The designer realized that this was a potential problem so they put emitter resistors on each of the Outputs as this helps to balance the load. This are the stretched out coils that we see on one circuit board. I am sure that they help but apparently not enough to prevent failure. Since we have seen two of these units with the same problem on the forum I would guess that these failures are a design problem.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer