Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14714 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
Parents
  • mpulliam
    0 mpulliam over 6 years ago

    7812 voltage regulator test results:

    w/ Power off and writing facing me

    Black lead on the center pin, read lead on the left pin = 1.2mV and it trickled down to 0

    Black lead on the center pin, read lead on the right pin = .5mV and it trickled down to a negative number

     

    w/ Power On and writing facing me

    Black lead on the center pin, read lead on the left pin = 30V

    Black lead on the center pin, read lead on the right pin = 12.04v

     

    I re-tested the D313 for continuity (after the unit has been turned on and off)

    There is NO continuity between the base and the emitter or collector

    There IS continuity between the emitter and the collector

     

    I retested the corroded diode and it is ok.  The corrosion was giving me a bad reading previously but I scraped it off and the diode shows a voltage reading of .519v in one direction and nothing in the other.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    All sounds good and normal except the D313. We need to test that one out of circuit and verify if it is good or bad.

     

    At some point I mistyped Read when I meant to type Red. I mention it so that we don't start a new convention for what is the correct nomenclature.  Sorry about that. I always try to proofread but at 1:30 AM I may miss things.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

    At this point based on your voltage readings the Output transistors are definitely a problem. I would start by replacing them. If that doesn't solve the problem we can go back and look at secondary causes. There are two wires on each output transistor that need to be replaced. The collector is connected through the screws that mount the transistor. You could even cut the pins off the old transistors and then solder on a short piece of wire and seal the connection with heat shrink. This would give extra wire to come through the heat sink and solder on to the new transistor. This extra wire could then be pushed back through the heat sink when the transistor is remounted to the sink. Hold off on replacing anything else until we have done the outputs. If you want to take more detailed pictures of the difficulty replacing the outputs I will see if I can come up with more ideas to make it easier.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    Hi John,

     

    I have a thought.  If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between the blue terminal and the red banana jack could be bad, (and not the output transistor) thus creating the low voltage?

     

    For example, the blue terminal on the output transistors tested positive for continuity with pin 2 on one of the LM741 IC (the lower right one) but gave a weird electronic sound when testing for continuity with pin 2 on the top left LM741 IC.  If the LM741's function is the same on this linear power supply as the ICs on switching power supplies, as detailed HERE in the 6th paragraph down, (which regulates the output voltage of the transistors) then a bad IC could result in low voltage.

     

    Thoughts?

    Matt

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

     

    Sorry but due to the physics of a functional transistor the voltages that you have measured are not possible. Therefore we must conclude that these are not functional transistors. there is an energy barrier of about 0.7 Volts between the Base and the Emitter. Any time that energy barrier is exceeded current flow in the BE circuit. This also causes the CE current to flow. I think the BE junction can handle a few volts for a short period of time but anything more than that would cause it to burn out. Your measurements indicate that there is over 36 volts across this junction and therefore it is apparently already burned out. Until these transistor are replaced and functional we can't further trouble shoot the circuit easily.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    Hi John

    So what do I need to order?

    NTE130 or 2N3055H

    Do I need thermal paste?

     

    What type of LM741CN IC?  This one?  If so, it's backordered, is there a suitable replacement you'd recommend?

    Ceramic capacitors? Diodes?  Resistors?

     

    It cost $9.99 to ship a .10 cent component.   I'm already in for about $35 with the analog multimeter and the transistor.  I could buy a new unit with free shipping for $83.

    It doesn't make sense to buy one component at time to see if it's a fix.

     

    Thanks,
    Matt

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to mpulliam

    mpulliam  wrote:

    ...

    It cost $9.99 to ship a .10 cent component.

    ...

    For companies that have free delivery above an amount, I add consumables like solder, flux, wick, spare cutter blades ...

    Your repair will never be economical. If you do it for the fun of learning, you'll have a good time. Even if it fails.

    But it 'll never be worth it in $$.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 5 years ago in reply to mpulliam

    Hi Matt,

     

    I would get the 2N3055 as opposed to the NTE 130s if I had the choice.

     

    https://www.newark.com/multicomp/2n3055h/bipolar-transistor-npn-60v/dp/78M7081?st=2n3055

     

    You will also need to get some of these:

     

    https://www.newark.com/nte-electronics/tp0001/thermal-insulators-thermo-pad/dp/79M5626?st=to-3%20insulator

     

    Which can be used without thermal paste. If you want to reuse the current mica insulators, if they are in good condition, you will need to put a thin layer of thermal paste on the contacting surfaces. Be sure to install the insulators before soldering the wires to the pins..

     

    If you want to save on shipping you might check to see what your electronic store resources are in your city. I would be surprised if you couldn't find a local store that would have these two items though what you save in shipping might be offset by higher component prices.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to jw0752

    jw0752  wrote:

     

    H...

     

    If you want to save on shipping you might check to see what your electronic store resources are in your city. I would be surprised if you couldn't find a local store that would have these two items though what you save in shipping might be offset by higher component prices.

     

    John

    I do that here. In Brussels there's a shop called Elak. They have loads in stock. And I can order anything from element14 / Farnell.

    Because they order from there, my components are a tiny part of their order.

    They have a markup. For most orders lower than what I'd pay for shipping.

    And I prefer to spend the extra money there rather than on FedEx/UPS - who try to make my life miserable whenever they spot the opportunity.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to jw0752

    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy

     

    and...

     

    imageimage

     

    Success!!!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mpulliam
    0 mpulliam over 5 years ago in reply to mpulliam

    BTW

    I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055.  There is no continuity between any of the terminals

    But when I run a diode test, a new 2N3055 tests at .486 volts with negative on the emitter, and the positive on the base.  .OL in any other test configuration.

    The old 2N3055's test at .OL in every test configuration.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fmilburn
    0 fmilburn over 5 years ago in reply to mpulliam

    Hi Matt,

    Hurray!  Well done.  I am curious what the theory is on why these failed.  If I remember correctly it was working one day for you and the next time you turned it on it wasn't working.  Maybe John has a thought.

    Frank

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fmilburn
    0 fmilburn over 5 years ago in reply to mpulliam

    Hi Matt,

    Hurray!  Well done.  I am curious what the theory is on why these failed.  If I remember correctly it was working one day for you and the next time you turned it on it wasn't working.  Maybe John has a thought.

    Frank

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 5 years ago in reply to fmilburn

    Hi Frank,

     

    I think that the problem comes from the paralleling of the (4) 2N3055 output transistors. When the unit is used at High current and low voltage the 4 transistors have the challenge of getting rid of the extra power that is not being used. In a perfectly balanced system they would each carry 1/4th of the load and all might be well. Unfortunately they are not perfectly balanced and the one transistor that insists on taking more of the load gets hotter and hotter until it fails. In this case it seems that they fail open Base Emitter which takes the most ambitious transistor off line and transfers the load to the remaining three. One by One they fail until we are left with the situation that Matt had. The designer realized that this was a potential problem so they put emitter resistors on each of the Outputs as this helps to balance the load. This are the stretched out coils that we see on one circuit board. I am sure that they help but apparently not enough to prevent failure. Since we have seen two of these units with the same problem on the forum I would guess that these failures are a design problem.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • fmilburn
    0 fmilburn over 5 years ago in reply to jw0752

    I thought that might be it.  It is a common problem in parallel systems whether they be splitting fluids or electrons unless there is some sort of active control.