Power & Energy
  • Technologies
  • More
Power & Energy
Forum Need to get MG Electronics Power Supply repaired...or NOT!?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 120 replies
  • Answers 51 answers
  • Subscribers 285 subscribers
  • Views 14684 views
  • Users 0 members are here
Related

Need to get MG Electronics Power Supply repaired...or NOT!?

e14 Contributor
e14 Contributor over 11 years ago

Hi.

I just bought a lot of Slot Car stuff, yes those cars that go around a track. The guy was serious about his hobby he didn't have the usual wall plug in power pack, he used a MG Electronics PS-10AD, 0-20 VDC at 10 Amps. Well this power supply doesn't work anymore. It does turn on and the red overload light stays on. It doesn't put out anything. I used my multimeter etc., nothing. I know that these are made overseas . They did retail for about $200. So the questions is were can I get it repaired OR should I ? I'm in Western MAss.

I did check the fuse , it's fine. I've got a heavy door stop on my hands, it does have a nice handle and cord on it !

Many thanks for info, Ted

 

http://www.mgelectronics.com/shopexd.asp?id=179

  • Sign in to reply
  • Cancel

Top Replies

  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +4 suggested
    Well, I spent all day replacing four 2N3055 transistors....it wasn't easy and... Success!!!
  • mpulliam
    mpulliam over 5 years ago in reply to jw0752 +3
    Hi John, I have a thought. If the output transistors (or is it pass or power transistors?) NTE130 or 2N3055H are giving a bad voltage reading in the voltage test, could it be that any component between…
  • mpulliam
    mpulliam over 5 years ago in reply to mpulliam +3 suggested
    BTW I tested the old 2N3055 transistors, the continuity is the same as a new 2N3055 . There is no continuity between any of the terminals But when I run a diode test, a new 2N3055 tests at .486 volts with…
  • mpulliam
    0 mpulliam over 6 years ago in reply to mpulliam

    Discovery, by following the wires I figured out there are actually a total of (4) 2N3055 power transistors (not 2) hidden in all the heat sinks.... the blue and yellow wires are soldered to the transistor leads so removing them completely will be a chore. 

     

    Here a pic of the transistor tucked away behind a set of heat sinks...  the picture is actually upside down so I could read the description.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    I believe that the transistors are not soldered in but rather plugged into sockets. Once you have taken the screws out I believe that the transistors will unplug. At least I hope this is the case. If the wires are indeed soldered to the pins then you will have no choice except to unsolder them. The reason that they use matched pairs is so the transistors, which all vary slightly from one another, work together and share the load equally. If the transistors are badly mismatched the burden of the work will fall on the weaker of the two devices and it will fail more quickly. Keep in mind that unless there is a short between the Emitter and the Collector these transistors are not likely to be the cause of the problem with the power supply.  I am still trying to figure out what the next step is.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    Hi Matt;

    I think your best bet for continuing will be to see if you can find, locally, an old retired radio TV service technician to look over your shoulder and help trouble shoot the unit. I really can't think of any way to direct you to the next steps remotely. When you finally crack this puzzle please come back and post about it as my curiosity is killing me.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    The are definitely soldered and it would be a major pain to take it all apart to completely isolate the transistors from the unit in order to test them.

     

    There are also the rectifier diodes, which I didn't know what they were at first because they tested like capacitors while on the board.

     

    I can desolder one end of each diode and test them before I completely remove the transistors

     

    image

    Solder joints on one of the transistors.  Hardly any wiggle room to work with and the back end of the unit would have to be dissembled in order to reconnect everything.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    Hi Matt,

     

    As long as there isn't continuity between the yellow and the metal case of the transistor they are probably good and I would not unsolder them. The diodes that you show should be able to be tested in the circuit using your diode test. I would expect about 0.5 Volts on each of them in one polarity only.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    The rectifier diodes test at .403 V with the black lead on anode side. When I reverse the leads, I get a reading of about .5V and it starts going up to 1V where I'll get a .0L reading (overload)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    The 0.403 Volts would be normal for a Schottky Diode. Can you read the numbers on the diode? We can look it up to verify this. The voltage you are seeing on the reverse polarity is likely just seeing the capacitors charging and sounds normal for in circuit measuring.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    I can make out N5402 with an NB below it. Maybe there's a 1 before the N, but I'm not certain.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jw0752
    0 jw0752 over 6 years ago in reply to mpulliam

    Yes that would be a 1N5402 which has a 3 Amp current capacity and can tolerate 200 Volts. The some of the ones in your power supply are probably being used in parallel to accommodate the higher current of the power supply. If you were to take them out of the circuit I would expect the diode test to be closer to 0.55 Volts as these are not Schottky diodes. Your test however has convinced me that they are not the problem.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mpulliam
    0 mpulliam over 6 years ago in reply to jw0752

    I sent an email to MG Electronics asking for a schematic, but I doubt they will respond as they have been unresponsive so far.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>