Power & Energy
  • Technologies
  • More
Power & Energy
Forum Single Phase to three signal generator.
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Subscribers 280 subscribers
  • Views 4451 views
  • Users 0 members are here
  • power supply
  • circuit
  • power_supply
  • power
  • power.power
Related

Single Phase to three signal generator.

Jere9522
Jere9522 over 4 years ago

Hello everyone,
I am designing a low voltage power supply that will run single phase to three phase circuit and will be using ultrosonic frequency as its signal input. The current circuit design uses three operational amplifiers that has a 60 degress phase shift. I am encountering a problem with regards to the output amplitude of the three phase signals. It seems to have a decrease in the amplitude. I also used RC oscillator circuit in front of the op-amp to have a precise phase shift. I am asking for any suggestions or how to deal with this problem? Also, are there any concept that I can study to approach this problem? I am also thinking to apply DSP filtering to elimate the noise in the output. Thank you in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 4 years ago +2 verified
    I'm not entirely sure what you're looking for, especially the ultrasonic bit! A diagram would definitely help. For the 3-phase generation portion, in theory that's quite easy using any microcontroller…
  • genebren
    genebren over 4 years ago +2 verified
    It would appear from your schematic, that because the output of the first stage, feeds the input of the second stage, and the output of the second stage feeds the input for the third, the amplitude changes…
  • jc2048
    jc2048 over 4 years ago in reply to Jere9522 +2
    Don't try it as you've drawn it. The maximum supply for a MCP6291 is 6V, 10V will blow it up.
Parents
  • phoenixcomm
    0 phoenixcomm over 4 years ago

    First, let me quote you. 

    "I am designing a low-voltage power supply that will run single-phase to three-phase circuit and will be using ultrasonic frequency as its signal input. The current circuit design uses three operational amplifiers that has a 60 degrees phase shift."

    To convert single-phase to three-phase should be at 120 degrees apart, Not 60 degrees as 60+60+60 = 180 degrees not 360 degrees. Also, your scope trace clearly shows two signals not three. I work at 400Hz and I use three audio amps to provide isolation. And besides my target voltage is 48 vac which I step up to 11 5vac to get a clean signal you will need to clean up the source I assume ( your input is a PWM output from sort of a processor )  you can clean it up with a RC network.  this would be phase A, then you need to delay it 120 degrees for phase B and one more time to get the phase C. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to phoenixcomm
    phoenixcomm said:
    your scope trace clearly shows two signals not three

    There are 3 signals. The blue one is hard to spot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 4 years ago in reply to Jan Cumps

    do you mean the noise on the base line?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to phoenixcomm

    No:
    image

    There's a dark blue line there. Hard to see. I drew over it in light blue to make it standing out more.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to phoenixcomm

    No:
    image

    There's a dark blue line there. Hard to see. I drew over it in light blue to make it standing out more.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 4 years ago in reply to Jan Cumps

    I could not see that too on the original image. The OP is using Multisim, where the colors can be user-selected, but the original dark black-blue was not ideal : )