Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power supply for a tethered drone
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 281 subscribers
  • Views 5026 views
  • Users 0 members are here
Related

Power supply for a tethered drone

roineust
roineust over 4 years ago

There is a drone which I'm experimenting with and want to move from batteries to a 2-15 meters 14AWG tethered cable.

The drone voltage is 15-21 Volts and consumes up to 200 Amps.

What would be the best method of searching for and the best brand, model and condition new or used, to find a good but not expensive power supply for the drone?

What are the chances that the following ebay unbranded power supply, would be a bad choice?

www.ebay.com/.../284832076705

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago +4
    I think you would be risking your $1200 - I've had mixed results from very low cost power supplies, never tried one as big as this. That's a very low price for a 6kw power supply - the spec on Ebay isn…
  • Gough Lui
    Gough Lui over 4 years ago +4
    Aside from that very suspect power supply, the cable is not going to be cheap or light. Just look at the ampacity charts ( learnmetrics.com/.../) and it seems you need something about 85mm^2 cross-section…
  • dougw
    dougw over 4 years ago +4
    That sounds like a beast of a drone - over 5 horsepower. At 200 Amps you would be looking at welding cables. Even the mains supply will need to be pretty substantial. Are you planning to put the power…
Parents
  • Gough Lui
    Gough Lui over 4 years ago

    Aside from that very suspect power supply, the cable is not going to be cheap or light. Just look at the ampacity charts (learnmetrics.com/.../) and it seems you need something about 85mm^2 cross-section. That's jumper-cable thickness. The weight of that alone would also likely keep your drone tethered quite firmly to the ground ... The cost is also around US$30/m per conductor, multiplied by two for positive and negative. That works out to be US$900 of cable alone.

    - Gough

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Gough Lui
    Gough Lui over 4 years ago

    Aside from that very suspect power supply, the cable is not going to be cheap or light. Just look at the ampacity charts (learnmetrics.com/.../) and it seems you need something about 85mm^2 cross-section. That's jumper-cable thickness. The weight of that alone would also likely keep your drone tethered quite firmly to the ground ... The cost is also around US$30/m per conductor, multiplied by two for positive and negative. That works out to be US$900 of cable alone.

    - Gough

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to Gough Lui

    The only way to get those costs lower, is to lower the current. To do that, roineust will have to up the voltage.

    But then, a DC-DC converter will have to be built into the drone. Again, not a light component to get into the drone - albeit lighter than meters of a 85 mm^2 copper cable.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to Jan Cumps

    Agree, maybe 48V or higher, if it's allowed. Also, maybe a hybrid method could be interesting too, using the battery for high current demand periods, but using the tethered connection at all other times. Probably requires a lot more sophisticated design and software!