Power & Energy
  • Technologies
  • More
Power & Energy
Forum Power supply for a tethered drone
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 281 subscribers
  • Views 5022 views
  • Users 0 members are here
Related

Power supply for a tethered drone

roineust
roineust over 4 years ago

There is a drone which I'm experimenting with and want to move from batteries to a 2-15 meters 14AWG tethered cable.

The drone voltage is 15-21 Volts and consumes up to 200 Amps.

What would be the best method of searching for and the best brand, model and condition new or used, to find a good but not expensive power supply for the drone?

What are the chances that the following ebay unbranded power supply, would be a bad choice?

www.ebay.com/.../284832076705

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 4 years ago +4
    I think you would be risking your $1200 - I've had mixed results from very low cost power supplies, never tried one as big as this. That's a very low price for a 6kw power supply - the spec on Ebay isn…
  • Gough Lui
    Gough Lui over 4 years ago +4
    Aside from that very suspect power supply, the cable is not going to be cheap or light. Just look at the ampacity charts ( learnmetrics.com/.../) and it seems you need something about 85mm^2 cross-section…
  • dougw
    dougw over 4 years ago +4
    That sounds like a beast of a drone - over 5 horsepower. At 200 Amps you would be looking at welding cables. Even the mains supply will need to be pretty substantial. Are you planning to put the power…
Parents
  • dougw
    dougw over 4 years ago

    That sounds like a beast of a drone - over 5 horsepower.

    At 200 Amps you would be looking at welding cables. Even the mains supply will need to be pretty substantial.

    Are you planning to put the power supply onboard and run AC through the tether? It might be less weight than 200 A cables.

    As far as using that power supply, I wouldn't expect it to put out its maximum power over long periods - it only weighs 8 Kg.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 4 years ago

    That sounds like a beast of a drone - over 5 horsepower.

    At 200 Amps you would be looking at welding cables. Even the mains supply will need to be pretty substantial.

    Are you planning to put the power supply onboard and run AC through the tether? It might be less weight than 200 A cables.

    As far as using that power supply, I wouldn't expect it to put out its maximum power over long periods - it only weighs 8 Kg.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to dougw
    dougw said:
    At 200 Amps you would be looking at welding cables. Even the mains supply will need to be pretty substantial.

    Yes. Most 100+ amp designs I've seen, the cable was a fixed copper bar. And the cables that allow 200 A are almost as inflexible as such a bar.

    • Cancel
    • Vote Up +3 Vote Down