Power & Energy
  • Technologies
  • More
Power & Energy
Forum You might not want to monitor your electricity, but I do! Help?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 283 subscribers
  • Views 1785 views
  • Users 0 members are here
  • internet of things
  • raspberry pi
  • iot
  • power usage
  • energy efficiency
  • electricity monitoring
  • arduino
Related

You might not want to monitor your electricity, but I do! Help?

cstanton
cstanton over 10 years ago

Last month I asked people over Twitter and on the element14 Community how you monitored your electrical usage. I was surprised to discover that a lot of people, don't. I'm not to be dissuaded when there's statistics to be had, especially when it's something close to home (oh dear, I'm resorting to puns).

 

So I have one of these electricity monitors:

 

image

 

That my electric provider gave me, turns out they're really common, except I'm having a hard time determining how to get data out of it. You see, there's an RJ45 socket on the underside of it, which it turns out, dumps serial, but I cannot discover an authoritative answer on its pinout, though it turns out there are cables you can buy that're 'pre-made' for this, apparently it's also 3v3 logic. I decided to make my own:

 

image

 

Part one of my troubles is, how do I work out the correct pinout? Admittedly I am a novice when it comes to using oscilloscopes (and they're too high priced for my tastes) so what's a safe hack-ey way I can go about this? (the USB device in the pic' happens to be a UART type device which usefully has pins on it).

 

Part two of my troubles, is how shall I handle the data it outputs? About every second, it apparently dumps out XML over serial. Something like this:

 

<msg>                            start of message

   <src>CC128-v0.11</src>        source and software version

   <dsb>00089</dsb>              days since birth, ie days run

   <time>13:02:39</time>         24 hour clock time as displayed

   <tmpr>18.7</tmpr>             temperature as displayed

   <sensor>1</sensor>            Appliance Number as displayed

   <id>01234</id>                radio ID received from the sensor

   <type>1</type>                sensor Type, "1" = electricity

   <ch1>                         sensor channel

      <watts>00345</watts>       data and units

   </ch1>

   <ch2>

      <watts>02151</watts>

   </ch2>

   <ch3>

      <watts>00000</watts>

   </ch3>

</msg>                           end of message

 

I thought that perhaps I should connect it to an ArduinoArduino, or perhaps a Raspberry PiRaspberry Pi? I will need a way to do the following:

 

  • Receive the data and ensure it is legible
  • Store the data so that we can use it
  • Ensure the data is stored at an accurate or relevant timestamp (apparently the device just counts from when it was turned on)
  • Convert the values it gives to something that makes sense
  • Present the values that its stored in ways that are useful and relevant to cost
    • Such as graphs over time

 

The way I see this being useful, is to correlate the electricity usage with house temperature, external house temperature, and maybe further down the line link in my central heating system, so I'm creating almost a house profile, or prevent something turning on when electricity usage is high (for example, electricity is of course used when the boiler kicks in for the water pump, but I'm getting ahead of myself).

 

With all this in mind, does this change anyone else's mind about monitoring their electrical usage? Or perhaps someone can give me advice on where to begin with either part of this project? Or should I construct an electricity monitor out of something else entirely?

 

Thanks for reading!

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 10 years ago in reply to shabaz +2
    9600 baud? No, that doesn't seem it.. 1200 baud? Hmm, not there yet! 2400 baud? Hello data! Looks like the pin-out is correct after all. <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>22</sec…
  • mcb1
    mcb1 over 10 years ago in reply to shabaz +1
    I looked at it a while back, and after multiple revisions it seemed an odd design choice to still use an ATmega and its single built-in 10-bit ADC I didn't look too hard into the actual hardware side,…
  • shabaz
    shabaz over 10 years ago in reply to mcb1 +1
    Agree, it is easy to become OCD and want super-high granularity when in reality you might actually only be interested at the power-hungry stuff.
Parents
  • mcb1
    mcb1 over 10 years ago

    Christopher

    Rather than re-invent the wheel I'd be looking at these guys.

    https://openenergymonitor.org/emon/

     

    I'm aware of a few guys here that have solar and used their monitoring to 'moduate' their hot water cylinder, rather than supply electricity at a very low return.

    I posted a picture of one of their projects here

    Forget Me Not :  eLDERmon  Electrical

    I also pointed out that they nearkly had it right in terms of meeting electrical safety along with a few others that didn't meet anything like safety.

     

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 10 years ago

    Christopher

    Rather than re-invent the wheel I'd be looking at these guys.

    https://openenergymonitor.org/emon/

     

    I'm aware of a few guys here that have solar and used their monitoring to 'moduate' their hot water cylinder, rather than supply electricity at a very low return.

    I posted a picture of one of their projects here

    Forget Me Not :  eLDERmon  Electrical

    I also pointed out that they nearkly had it right in terms of meeting electrical safety along with a few others that didn't meet anything like safety.

     

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 10 years ago in reply to mcb1

    Hi Mark,

     

    The hardware for that project is unusual, although some of their software may be reusable. I looked at it a while back, and after multiple revisions it seemed an odd design choice to still use an ATmega and its single built-in 10-bit ADC (they themselves acknowledge the implications of this here https://openenergymonitor.org/emon/buildingblocks/measurement-implications-of-adc-resolution-at-low-current-values  and here: https://openenergymonitor.org/emon/emontx/accuracy  ), when instead there are 24-bit simultaneous-sampling dedicated energy meter ICs which are low cost, and do all the calculations according to the same standards that should be used by all energy meters (as I understand). The other interesting thing is that their accuracy page ( https://openenergymonitor.org/emon/emontx/accuracy   ) used a mainly resistive load (a 20W, and 60W lamp) so the actual error could be far worse yet they didn't address this.

    I've no idea about the one that Christopher's got, but it is likely to be far higher granularity and accuracy. I guess if the openenergymonitor design is lower-cost it might be worthwhile as a rough indicator (they do share the hardware across 4 circuits so that would reduce cost a bit).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to shabaz

    I looked at it a while back, and after multiple revisions it seemed an odd design choice to still use an ATmega and its single built-in 10-bit ADC

    I didn't look too hard into the actual hardware side, as there were various other projects based on the work.

     

    Yes you can worry about the exact measurement of voltage and current but in reality you are looking to have some control over the energy hungry devices, not individual lamps.

    If you do require that sort of resolution then there are hardware alternatives as you say.

     

    I thought the software side might have some useful pieces.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to mcb1

    Agree, it is easy to become OCD and want super-high granularity when in reality you might actually only be interested at the power-hungry stuff.