Power & Energy
  • Technologies
  • More
Power & Energy
Forum You might not want to monitor your electricity, but I do! Help?
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 283 subscribers
  • Views 1788 views
  • Users 0 members are here
  • internet of things
  • raspberry pi
  • iot
  • power usage
  • energy efficiency
  • electricity monitoring
  • arduino
Related

You might not want to monitor your electricity, but I do! Help?

cstanton
cstanton over 10 years ago

Last month I asked people over Twitter and on the element14 Community how you monitored your electrical usage. I was surprised to discover that a lot of people, don't. I'm not to be dissuaded when there's statistics to be had, especially when it's something close to home (oh dear, I'm resorting to puns).

 

So I have one of these electricity monitors:

 

image

 

That my electric provider gave me, turns out they're really common, except I'm having a hard time determining how to get data out of it. You see, there's an RJ45 socket on the underside of it, which it turns out, dumps serial, but I cannot discover an authoritative answer on its pinout, though it turns out there are cables you can buy that're 'pre-made' for this, apparently it's also 3v3 logic. I decided to make my own:

 

image

 

Part one of my troubles is, how do I work out the correct pinout? Admittedly I am a novice when it comes to using oscilloscopes (and they're too high priced for my tastes) so what's a safe hack-ey way I can go about this? (the USB device in the pic' happens to be a UART type device which usefully has pins on it).

 

Part two of my troubles, is how shall I handle the data it outputs? About every second, it apparently dumps out XML over serial. Something like this:

 

<msg>                            start of message

   <src>CC128-v0.11</src>        source and software version

   <dsb>00089</dsb>              days since birth, ie days run

   <time>13:02:39</time>         24 hour clock time as displayed

   <tmpr>18.7</tmpr>             temperature as displayed

   <sensor>1</sensor>            Appliance Number as displayed

   <id>01234</id>                radio ID received from the sensor

   <type>1</type>                sensor Type, "1" = electricity

   <ch1>                         sensor channel

      <watts>00345</watts>       data and units

   </ch1>

   <ch2>

      <watts>02151</watts>

   </ch2>

   <ch3>

      <watts>00000</watts>

   </ch3>

</msg>                           end of message

 

I thought that perhaps I should connect it to an ArduinoArduino, or perhaps a Raspberry PiRaspberry Pi? I will need a way to do the following:

 

  • Receive the data and ensure it is legible
  • Store the data so that we can use it
  • Ensure the data is stored at an accurate or relevant timestamp (apparently the device just counts from when it was turned on)
  • Convert the values it gives to something that makes sense
  • Present the values that its stored in ways that are useful and relevant to cost
    • Such as graphs over time

 

The way I see this being useful, is to correlate the electricity usage with house temperature, external house temperature, and maybe further down the line link in my central heating system, so I'm creating almost a house profile, or prevent something turning on when electricity usage is high (for example, electricity is of course used when the boiler kicks in for the water pump, but I'm getting ahead of myself).

 

With all this in mind, does this change anyone else's mind about monitoring their electrical usage? Or perhaps someone can give me advice on where to begin with either part of this project? Or should I construct an electricity monitor out of something else entirely?

 

Thanks for reading!

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 10 years ago in reply to shabaz +2
    9600 baud? No, that doesn't seem it.. 1200 baud? Hmm, not there yet! 2400 baud? Hello data! Looks like the pin-out is correct after all. <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>22</sec…
  • mcb1
    mcb1 over 10 years ago in reply to shabaz +1
    I looked at it a while back, and after multiple revisions it seemed an odd design choice to still use an ATmega and its single built-in 10-bit ADC I didn't look too hard into the actual hardware side,…
  • shabaz
    shabaz over 10 years ago in reply to mcb1 +1
    Agree, it is easy to become OCD and want super-high granularity when in reality you might actually only be interested at the power-hungry stuff.
Parents
  • shabaz
    shabaz over 10 years ago

    Hi Christopher,

     

    Interesting project. If the unit autonomously dumps data every second, then perhaps just the TX output from the unit is needed, and not the RX, so if you had a USB-UART adapter then you could probe with the USB-UART-RX input line only, until you saw data on the terminal window.

     

    According to that link however it sounds like pin 8 is the one that will be outputting from the unit.

    I think this arrangement might work, but I'm not sure since I'm just basing it on that thread : ( :

    image

    Not that I like recommending FTDI parts : ) but it might be quickest to use that one since it is designed for 3.3V logic levels.  I'm designing a USB UART mini project here 5V UARTs on SBCs?   , maybe you might want to swap some day : )

    [EDIT: oh, just noticed you already have a USB UART. That is fine since it is 3.3V too.].

     

    Regarding software, there are a few challenges, firstly (regardless of programming language) the input needs to be read, but to also know when the entire information has been captured. One method is to set a timeout so if you have no more bytes to read for a certain amount of time then the read function exits and you can start parsing the data. If you're using C then this should be straightforward, there is the 'termios' option value VTIME that can be set appropriately (e.g. to 5 tenths of a second), and probably other languages offer the same thing since their libraries use the same underlying capabilities.

    As an example, there is some code here https://github.com/shabaz123/u1282a_fastlog/blob/master/fastlog.c   , it basically reads from a USB UART too and line 321 of the code is setting to 5 tenths of a second.

    Python will have the same thing I'm sure. There is also the 'expect' library (i.e. libexpect) but that feels like overkill.

    The next challenge is to parse the content, which really depends on how regular the structure is. I quite like just using the standard C++ string library for that, although some would say that is like bringing a knife to a gunfight. But equally there are libraries specifically to parse XML but that might be overkill since there isn't much to be parsed by the looks of it. So perhaps usual string find functions are ok to use, and (say) sscanf for reading in the values into floating point variables.

    Regarding what to do with the data, you could push to a cloud (I don't have any recommendation however) say every 5 minutes or (or simultaneously) plot it in real-time to the display. There is an example here, which uses 'kst': Raspberry Pi 3 Dynamic Current Consumption, Power and Temperature Tests

    To do that, I just got the program to dump data regularly to a file, and then 'kst' would read it every second. Maybe there is no need to worry about file size for about a month, and then possibly save it off (e.g. give it a filename with a timestamp). Or put it into a database, but the basic CSV file method isn't bad, easier too. It would be nice to have some analysis as part of the app though, e.g. the stats for the month, and the same month the previous year, etc. However that is all accoutrements, i.e. phase 2 type stuff maybe.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 10 years ago in reply to shabaz

    9600 baud?

    image

     

    No, that doesn't seem it..

     

    1200 baud?

    image

     

    Hmm, not there yet!

     

    2400 baud?

    image

     

    Hello data! Looks like the pin-out is correct after all.

     

     

    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>22</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00651</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>28</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>34</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>41</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00646</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>47</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>53</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>59</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>05</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00590</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>17</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00592</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>23</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00597</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>29</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>35</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>41</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00622</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>47</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00581</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>53</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>59</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>05</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00601</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00642</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00630</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00590</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>48</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>54</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00625</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00604</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00646</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00578</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>47</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00584</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00592</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00587</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00578</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00583</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00596</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>48</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>54</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00610</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00600</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00614</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00648</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>48</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00583</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>54</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00636</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00602</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00648</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>43</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00651</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>49</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>55</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00605</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>01</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00596</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>07</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>19</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00584</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>31</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00584</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>37</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00583</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>43</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>49</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>55</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>01</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00602</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>07</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00622</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00615</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>19</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00635</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>31</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>44</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>02</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00599</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00667</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>32</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00650</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>37</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>44</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>56</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00640</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00634</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00710</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00619</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>31</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>37</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00592</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>43</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00604</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>49</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>55</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00624</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>07</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>14</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00598</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00609</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>26</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00620</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>32</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00625</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>44</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00590</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00604</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>56</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00609</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00608</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>14</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00595</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00607</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>27</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00613</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>33</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00616</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>45</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00630</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>51</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>57</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00606</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>02</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>14</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00595</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>26</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>32</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00579</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00581</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>45</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00579</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00606</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>57</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00605</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>

     

    It dumps data every 5 seconds by the look of it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cstanton
    cstanton over 10 years ago in reply to shabaz

    9600 baud?

    image

     

    No, that doesn't seem it..

     

    1200 baud?

    image

     

    Hmm, not there yet!

     

    2400 baud?

    image

     

    Hello data! Looks like the pin-out is correct after all.

     

     

    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>22</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00651</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>28</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>34</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>41</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00646</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>47</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>53</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>53</min><sec>59</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>05</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00590</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>17</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00592</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>23</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00597</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.6</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>29</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>35</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>41</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00622</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>47</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00581</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>53</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>54</min><sec>59</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>05</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00601</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00642</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00630</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00590</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>48</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>55</min><sec>54</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00625</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00604</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00646</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00578</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>56</min><sec>47</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00584</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00592</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00587</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00578</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00583</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00596</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>48</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>57</min><sec>54</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00610</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00600</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00614</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00648</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>42</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>48</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00583</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>58</min><sec>54</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00636</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>00</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>06</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00602</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>12</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>18</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00648</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>24</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>30</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>36</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>43</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00651</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>49</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>22</hr><min>59</min><sec>55</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00605</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>01</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00596</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>07</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>19</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00584</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>31</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00584</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>37</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00583</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>43</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>49</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>00</min><sec>55</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00591</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>01</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00602</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>07</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00622</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00615</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>19</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00635</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00582</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>31</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>44</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>01</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>02</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00599</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00667</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>32</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00650</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>37</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>44</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.7</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>02</min><sec>56</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00640</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00634</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>13</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00710</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>25</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00619</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>31</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>37</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00592</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>43</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00604</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>49</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>03</min><sec>55</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00624</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>07</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00589</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>14</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00598</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00609</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>26</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00620</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>32</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00625</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00611</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>44</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00590</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00604</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>04</min><sec>56</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00609</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00608</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>14</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00595</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00607</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>27</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00613</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>33</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00616</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>45</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00630</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>51</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00593</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>05</min><sec>57</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00606</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>02</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00588</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>08</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>14</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00586</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>20</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00595</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>26</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00585</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>32</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00579</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>38</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00581</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>45</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00579</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>50</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00606</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>
    <msg><date><dsb>01343</dsb><hr>23</hr><min>06</min><sec>57</sec></date><src><name>CC02</name><id>01191</id><type>1</type></src><ch1><watts>00605</watts></ch1><ch2><watts>00000</watts></ch2><ch3><watts>00000</watts></ch3><tmpr>20.8</tmpr></msg>

     

    It dumps data every 5 seconds by the look of it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 10 years ago in reply to cstanton

    Oh Awesome!!