Power & Energy
  • Technologies
  • More
Power & Energy
Forum Charging two 18650 batteries with one TP4056 module
  • Blog
  • Forum
  • Quiz
  • Documents
  • Polls
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 283 subscribers
  • Views 16379 views
  • Users 0 members are here
Related

Charging two 18650 batteries with one TP4056 module

yukardo
yukardo over 7 years ago

Hello,

 

I want to know if it is possible to charge two 3.7 V 18650 batteries with one TP4056 module.

 

The batteries would be connected in parallel.

 

I hope you can help me.

 

Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 7 years ago +4
    You can, as paralleled cells behave like one larger cell. Charge time will be longer, accordingly. Just be sure the cells you are paralleling are of the same make/model/capacity/state of charge/age and…
  • afmishaq
    afmishaq over 7 years ago in reply to Gough Lui +1
    " ... the same make/model/capacity/state of charge/age ..", is required, otherwise a damage to cell or charger or both may result. I would not take a chance considering that the TP4056 module is a small…
  • michaelkellett
    michaelkellett over 7 years ago +1
    Obviously you are doing this to get more battery capacity. What is the battery capacity you are aiming for ? MK
Parents
  • station240
    station240 over 7 years ago

    There is also a TP5000 module which charges at 2A, slightly more expensive but more efficient.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • station240
    station240 over 7 years ago

    There is also a TP5000 module which charges at 2A, slightly more expensive but more efficient.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Pavel.Simon
    Pavel.Simon over 7 years ago in reply to station240

    Very good description of TP5000 could be find there: Test/Review of Charger 1.5A 3.6-4.2V (TP5000)