Robotics
  • Technologies
  • More
Robotics
Forum Hi there,can we can just discuss about low cost solutions for generating 4-20 ma current?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 79 subscribers
  • Views 1709 views
  • Users 0 members are here
  • transducers
  • 4-20
  • plc_control
Related

Hi there,can we can just discuss about low cost solutions for generating 4-20 ma current?

coolbox
coolbox over 11 years ago

Hi there,

 

4-20 ma is standard for data acquisition from sensors in industrial environment.There are are many techniques like PWM and DAC for 4-20 ma current generation.But still i want to hear from automation experts for options about generating 4-20 ma.Is any micro controller which can directly output 4-20ma?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to johnbeetem +1
    The nice thing is it can detect outages as 0 reading is not 0 current, it is 4mA (Just enough to drive the remote sensor and nowadays a micro, ADC, DAC etc) and as it is a current system, can tolerate…
Parents
  • coolbox
    coolbox over 11 years ago

    measurement-converter-programmable-69147-2498663.jpg

     

    Dear peter,

     

    I am a firmware developer and i have not seen transducers in working environment.but I want to make my doubts clear.

    In above image you can see that 0 to 10 kv reprented by 0 to 20 mA.

     

    parth pandya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to coolbox

    I did say there are always exceptions and also that the sensor would have to be powered by other means, all the sensors I have worked with for British Gas where loop powered and hence there could not be a zero current. I did not say it did not exist. but I am glad your on top of it, it has been quite a few years and I am sure there are many advances since I was in the field (Literally image). Also my experience is based on the gas industry, looking at that DIN Rail mount module I would guess your in the Power industry, it looks to be some kind of power meter / remote sensor (I have not looked up the part, just guessing image )

     

    btw, TI has a number of chips designed to work directly with 4-20mA (or 0-20mA ) loops, you should check them out, but you can also create the loop driver with not much more than an op amp or two and a few other components

     

    I also found this, it may be of interest: http://forum.arduino.cc/index.php?topic=134213.0

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to coolbox

    I did say there are always exceptions and also that the sensor would have to be powered by other means, all the sensors I have worked with for British Gas where loop powered and hence there could not be a zero current. I did not say it did not exist. but I am glad your on top of it, it has been quite a few years and I am sure there are many advances since I was in the field (Literally image). Also my experience is based on the gas industry, looking at that DIN Rail mount module I would guess your in the Power industry, it looks to be some kind of power meter / remote sensor (I have not looked up the part, just guessing image )

     

    btw, TI has a number of chips designed to work directly with 4-20mA (or 0-20mA ) loops, you should check them out, but you can also create the loop driver with not much more than an op amp or two and a few other components

     

    I also found this, it may be of interest: http://forum.arduino.cc/index.php?topic=134213.0

     

    Peter