Robotics
  • Technologies
  • More
Robotics
Forum Hi there,can we can just discuss about low cost solutions for generating 4-20 ma current?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 79 subscribers
  • Views 1713 views
  • Users 0 members are here
  • transducers
  • 4-20
  • plc_control
Related

Hi there,can we can just discuss about low cost solutions for generating 4-20 ma current?

coolbox
coolbox over 11 years ago

Hi there,

 

4-20 ma is standard for data acquisition from sensors in industrial environment.There are are many techniques like PWM and DAC for 4-20 ma current generation.But still i want to hear from automation experts for options about generating 4-20 ma.Is any micro controller which can directly output 4-20ma?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to johnbeetem +1
    The nice thing is it can detect outages as 0 reading is not 0 current, it is 4mA (Just enough to drive the remote sensor and nowadays a micro, ADC, DAC etc) and as it is a current system, can tolerate…
Parents
  • coolbox
    coolbox over 11 years ago

    measurement-converter-programmable-69147-2498663.jpg

     

    Dear peter,

     

    I am a firmware developer and i have not seen transducers in working environment.but I want to make my doubts clear.

    In above image you can see that 0 to 10 kv reprented by 0 to 20 mA.

     

    parth pandya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • coolbox
    coolbox over 11 years ago

    measurement-converter-programmable-69147-2498663.jpg

     

    Dear peter,

     

    I am a firmware developer and i have not seen transducers in working environment.but I want to make my doubts clear.

    In above image you can see that 0 to 10 kv reprented by 0 to 20 mA.

     

    parth pandya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to coolbox

    I did say there are always exceptions and also that the sensor would have to be powered by other means, all the sensors I have worked with for British Gas where loop powered and hence there could not be a zero current. I did not say it did not exist. but I am glad your on top of it, it has been quite a few years and I am sure there are many advances since I was in the field (Literally image). Also my experience is based on the gas industry, looking at that DIN Rail mount module I would guess your in the Power industry, it looks to be some kind of power meter / remote sensor (I have not looked up the part, just guessing image )

     

    btw, TI has a number of chips designed to work directly with 4-20mA (or 0-20mA ) loops, you should check them out, but you can also create the loop driver with not much more than an op amp or two and a few other components

     

    I also found this, it may be of interest: http://forum.arduino.cc/index.php?topic=134213.0

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to coolbox

    The device in your picture has multiple outputs - the 0 - 20mA output is quite different from and not compatible with the industry standard 4-20mA signalling. In 4-20 4mA is zero and 20mA is full scale - since the transmitting device expects to draw power from the loop the current can never drop to zero.

    The CEWE device in your picture needs power from another source to work.

     

    Are you trying to design a transmitting device ?

     

    MK