Robotics
  • Technologies
  • More
Robotics
Forum Hi there,can we can just discuss about low cost solutions for generating 4-20 ma current?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Robotics to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 79 subscribers
  • Views 1715 views
  • Users 0 members are here
  • transducers
  • 4-20
  • plc_control
Related

Hi there,can we can just discuss about low cost solutions for generating 4-20 ma current?

coolbox
coolbox over 11 years ago

Hi there,

 

4-20 ma is standard for data acquisition from sensors in industrial environment.There are are many techniques like PWM and DAC for 4-20 ma current generation.But still i want to hear from automation experts for options about generating 4-20 ma.Is any micro controller which can directly output 4-20ma?

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to johnbeetem +1
    The nice thing is it can detect outages as 0 reading is not 0 current, it is 4mA (Just enough to drive the remote sensor and nowadays a micro, ADC, DAC etc) and as it is a current system, can tolerate…
Parents
  • coolbox
    coolbox over 11 years ago

    measurement-converter-programmable-69147-2498663.jpg

     

    Dear peter,

     

    I am a firmware developer and i have not seen transducers in working environment.but I want to make my doubts clear.

    In above image you can see that 0 to 10 kv reprented by 0 to 20 mA.

     

    parth pandya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to coolbox

    The device in your picture has multiple outputs - the 0 - 20mA output is quite different from and not compatible with the industry standard 4-20mA signalling. In 4-20 4mA is zero and 20mA is full scale - since the transmitting device expects to draw power from the loop the current can never drop to zero.

    The CEWE device in your picture needs power from another source to work.

     

    Are you trying to design a transmitting device ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 11 years ago in reply to coolbox

    The device in your picture has multiple outputs - the 0 - 20mA output is quite different from and not compatible with the industry standard 4-20mA signalling. In 4-20 4mA is zero and 20mA is full scale - since the transmitting device expects to draw power from the loop the current can never drop to zero.

    The CEWE device in your picture needs power from another source to work.

     

    Are you trying to design a transmitting device ?

     

    MK