University of Southern California researchers stimulated a blind rat’s eye with ultrasound waves to provide visualizations. (Image Credit: University of Southern California)
$44 billion for Twitter, barely anything for what really matters in ...
H2L’s armband applies electrical shocks to the wearer’s arm whenever they experience sensations in the metaverse. (Image Credit: H2L Technologies)
The metaverse is about to get a whole lot more realistic, on its way to replacing the real...
Hello everyone, this is my first time posting in the forum.
So i am working with thunderboard sense 2 and simplicty studio. I want to use an external PIR sensor connected to the board to get PIR data in my PC. As in read the analog PIN and valu...
The James Webb Telescope captured this stunning image of a Milky Way star, 2MASS J17554042+6551277, along with distant galaxies in the background. (Image Credit: NASA/STScl)
On March 16th, the James Webb Telescope transmitted its most detailed image...
A recent study revealed that mushrooms could potentially communicate with each other via electrical signals. (Image Credit: Hans Veth/Unsplash)
Mushrooms may possess complex communication capabilities. A recent study conducted by Andrew Ad...
Scientists associated with the Exploring the Great Pyramid mission plan to use advanced detectors to map the pyramid. (Image Credit: Jeremy Bezanger/Unsplash)
Scientists affiliated with the Exploring the Great Pyramid (EGP) project announced&nb...
The acoustic fiber, woven into the fabric, converts sound vibrations into electrical signals for sound detection capabilities. (Image Credit: Greg Hren/MIT)
MIT engineers developed a flexible piezoelectric fabric microphone, which picks up and ...
Stretching the display in one direction causes an equal stretch distribution on the other side, which prevents image distortion. (Image Credit: Korea Institute of Machinery and Materials (KIMM))
Researchers at the Korea Institute of Machinery and Ma...
Researchers discover that spiders rely on the electric field in the Earth’s atmosphere to provide lift. (Image Credit: Vidar Nordli-Mathisen/Unsplash)
While completely wingless, some spider species evolved to take flight using nothing but thei...
The image shows solar panels that supply power to the electronics. (Image Credit: Mark Stone/University of Washington)
University of Washington researchers recently built a sensor-carrying device that rides the wind to travel while falling. Overall,...
Astronauts installed the ICARUS system on the International Space Station. (Image Credit: ESA/NASA/AstroSerena)
Bio-logging, also known as wildlife monitoring, has been around for a while and recently made some significant advancements. Back in the ...
LunAero observes migrating birds as they pass in front of the moon. (Image Credit: University of Oklahoma)
For centuries, scientists have been perplexed by birds and what they may be doing during the night. Some even theorized that birds would go un...
The image shows a Weddell seal with a conductive, temperature, and depth sensor attached to its head. (Image Credit: Nobuo Kokubun (NIPR))
Like living robots. Every hear of the "Internet of Animals?"
It may seem bizarre at first,...
The team used a vinyl cutter to create a stretchable smart mesh, which can be used for sweat sensing applications. (Image Credit: Peisheng He/UC Berkeley))
UC Berkley engineers devised a new technique that allows medical researchers to test new wear...
Graphical representation of the sensor and the color changes in response to heat. (Image Credit: DOI: 10.1109/JSEN.2021.3135941)
Liverpool Hope University researchers developed the first robotic sensor capable of imitating a human's response to ...
Professor Yael Hanein of the Tel Aviv University (Image credit: TEL AVIV UNIVERSITY)
Researchers at Tel Aviv University in Israel developed a new lie detector test that could eventually substitute the ones commonly used today. This system uses a per...
Australian researchers implanted bionic eyes in sheep to determine if it helps improve their vision. (Image Credit: Skitterphoto/pixabay)
Australian researchers managed to improve sheep's vision by implanting bionic eyes, called Phoenix 99, behi...
The biohybrid fish, inspired by the zebrafish, can improve its swimming motion over time. (Image Credit: Michael Rosnach, Keel Yong Lee, Sung-Jin Park, Kevin Kit Parker)
Harvard University and Emory University researchers recently developed an auton...
The team recreated surface waves found on insects by stretching the material at a right angle. (Image Credit: Imperial College London)
The whole world covered in this?
Imperial College London researchers developed materials with complex patterns tha...
The implant system uses flat electrodes positioned between the spinal nerves and vertebrae to send electrical signals to the spine to perform selected actions, such as taking steps or kicking. (Image credit: EPFL via Nature)
Scientists from t...
The system uses the Pi, an H-field probe and an o-scope to detect electromagnetic wave signatures from multiple virus types. (Image credit: Institute of Computer Science and Random Systems)
Researchers from the Institute of Computer Science and Rand...
Cows could wear VR headsets to help reduce anxiety during the winter, leading to a larger milk yield. (Image Credit: Monika Kubala/Unsplash)
Cows are living in the matrix for real. It’s sad, in a way. But it seems the cows are happy.
This may ...
I was Road Testing the Rohm SensorShield-EVK-003 (Arduino Compatible) and the sensors that come with it, in 2017.One of the sensors that I hadn't reviewed during the test, is the BH1790GLC Heart Rate Monitor.I'm going to use tha...