Sensors
  • Technologies
  • More
Sensors
Sensor Forum Temperature sensor to measure surface temperature compatible with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 350 subscribers
  • Views 4238 views
  • Users 0 members are here
  • temp sensor
Related

Temperature sensor to measure surface temperature compatible with Raspberry Pi

kas.lewis
kas.lewis over 9 years ago

Hello All,

 

I am looking for a temperature sensor that I can use to monitor the temperature of a surface with a raspberry pi. With no A/D on board the choices seem limited added to this is the need to find something that I can connect to a surface easily is not helping. Any ideas or suggestions would be greatly appreciated.

 

I was thinking of using a thermopile facing the surface but I cant seem to finf one that as a simple to use output (unclear data sheets aren't helping)

 

Thanks

Kas

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +2 suggested
    Hi Kas, bwelsby and I did some fairly extensive (at the time) tests on the Pi 3, we used a thermistor and also examined the in-built measurement. The information is dotted in multiple posts and comments…
  • shabaz
    shabaz over 9 years ago +2 suggested
    Just re-reading, I may have misunderstood your requirement. If you're measuring the temperature of a different surface (i.e. not the Pi) then similar comments may apply, or you may need a different method…
  • shabaz
    shabaz over 9 years ago in reply to kas.lewis +2 suggested
    Hi Kas, For low thermal mass perhaps a very small SMD sized silicon sensor, or a thermocouple or thermistor or RTD as you say with small size. If you want to use on of the latter devices, then you'll need…
Parents
  • dougw
    0 dougw over 9 years ago

    There are many I2C sensors that could be used:

    TMP102

    MCP9808

    Si705x

     

    or spi sensors

    LM74

    MAX6662

    DS1722

    TC77

     

    etc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 9 years ago in reply to dougw

    Thank you for the information, Those are all great suggestions but I was hoping for a more complete solution especially for surface sensing. Something that has low thermal mass. But I think your suggestions have put me back on track and let me see that high cost/complete solution may not be needed.

     

    Kas

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kas.lewis
    0 kas.lewis over 9 years ago in reply to dougw

    Thank you for the information, Those are all great suggestions but I was hoping for a more complete solution especially for surface sensing. Something that has low thermal mass. But I think your suggestions have put me back on track and let me see that high cost/complete solution may not be needed.

     

    Kas

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 9 years ago in reply to kas.lewis

    Hi Kas,

     

    For low thermal mass perhaps a very small SMD sized silicon sensor, or a thermocouple or thermistor or RTD as you say with small size. If you want to use on of the latter devices, then you'll need an ADC, and you could use the same ADC as in the project mentioned earlier, since they are available on a PCB at low cost from ebay, it is the ADS1118. Here is an example one: ADS1118 16-bit AD Converter ADC SPI Communication Module Development Board | eBay

    RTDs are available as small flat devices, so could be taped onto a wall for example. Another approach could be non-contact IR thermal sensing.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer