Sensors
  • Technologies
  • More
Sensors
Sensor Forum Temperature sensor to measure surface temperature compatible with Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Sensors to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 350 subscribers
  • Views 4234 views
  • Users 0 members are here
  • temp sensor
Related

Temperature sensor to measure surface temperature compatible with Raspberry Pi

kas.lewis
kas.lewis over 9 years ago

Hello All,

 

I am looking for a temperature sensor that I can use to monitor the temperature of a surface with a raspberry pi. With no A/D on board the choices seem limited added to this is the need to find something that I can connect to a surface easily is not helping. Any ideas or suggestions would be greatly appreciated.

 

I was thinking of using a thermopile facing the surface but I cant seem to finf one that as a simple to use output (unclear data sheets aren't helping)

 

Thanks

Kas

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +2 suggested
    Hi Kas, bwelsby and I did some fairly extensive (at the time) tests on the Pi 3, we used a thermistor and also examined the in-built measurement. The information is dotted in multiple posts and comments…
  • shabaz
    shabaz over 9 years ago +2 suggested
    Just re-reading, I may have misunderstood your requirement. If you're measuring the temperature of a different surface (i.e. not the Pi) then similar comments may apply, or you may need a different method…
  • shabaz
    shabaz over 9 years ago in reply to kas.lewis +2 suggested
    Hi Kas, For low thermal mass perhaps a very small SMD sized silicon sensor, or a thermocouple or thermistor or RTD as you say with small size. If you want to use on of the latter devices, then you'll need…
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Kas,

     

    bwelsby and I did some fairly extensive (at the time) tests on the Pi 3, we used a thermistor and also examined the in-built measurement.

    The information is dotted in multiple posts and comments though:

    See here Raspberry Pi 3 Dynamic Current Consumption, Power and Temperature Tests

    and Raspberry Pi temperature and cooling testing Part 1 initial tests.

    Raspberry Pi 3 temperature and cooling testing Part 2 with a HAT tests.

    Raspberry Pi 3 Cooling / Heat Sink Ideas

     

    As you say, there is no ADC so that makes it a bit awkward. An option is to attach one (SPI or I2C for example) or use a multimeter and pen/paper, if you're capturing data over slower periods. The thermistor was a bead, so I drilled a hole for it (in heatsink).

    An alternative could be an RTD device (e.g. PT100), they are also tiny and some have a flat surface, so you could tape it onto the chip.

    You could use a larger semiconductor device (e.g. TO-92 package) but they have a slow thermal response.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago

    Hi Kas,

     

    bwelsby and I did some fairly extensive (at the time) tests on the Pi 3, we used a thermistor and also examined the in-built measurement.

    The information is dotted in multiple posts and comments though:

    See here Raspberry Pi 3 Dynamic Current Consumption, Power and Temperature Tests

    and Raspberry Pi temperature and cooling testing Part 1 initial tests.

    Raspberry Pi 3 temperature and cooling testing Part 2 with a HAT tests.

    Raspberry Pi 3 Cooling / Heat Sink Ideas

     

    As you say, there is no ADC so that makes it a bit awkward. An option is to attach one (SPI or I2C for example) or use a multimeter and pen/paper, if you're capturing data over slower periods. The thermistor was a bead, so I drilled a hole for it (in heatsink).

    An alternative could be an RTD device (e.g. PT100), they are also tiny and some have a flat surface, so you could tape it onto the chip.

    You could use a larger semiconductor device (e.g. TO-92 package) but they have a slow thermal response.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer