Test & Tools
  • Technologies
  • More
Test & Tools
Blog Agilent Wireless Remote Connectivity
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 11 Jul 2013 5:11 PM Date Created
  • Views 1219 views
  • Likes 1 like
  • Comments 3 comments
  • android
  • bluetooth
  • ir_port
  • sensors_and_controls
  • google_play_store
  • handheld_multimeter
  • car
  • wireless_communication
  • thermocouple
  • probes
  • data_logger
  • measurement
  • automotive
  • data_logging
  • wireless_remote_connectivity
  • error_code
  • agilent
  • diagnostics
Related
Recommended

Agilent Wireless Remote Connectivity

e14 Contributor
e14 Contributor
11 Jul 2013

image

Today’s vehicles, whether a concept car or your commuter, are choke full of sensors and controls.  In the idealized world of the car designers these sensors and controls totally and completely monitor and control all the functions of the vehicle at all times.  Any problem will be reported in error codes.  Their subsequent remedies are detailed in service procedures.  Still for designer or servicer alike, sometimes these sensor inputs need to be verified.  One may want to have an actual temperature measurement, or a sensor voltage reading independent of the diagnostic system. 

 

One of Agilent’s customers, Tracy, is a design engineer for automotive sensors and controls systems.  He helps us understand some of the challenges working with a vehicle platform.  In particular, there is a hard divide between the engine and the passenger compartment.  There are no port holes or service doors.  There is no easy way to run test leads, wires or thermocouples from the engine to the driver, so that he can see how the temperature or voltage behaves as the vehicle is driven through different conditions.

 

image

[Caption:  a thermocouple, blue wire, inside the engine compartment.  In an actual measurement, the wire will terminate inside the airbox, for  example, and not be visible to the camera.]

 

 

image

 

[Caption:  a connector where voltage measurement can be taken with test leads, or back probe pins.]

 

 

Using the Agilent WRC (wireless remote connectivity) meter, Tracy now can access the measurements inside the passenger compartment wirelessly.  It is simple and painless.  The thermocouple or test leads are connected to an Agilent handheld multimeter, which is secured inside the engine compartment with the hood closed.  The measurement results are transmitted via a Bluetooth adaptor to an Android tablet (or phone) inside the passenger compartment.  The Android app is free from Agilent or Google Play Store.  It takes only a few clicks to get going, much easier than any other alternatives.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    Just curious, has anyone considered using the bluetooth connection to collect measurements and then do a voice output on the smart phone?

     

    I sometimes set up experiments where I need to monitor several measurements or a period of time and I need periodic updates without moving away from other instruments.  I am sure it would be an easy app to make and I suspect that others would have a need for the capabililty.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 13 years ago

    Just curious, has anyone considered using the bluetooth connection to collect measurements and then do a voice output on the smart phone?

     

    I sometimes set up experiments where I need to monitor several measurements or a period of time and I need periodic updates without moving away from other instruments.  I am sure it would be an easy app to make and I suspect that others would have a need for the capabililty.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • sqkybeaver
    sqkybeaver over 13 years ago in reply to DAB

    Just curious, has anyone considered using the bluetooth connection to collect measurements and then do a voice output on the smart phone?

     

     

                       

     

     

                        I can say the blue tooth adaptor works well, and would also like the ability to have my phone or tablet to "talk" to me. perhaps using the trigger on a preset low or high reading to get a verbal warning. this would be great when working on a complicated assembly line machine while opperating it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to sqkybeaver

    The latest version of the Agilent Mobile apps has voice out features, using the resident smart phone or tablet voice out software.  If you use the Mobile Logger app, set the alarm at the preset trigger levels, you would be able to do exactly as you described.