Test & Tools
  • Technologies
  • More
Test & Tools
Blog Cheap active oscilloscope probe
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kk99
  • Date Created: 4 Aug 2026 3:58 PM Date Created
  • Views 277 views
  • Likes 8 likes
  • Comments 1 comment
  • siglent
  • active probe
  • measurement
Related
Recommended

Cheap active oscilloscope probe

kk99
kk99
4 Aug 2026
Cheap active oscilloscope probe

image

During the last test of the Si5351 clock generator, I thought that it would be nice to compare measurement results between a passive probe to an active probe. I have found one based on a well-known design with usage of the high frequency BF998 FET transistor input stage. It is really cheap as for an active oscilloscope probe, and based on opinions on the network, it performs really well, especially up to the 500 MHz, which is the limit of my scope. I have bought one on eBay. The probe came with a SMA to BNC cable, SMA connector and 2pcs of golden-plated spring-loaded pins. This oscilloscope active probe has the following parameters:

  • 100kHz - 1.5GHz bandwidth 
  • input capacitance 0.5pF
  • input impedance 10Mohm
  • gain -15dB +/-2.5dB (fits approx. 5:1 the probe voltage ratio)
  • DC supply voltage 7V - 30V
  • reverse supply voltage protection

After soldering the pins, SMA connector and power supply wires, I was ready for a measurement of the clock from the output of the Si5351 generator.
image

image

I have powered a probe at 12 V and changed the oscilloscope input to 50 Ohm. Here are the results of measurements for different frequencies:

{gallery}Measurements

image

10 MHz clock

image

20 MHz clock

image

50 MHz clock

image

100 MHz clock

image

150 MHz clock

There is real improvement in the quality of the measured signal. Here is a comparison of the measured 150 MHz signal with the SPL5050A passive probe, which has a bigger capacitance:
image
to the same signal measured with active probe:

image

Probably a similar improvement in that case could be achieved with the Z0 probe (low-impedance probe), when the high impedance of the probe is not required (e.g. for digital signals).

This active probe meets my expectations. I need to think about a case for it and maybe change the power supply to a battery.

Update 08.08.2026

I have found that a container for the iron tip will really fit the PCB with an active probe. The only things that required modification were to perform holes with proper free space for spring-loaded pins and enlarge holes for power supply wires. The holes for spring-loaded pins I performed with a thick needle. The holes for power supply wires were cut with wire cutters and finished with a scalpel. After inserting the PCB with an active probe, everything fitted very well. Below there are photos with the result of this modification:

image

image

Now it is much easier to operate or hold it.

  • Sign in to reply
Parents
  • DAB
    DAB 2 months ago

    Very good post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB 2 months ago

    Very good post.