Test & Tools
  • Technologies
  • More
Test & Tools
Blog DC Voltage Measurement Accuracy: AD584KH voltage reference
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 20 Jun 2023 8:47 PM Date Created
  • Views 5229 views
  • Likes 14 likes
  • Comments 37 comments
  • dmm6500
  • reference
  • keithley
  • AD584
Related
Recommended

DC Voltage Measurement Accuracy: AD584KH voltage reference

Jan Cumps
Jan Cumps
20 Jun 2023
DC Voltage Measurement Accuracy: AD584KH voltage reference

Follow up on  DC Voltage Measurement Accuracy: Measuring DC voltage with high accuracy on a DMM6500 . 
I bought a little voltage reference based on Analog Device's AD584 .

image

The reference is the AD584KH. The kit supports the 4 programmable reference values. It comes with a label showing measurements on a HP 3458A

image

image

image source: analog devices datasheet

Calibration values (25° / 49% humidity):

  • 2.49974
  • 5.00203
  • 7.50113
  • 10.00277

Calibrated by http://www.haoqielec.com/wap/en/aboutus.html

Checking Keithley DMM6500

I let the reference and DMM warm up for an hour. Room temperature was 26°. Humidity unknown

image

I used Keithley's TSP script "Measuring DC voltage with high accuracy". I used that in the previous post too.
The Test Script Builder log gives a higher resolution than the 6500 display.
I let the reference settle for 5 minutes on each value before running the script and getting the measurement

CAL (HP 3458A DMM6500 round
2.49974 2.4997806153 2.49978
5.00203 5.0021082424 5.00211
7.50113 7.5012037198 7.50120
10.00277 10.002870735 10.00287

Thoughts and remarks? Post them in the comments

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 3 years ago in reply to ggabe +2
    Hopefully these photos can be zoomed up without the content system compression causing issues: The marking is A1 HB , or possibly A1sHB , and it looks like it is Si2301 (P-ch MOSFET) . I have some…
  • ggabe
    ggabe over 3 years ago in reply to Jan Cumps +1
    Could it be a ground current? What if you battery power and also connect the USB ground?
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps

    Wow Scream 31 digits....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Jan Cumps

     Jan Cumps wrote

    "I don't need a voltage reference."

    Correcting myself. I just found a use for it. I'm reviewing a Renesas µController with decent analogue front end for a road test.
    When I measure the AD584KH 2.5 V reference with it, averaging over a few 100 samples, I get 2,4981760002173721790313720703125 V

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to ggabe

    I don't need a voltage reference. If you look at it from that perspective, it's way better than what I need.
    I bought it as an experimental toy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ggabe
    ggabe over 3 years ago in reply to ggabe

    Honest disclosure: in my stash are AD588, MAX6126, LTC6655, ADR1399

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ggabe
    ggabe over 3 years ago

    Good, but not great. Better references are available today. It’s a “gateway drug” for higher precision references, a voltnut will buy eventually. So what not start at a higher precision one, if this one will be a throw away?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>