Test & Tools
  • Technologies
  • More
Test & Tools
Blog Drag-soldering Surface-mount components
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 12 May 2020 1:23 AM Date Created
  • Views 11298 views
  • Likes 17 likes
  • Comments 28 comments
  • smt soldering
  • smd
  • prototying
  • learn to solder
  • drag soldering
Related
Recommended

Drag-soldering Surface-mount components

shabaz
shabaz
12 May 2020

I had to solder an IC today, nothing new there, but usually I'll use a 1mm conventional soldering tip (slice off conical shape) to solder each individual pin one-by-one, deal with any bridges with desoldering braid, and call it a day.

 

There are dozens of different ways to solder though. I have a reflow oven, but it is overkill for a single IC. I have a pre-heater and a hot air tool but the ones I have are under-powered. 

 

Although I have seen an expert present drag soldering once, I have never tried it because I've been ok with the way I do it - it works, although it is a bit tedious. However, there has been a drag-soldering tip (also known as a spoon tip or gull-wing tip) in my drawer for years, of size 1.9mm diameter. I figured I'd give it a shot since I was soldering a relatively cheap component, and with the recent activity on element14 concerning soldering tools Cool Tools Kit Awards 2020  and soldering station reviews Weller Soldering Station WT Series I figured I'd post a photo of the results..

 

The part was PCF85176T which is a 56-pin 0.5mm pitch device - it was for an LCD board Building a 3.5 Digit Low Power LCD Module .

The finest SMD part I've had to do with a soldering iron was 0.4mm pitch, so this was not going to be as bad as that, but still a good test.

 

The result with the drag soldering was quite good! If your soldering iron accepts such a tip, I think it is worth giving it a go!

 

image

 

Here is the result, close-up (click to enlarge further):

image

I didn't take photos or a video [edit - see below for a second attempt which was recorded] of the process (because I fully expected to fail the first time), but in brief, this is what I did - I can take more photos next time:

 

  1. Put on head magnifier and switch on a desk lamp!
  2. Position the IC and temporarily affix it to the board (can use paper or Kapton tape for that, or two small blobs of blu-tack [temporary putty] at either end - I used the blu-tack this time and was able to very finely adjust the position of the IC by just pressing against the blue-tack)
  3. Solder a corner pin on either side, using regular solder so that the part would stay in position, and then removed the blu-tack
  4. Apply a thin long bead of flux along the pins (I actually applied some liquid flux because I couldn't find the syringe of paste, but then 10 seconds later I found it - so I had a mix of both!)
  5. Feed some solder into the spoon tip until it is nicely convex (I didn't make it bulge a lot, perhaps just 70% of capacity, I'll explore that more next time)
  6. Place the tip so that it was touching the board for helping with position support, and then angled down so that the blob was into the pins, and just ran the iron along! In a couple of places where I thought it wasn't adequately soldered or there was a bridge, I just repeated in that area using the same method.
  7. Dab with a half of a dry wipe to soak up some of the flux, and then put a few drops of isopropanol (isopropyl alcohol or IPA) on the board, rubbed with an antistatic stiff brush, and then wiped it all off with the clean part of the wipe.
  8. Using a thin scalpel blade (very small, surgical type), and with the head magnifier on, using the unsharpened side of the blade, i.e. sharp side up, I pressed against the side of each pin (the thin scalpel blade flexes slightly) to confirm it was stuck with solder, and did that for each pin - it doesn't take long to do this, and gives me peace of mind rather than having to troubleshoot with potentially unsoldered pins later.

 

I have no idea if my technique was entirely correct or not, all I can say is that it was far quicker than soldering each pin individually, and the result visually looks good I think.

It would be great to learn any tips, and about other peoples drag soldering or alternate techniques for surface-mount too!

 

Second attempt

This time around I recorded it, this is uncut from start to finish:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 6 years ago +3
    It sure looks pretty! John
  • Fred27
    Fred27 over 6 years ago in reply to Andrew J +3
    If it looks OK then I just power it up and hope!
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +3
    I reckon that the key to re-touching surface mount parts is to use lots and lots of really runny flux. I use the Warton metals Future 315 from Rapid Electronics, and it's just like water in terms of viscosity…
Parents
  • Andrew J
    Andrew J over 6 years ago

    How do you test the connections once soldered Shabaz?  I’m always concerned that solder has bridged under the chip that braid or dragging doesn’t pull out, or that a pin that looks soldered actually isn’t.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to Andrew J

    Hi Andrew,

     

    For this style of part and QFP, bridges and excess solder behind a pin are identifiable visually (or with a lens+light to look at the pins from a few angles) and as Fred says, re-dragging can fix that (or if really persistent, then some desoldering braid). For the unsoldered pins, I think I've got a reliable method, it hasn't failed for me yet. That's to scrub first with the IPA+stiff brush, because otherwise dried sticky flux could make it seem like a pin is connected, so it needs cleaning first. Then, the step 8 (nudging each pin with the blunt side of a small scalpel) with just enough pressure that the blade can flex slightly will soon identify if a pin is unsoldered. The risk is that nudging an unsoldered pin will bend it of course, but it is easily unbent.

    After this drag soldering test, I cleaned and tested each pin in this way, and no pin was disconnected, which is awesome! That might not always be the case (especially when a part has slightly bent pins before it is soldered) but the nudge test seems to always work for me so it should detect that.

    And then just power up!

    You can see the approx blade size below, the brushbrush is from Farnell, there are ebay ones that look similar but those come with soft bristles which don't help. This one has stiff bristles, and was purchased about 8 years ago, so still doing fine.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 6 years ago in reply to shabaz

    I do have one of those brushes - I'm sure you've recommended it in the past.  I'm not much of a fan of the 'power up and hope' approach and was wondering if there was something better!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Andrew J
    Andrew J over 6 years ago in reply to shabaz

    I do have one of those brushes - I'm sure you've recommended it in the past.  I'm not much of a fan of the 'power up and hope' approach and was wondering if there was something better!