Test & Tools
  • Technologies
  • More
Test & Tools
Blog Drag-soldering Surface-mount components
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 12 May 2020 1:23 AM Date Created
  • Views 11415 views
  • Likes 17 likes
  • Comments 28 comments
  • smt soldering
  • smd
  • prototying
  • learn to solder
  • drag soldering
Related
Recommended

Drag-soldering Surface-mount components

shabaz
shabaz
12 May 2020

I had to solder an IC today, nothing new there, but usually I'll use a 1mm conventional soldering tip (slice off conical shape) to solder each individual pin one-by-one, deal with any bridges with desoldering braid, and call it a day.

 

There are dozens of different ways to solder though. I have a reflow oven, but it is overkill for a single IC. I have a pre-heater and a hot air tool but the ones I have are under-powered. 

 

Although I have seen an expert present drag soldering once, I have never tried it because I've been ok with the way I do it - it works, although it is a bit tedious. However, there has been a drag-soldering tip (also known as a spoon tip or gull-wing tip) in my drawer for years, of size 1.9mm diameter. I figured I'd give it a shot since I was soldering a relatively cheap component, and with the recent activity on element14 concerning soldering tools Cool Tools Kit Awards 2020  and soldering station reviews Weller Soldering Station WT Series I figured I'd post a photo of the results..

 

The part was PCF85176T which is a 56-pin 0.5mm pitch device - it was for an LCD board Building a 3.5 Digit Low Power LCD Module .

The finest SMD part I've had to do with a soldering iron was 0.4mm pitch, so this was not going to be as bad as that, but still a good test.

 

The result with the drag soldering was quite good! If your soldering iron accepts such a tip, I think it is worth giving it a go!

 

image

 

Here is the result, close-up (click to enlarge further):

image

I didn't take photos or a video [edit - see below for a second attempt which was recorded] of the process (because I fully expected to fail the first time), but in brief, this is what I did - I can take more photos next time:

 

  1. Put on head magnifier and switch on a desk lamp!
  2. Position the IC and temporarily affix it to the board (can use paper or Kapton tape for that, or two small blobs of blu-tack [temporary putty] at either end - I used the blu-tack this time and was able to very finely adjust the position of the IC by just pressing against the blue-tack)
  3. Solder a corner pin on either side, using regular solder so that the part would stay in position, and then removed the blu-tack
  4. Apply a thin long bead of flux along the pins (I actually applied some liquid flux because I couldn't find the syringe of paste, but then 10 seconds later I found it - so I had a mix of both!)
  5. Feed some solder into the spoon tip until it is nicely convex (I didn't make it bulge a lot, perhaps just 70% of capacity, I'll explore that more next time)
  6. Place the tip so that it was touching the board for helping with position support, and then angled down so that the blob was into the pins, and just ran the iron along! In a couple of places where I thought it wasn't adequately soldered or there was a bridge, I just repeated in that area using the same method.
  7. Dab with a half of a dry wipe to soak up some of the flux, and then put a few drops of isopropanol (isopropyl alcohol or IPA) on the board, rubbed with an antistatic stiff brush, and then wiped it all off with the clean part of the wipe.
  8. Using a thin scalpel blade (very small, surgical type), and with the head magnifier on, using the unsharpened side of the blade, i.e. sharp side up, I pressed against the side of each pin (the thin scalpel blade flexes slightly) to confirm it was stuck with solder, and did that for each pin - it doesn't take long to do this, and gives me peace of mind rather than having to troubleshoot with potentially unsoldered pins later.

 

I have no idea if my technique was entirely correct or not, all I can say is that it was far quicker than soldering each pin individually, and the result visually looks good I think.

It would be great to learn any tips, and about other peoples drag soldering or alternate techniques for surface-mount too!

 

Second attempt

This time around I recorded it, this is uncut from start to finish:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 6 years ago +3
    It sure looks pretty! John
  • Fred27
    Fred27 over 6 years ago in reply to Andrew J +3
    If it looks OK then I just power it up and hope!
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz +3
    I reckon that the key to re-touching surface mount parts is to use lots and lots of really runny flux. I use the Warton metals Future 315 from Rapid Electronics, and it's just like water in terms of viscosity…
Parents
  • ralphjy
    ralphjy over 6 years ago

    Great job!!  Can't wait to see a video image.

     

    I can see that with a lot of pins in a row that this can save a ton of time.  I've always done the individual pins one-by-one, but probably because I haven't needed to do large parts.  I also haven't tried assembling my own boards - just rework.  I think some PCB design/fabrication/assembly might be a goal for this year.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to ralphjy

    Hi Ralph,

     

    Thanks! I made another of the boards today, and this time recorded it, inserted into the blog post above. It can be a lot of fun creating PCBs, so hopefully you'll enjoy the experience!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 6 years ago in reply to shabaz

    Thanks for the video.  I’m impressed at how well that works.

     

    I used to do a lot of PCBs 30-40 years ago, both both design and layout.  We ended up using the Cadence tools when we transitioned to multilayer boards with more than 4 layers.  I’m sure it will be a lot of fun but I’m sure the free tools won’t be as capable and by the time we got to SMD someone else was doing the layout for me.  It’s amazing the quality and low cost and quick turns that you can get from fab houses nowadays.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Andrew J
    Andrew J over 6 years ago in reply to ralphjy

    I'm no expert and my experience is limited to one tool - Kicad - but it's pretty good, and will deal with multiple layers.  Need to watch the footprint library though, they aren't always accurate for non-common parts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Andrew J
    Andrew J over 6 years ago in reply to ralphjy

    I'm no expert and my experience is limited to one tool - Kicad - but it's pretty good, and will deal with multiple layers.  Need to watch the footprint library though, they aren't always accurate for non-common parts.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ralphjy
    ralphjy over 6 years ago in reply to Andrew J

    Good to hear....   Kicad is the tool that I’m going to try.