Test & Tools
  • Technologies
  • More
Test & Tools
Blog Electronic DC Load - Design and Build to test PSU Project
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Robert Peter Oakes
  • Date Created: 2 Jun 2015 5:14 AM Date Created
  • Views 12051 views
  • Likes 7 likes
  • Comments 32 comments
  • modular_power_supply
  • electronic_dc_load
  • energy_power
  • dc_load
Related
Recommended

Electronic DC Load - Design and Build to test PSU Project

Robert Peter Oakes
Robert Peter Oakes
2 Jun 2015

Back tot he Main Modular Bench power System Project The Modular Bench Power Supply ++, The Essential DIY Build for Every EE Student and Old Timer alike...

 

I keep promising myself I will build an Electronic DC Load and have kept defering it, well no longer, I finally ot it designed and tested on a breadboard and will be following up with a completed unit in a project case

 

It can go way above 30V (60 to be precice and upto 5Amps), the MOSFET I used the IRFP064 is able to go to 70Amps but thats more than my wiring would stand and way more than i need so I designed the load to go upto 5Amps for now. All I need to do though is change the current sense resistor and it can easily become a 10Amp unit

 

For the heatsink I tested with a standard one but subsiquently found an old CPU heatsing with a Fan attached which looks like it will do a grand job of cooling the MOSFET etc so it will be the one I use in the build.

 

Testin showed I can load as little as 250mV and still control upto an Amp which is great and once im over 1V source voltage I can go all the way to 5Amps with ease.

 

Now you all know the math "Power = Volts * Amps) so therefor will know that at 30V an 5Amps theres 150W being dissipated in the MOSFET and thats a lot of heat. I am pretty sure the CPU heatsing even with the fan will still get pretty hot and I look forward to characturizing it once the bukd is done. till then I have no idea how well it will work but I am sure it will be better than the one I tested the circuit with

 

for now, here is the schamitic I came up with

image

 

It will use between 12 and 24V for the DC in, has a REF02 Voltage reference to provide the manual setting via a 10 Turn pot and has a trimmer to accuratly set the top output to precisly 5A if so desired.

I also included a BNC input as an alternate control allowing a signal generator to control the load enabling many more test scenarious to be executed like transient response testing, noise response, Waveform based profile, pulse response etc.

 

The design does have a frequency limit before the output falls off of only a few hundred Hertz but that should be more than enough for this. It may be way better once it is off the bread board and the wiring is significanly shorter too but I wont be able to test that till the buld is complete. I will add a video to this blog once that is done and tested

 

anyway, enough banter, here is the video (Yes Im back to my 1+ hour videos... sorry I tried)

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Hope you enjoy

 

Thanks to Vishay Precision Group ( VPG) Bulk Metal Film division for their kind donation of the current sense resistors and precision metal film resistors used in the resistor divider part of the design. It takes the use of this project to the next level by bringing stability to the key parts of the design in the order of a few parts per million... oh yaaaa.

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor +3
    Hi Monica, Su Englais esta bien, mejor que mi Espanol. Don't worry too much about R-1. You can build one that will be accurate enough for this application. Just get a regular 0.1 ohm resistor and tie extra…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago in reply to stephanc +3
    I just checked on the first one ( IRL540N) and it is not even showing a DC spec, nothing more than a 10mS pulse This is the safe operating area.
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to jw0752 +2
    Perfect jw0752 , that is exactly what I would have done if Vishay had not been so generous with some samples and is a perfect example of how to roll your own when the needs arise Thanks for sharing
  • waelect
    waelect over 10 years ago in reply to jw0752

    I have done this with my system, but in all realism when there is a tolerance value to the resistor, it is not going to make much of a difference until the resistor gets really low 0.01ohms.

     

    No matter what, the whole set-up will need to be calibrated with a know source. I think those resistor have a 5-10% tolerance, so a couple of mm of wire attachment may not be an issue.

     

    Malcolm

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to jw0752

    Perfect jw0752, that is exactly what I would have done if Vishay had not been so generous with some samples and is a perfect example of how to roll your own when the needs arise

     

    Thanks for sharing

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 10 years ago in reply to e14 Contributor

    Hi Monica,

    Su Englais esta bien, mejor que mi Espanol.

     

    Don't worry too much about R-1. You can build one that will be accurate enough for this application. Just get a regular 0.1 ohm resistor and tie extra wires close to the body that will be used to take the voltage reading back to the Op Amp. Solder the wires. I have mocked up a picture to show you what I mean. This is a poor man's Kelvin Resistor.

     

    image

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Thank you    John

     

    Sorry for my English

     

       You know where I can buy the resistor R1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    Hi All, I am also now in the process of gearing up to continue the project, I will start by providing a review and then proceed to automation, adding DAC control and ADC feedback to various controllers like Arduino, LaunchPads and Raspberry PIs. I will include parts list this time arround as well to help out sourcing parts.

     

    But as John stated, my aim is to teach you what you need to design and build your own and as such am happy to answer any questions to help clarify the design I have presented

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>