Test & Tools
  • Technologies
  • More
Test & Tools
Blog LabVIEW NXG Community Edition: Post 2 - Hardware Abstraction Framework
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Andrew J
  • Date Created: 20 Oct 2020 4:03 PM Date Created
  • Views 1689 views
  • Likes 6 likes
  • Comments 2 comments
  • labview
Related
Recommended

LabVIEW NXG Community Edition: Post 2 - Hardware Abstraction Framework

Andrew J
Andrew J
20 Oct 2020

Introduction

In this post, Post 1, I reviewed LabVIEW NXG and want to carry on the series by describing a framework I have created to simplify the creation of test applications and the interaction with test instruments.  In Post 1 I went through the process of creating a very simple application to obtain a test instrument's identity using the NI VISA components; as I started to create some applications to get to grips with LabVIEW NXG it became very clear that I was duplicating code, and continually abstracting it out.  This was a prime candidate for creating a testing framework to support application development and doing that would be a great way of learning the intricacies of LabVIEW NXG.

 

This post, then, describes the framework as I've written it so far.

 

Overview

The goal of creating the Hardware Abstraction Framework (HAF) was to provide a non-instrument-specific way of interacting with a test instrument and provide a rich set of features to simplify the creation of test applications.  A LabVIEW NXG developer should be able to select pre-defined commands and encapsulate the complexities and specific instrument requirements for sending commands and reading responses so that a reasonably complex test application can be created quickly and simply.

 

As it's developed so far (version 1.3.0), a better moniker might be Hardware Somewhat-Abstracted Framework but the 'somewhat...' elements will improve as I develop it further.  Currently, it's very SCPI-focussed (although a developer doesn't need to get into SCPI commands unless they want to extend what already exists) and instruments have enough quirks that its proved impossible so far to completely abstract that away.  Nonetheless, the framework allows:

  • the use of non-SCPI named commands (called Executables) to communicate with any test instrument.  Actual commands are built by the framework with parameters if required, and results parsed automatically
  • the use of proper data types and conversion to-and-from strings automatically
  • co-ordinated sending of commands that ensures, where necessary, an instrument isn't overloaded when already processing a command
  • the ability to send commands:
    • one off: command sent once, and the result returned once
    • continuously: command sent over and over again, with the result processed each time, until the test application tells the framework to stop
    • timed: command sent over and over for a specific duration of time
    • repeatedly: command sent a specific number of times
  • extensibility of commands and execution methods.  For example, you may want to extend the framework to provide the means to run a command in a different way to those in the bullet above.
  • interfacing with USB connected instruments and Serially connected (COM port) instruments without exposing the mechanics of doing so
  • event processing: the framework will respond to Start, Stop, Pause, and Resume events raised by the test application
  • notification: results can be returned once all commands have finished processing OR notified to the test application as returned from the instrument.
  • reuse of a test application that is highly parallelised and incorporates all the run-time elements needed for a featured, complex test application.  The example applications with the framework use this test application.  It's not necessary to use the test application of course, it's just a potential starting point.
  • reuse of test instrument wrappers that I've provided for the test instruments I own, including Arduino.

The framework is developed enough that a developer just needs to decide what commands to use and how to run them and to build a suitable UI for that.  It's likely to be necessary to define your own test instruments to the framework assuming you don't have the same as me.

 

Downloading the Framework

The framework can be downloaded from GitHub here - instructions for doing so are provided and there are no licensing restrictions.  At the time of writing, the framework is at V1.3.0 and you should pull from the Master branch.  The Developer branch will contain in-progress features but these may not be fully tested and the Readme is only updated when I create a release.

 

It would be great if anyone wants to co-operate on developing this further, particularly by submitting Driver wrappers and new Executables.

 

Example Usage and Framework Overview

Before jumping in to describing the framework in more detail, I want to demonstrate two test applications that I have created using the framework.  I also provide a walkthrough of the re-usable test application and the framework itself.  Hopefully the videos aren't too bad - I still feel very self-conscious making them!

 

Measure example

This will use a DMM to continuously measure a resistance.  The DMM is connected to a 5K potentiometer and will measure resistance as I move the wiper.  The example can just as easily measure anything the DMM is capable of if an appropriate test circuit is set up.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Generate and Measure example.

This will use a PSU to generate a voltage and a DMM to measure it; both are connected to a 1K resistor.  The PSU will step the voltage from a starting value to an ending value and the DMM will grab a measurement after every increment

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Example Test Application Overview

In this video I walk through the example test application to describe how I've created the examples. The example test application (reused across all examples) can be re-used with your own test applications and it will give you pre-built access to Events, Messages and Notifiers in a performant, parallelised manner.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Framework Overview

In this video, I describe how the framework works once the test application calls it - it may be useful to watch the Example Test Application Overview video first if you haven't done so.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Detailed Description

The framework provides a means of driving test instruments through the use of abstract commands (non-instrument specific) in an automated way.  Currently, the framework is very SCPI focussed but can be extended to support other test syntaxes.  In the current version (1.3.0) available commands are limited but the fundamental framework is in place.

Overview

The basic approach to instrument testing is to send one or more commands to one or more instruments and process the results.  Some tests will be simple, one-off commands; others will be more complex involving multiple commands, over multiple instruments, over an extended period of time.

The framework attempts to meet these needs and has some basic concepts which a user should be aware of:

  • Commands: a command is an instruction sent to an instrument that it can understand, run and, if necessary, provide a result.  The framework seperates out *instrument specific* commands from *instrument independent* commands which means that you can build tests up without a specific understanding of instrument-specific syntax, e.g. you could use a command such as "Identity" rather than "*IDN?".  The framework calls these Executables and there are two types: a Write Executable - sends a command only - and Read Executable - sends a command then reads a result.

  • Instrument: a representation of an actual test device to be used.  This can be anything that can be driven by LabVIEW NXG and the framework doesn't require instrument-specific drivers.  Instruments are abstracted so that you can use them 'generically' leaving the framework to do any necessary translation into 'specifics'.  Obviously, to use your own instruments you will need to provide some of this translation but the benefit will be that your overarching tests can be generic and reusable across different instruments, e.g. substitution of one manufacturer's DMM with another manufacturer's DMM without change to the test.  The framework calls these instrument abstractions Drivers.  Drivers provide the interface between the framework and a physical instrument.
  • Processors: these actually run the Executables against a Driver in a controlled manner.  They control the overall execution flow utilising events and messages to interact with the test application itself.  Complex processing can be controlled by using specific types of processors: single-shot, repeating, continuous, timed and so on.  The framework calls these Executable Processor and Executable Director.

 

The basic approach to running a test is to follow these steps:

  1. Instantiate an Executable that represents the command you wish to use.

  2. Associate a Driver to that Executable which will represent the instrument to send the Executable (command) to.
  3. Repeat this for each command you want to run in your test.
  4. Associate these Executables to one or more Executable Directors, selected on the basis of how you wish the commands to run.  For example, you may select an Executable Director to run once a Reset Executable and a Repeating Director to run a Measure Executable 10 times.

  5. Associate these Executable Directors to an Executable Processor and run the test.  The Executable Processor will process each Executable Director until they have finished; results are sent back to the testing application as notifications and the Executable Processor will listen for events such as Pause, Resume, and Stop and modify the processing accordingly.

  6. Your test app can listen out for a Done event to know when processing has finished; it can also look for result messages or notifications to handle and display those.  How complex you make these is up to you but check out the examples for ideas.

 

Many Executables in the framework can be used as-is in test applications but there may be Executables that are missing for your purpose.  You can create your own by following the pattern established for the existing ones.  Similarly, the Executable Directors are likely to be sufficient for most test applications but again, you can create your own by following the pattern established for the existing ones.

 

Unless you use the same instruments that are wrapped by Drivers in the framework, it is most likely that you will have to create your own for your instruments.  Again you can follow the pattern established for the existing ones; you may want to consider uploading these to the repository for inclusion in a future release.

 

The rest of this document describes the framework in more detail and how you can use it.

 

Interacting with the Framework

Your test application will interact with the framework through other means than just asking it to process Executables.  The Framework is set up to respond to Events your test application can raise:

  • Pause: Processing will be paused at the end of the current processing of Executable Director(s) - remember these could be long-running.  It does need to finish any currently running processing so as to ensure instruments are not left in an unknown state.  The Pause will timeout after 60-seconds and all processing will finish with an error being returned indicating the timeout occurred.
  • Resume: Processing will be resumed if paused.
  • Stop: Processing will stop immediately after the current processing of Executable Director(s) - again, so that instruments are not left in an unknown state.

There is no concept of *Abort Immediately* - the framework will always attempt to properly close an instrument down so that it is not left in an unknown state.

 

The Framework will interact with your test application through Events as well:

  • Done: Raised by the Framework when all processing has completed. You could, perhaps, on hearing this event, unblock the UI, display any messages, quit the test app, write results to a database and so on.

 

It also interacts with your test application via messages on a Notification Queue or via a Notifier:

  • Result: When a Read Executable runs and receives a result, it stores that and posts itself on to the Notification Queue as message data for the Result message.  Your test application should be waiting to receive these messages so you can do something with the result.  The Executable knows how to process a raw result (from the instrument) into something useable and of a specific data type; any results for parameters can also be processed into useable information.  Each Executable has a unique ID and you can tie a result on the Notification queue to a specific Executable instance so your test application knows how to handle the result.
  • Result Notifier: Create a Notifier and pass it into the Framework.  Each result received will be posted through this notifier to the test app (as for Result, the data passed is the Executable itself which stores the result.)

 

Which to use?  The framework may block the Test App when it is called, until all processing is finished.  Whilst the results will be posted as messages on the Notification queue, your test app won't get a chance to process them until the Framework is Done.  This is fine for simple one-off commands but no use for long-running commands.  In the latter case, you will want a parallel thread waiting on a Notifier to appear containing the result - these can be processed as they are generated by the Framework, irrespective of whether the rest of the Test App is blocking.  There are examples that show both approaches.

 

Events, Messages and Notification Queues are all established by the Framework and are available for your test application to use.  You must create your own Notifier to pass into the Framework if you take this approach for result processing.

 

Examine the example applications to see how to use Events and Notifications.  These example applications form a great template for building your own applications on.

 

Framework Structure

The framework has been mostly written using LabVIEW NXG's object oriented features so the majority of interaction between your test application and the framework will involve the use of classes; extensions to the framework will likewise be done through extending existing classes and overriding methods.

 

As the source is provided, you are encouraged to use one of the examples and single-step through it observing how the framework is called and how interactions play back-and-forth.

 

In terms of processing, the framework follows a Queued Message Handler pattern which is standardised within LabVIEW NXG.  The examples, although simple in themselves, also use this approach to provide a basic pattern for you to follow in your own test applications.

NI decided that a by-value approach to objects will be used, rather than by-reference.  The implications of this is that all data flows work on *copies* of data rather than references.  You need to bear this in mind as it is easy to get caught out.  In many cases, changing some object's data member will be on that copy and not an originating instance - the data will need writing back to that instance.  This can be confusing when changes don't work!  The framework takes care of it correctly in its own processing, but any you add, or code within your test application must be carefully written to avoid data loss or unexpected behaviour.

 

There is very little in the way of reflection available in the language so some actions are not as independent of implementation as they could be otherwise.

Core Classes

Note: The diagrams below are intended to show main classes and methods and are not a complete picture of the framework.

image

 

The class diagram above shows the classes and relationships that form the core element of the framework.  I'll break it down into smaller sections.

Executable

image

An Executable represents a command that can be sent to a Driver for running on an instrument.  As the framework evolves over time, these will become much more than just commands for Drivers, and will represent other execution constructions such as optional pathways, or directives to help with processing.

 

There are two types of Executable:

  • WriteExecutable: represents a command that can be sent to an instrument but which requires no response.
  • ReadExecutable: represents a command that can be sent to an instrument and for which a response or result will be returned.  You will note it inherits some of its functionality from WriteExecutable: you don't need to run a Write Executable *and* a Read Executable as the latter incorporates the functionality for you.

 

An Executable is associated with a Driver whose responsibility it is to undertake any instrument specific translation of a command.  The framework will arrange for the Driver to run the command at the appropriate moment.

 

There are two ways a Driver can run an Executable:

  • Immediately: as it says - the Driver sends the command straight to the instrument.
  • When able: in this case, the Driver will wait for the instrument to finish processing any existing commands before sending this one.

 

An Executable controls this with its canOverlap property: if true, the Executable will be run immediately; if false, when able.

 

A ReadExecutable will hold a result returned from the instrument.  It does so in a raw form, rawResult - that is, it provides no interpretation of that result until asked to do so by the test application calling buildResult.  The test application will be notified of an available result via a result message raised on the Notification queue or a raised Notifier.  The result data is the same in both cases: the Executable itself is passed back to the test app and can be used to obtain the results as a raw value (String) or a typed value.

 

Executables can take parameters to send along with the base command.  These are represented by the Parameter class.  The framework will automatically add any requested parameters to the command before it is sent to the instrument: you just need to add the ones you want to the Executable when you create an instance of it.  A Parameter will hold a result, if available, and is capable of parsing that into a typed value for the test application.

 

Executable Settings are a way of provisioning configuration settings for Drivers, independently of how they may be applied to an instrument.  For example, you might use an Executable Setting called 'Settling Time'; on one DMM it might equate to 'Settle Time' whilst on another it might be 'Settling Duration'.  You won't care - the driver will map these to instrument specific configurations.

 

You'll see from the class diagram that Executable Settings provides no specific behaviour so is really just a placeholder.  There is more information in the Settings section below, but the functionality for settings hasn't needed any specific behaviour for Executables in the current version.

 

So what do you need to do to use the framework?  Basically, just use one of the existing Executables and add it to an Executable Director.  If none of the existing Executables are of any use, then create your own by following the pattern established by an existing one.

 

Here's an overview of two Executables:

image

You can see that all is needed is a concrete implementation of getBaseCommand (the command as it appears without any parameters or end of line characters) and, for Read Executables, a concrete implementation of buildResult which parses a raw result into a useable format for the test application - if the usable result is a string, this can just return the rawResult.

 

Driver

image

Driver is responsible for interfacing with actual test instruments providing the necessary mappings between a generic test language and instrument-specific language.  By doing this, a user of the framework can standardise on names for things like commands, parameter names, setting names and so on and leave the Driver to translate on an instrument-by-instrument basis.

 

SerialDriver should be used for instruments that will use a Serial communication method, e.g. Arduino Uno.  This operates the same way as the standard Driver but expects a device to be available on a mapped COM port rather than on, say, a USB port.

 

It is envisaged that future versions of the framework will be able to load mappings between the generic and specific from an external source to allow tests to be more configurable.  Lack of reflection in LabVIEW NXG makes this problematic at the moment.

 

A Driver will execute a query for an Executable when directed by the framework, obtaining a response as necessary.

 

Driver Settings are configurable items for an instrument and are mapped between a generic Executable Setting and the instrument setting.  More information is available in the Settings section.

 

So what do you need to do?  When you instantiate an Executable you need to give it a Driver to be used to process it.  It's likely you will need to create your own Driver instances but examples are available to draw from:

image

 

You can see here that all you need to provide is a concrete implementation for buildDriverSettingsMappings and getInstrumentAlias as the framework handles everything else.

 

The Arduino Uno Driver also provides an overridden readSerialPortAttributes because I want to communicate with it at 115200 baud, rather than the default 9600 baud, and I need the initialisation to wait 2000 milliseconds after opening a port to ensure the Arduino will be available to process commands.

 

These concrete Drivers are available in namespace Z_Implementation.

 

Setting

image

Setting is meant to represent a specific configuration setting that can be sent to the instrument by the Driver - you can see it has a name and value.

 

There are two types of Setting:

DriverSetting: This represents a setting *as known to the instrument*.  The type is so that the framework can properly parse the value; beenApplied is set by the framework once the setting has been made so that it doesn't constantly send it on every command (see the section on process flow) - this could be reset so it is re-applied.  In fact, if you use a Reset Executable, it ensures that the settings will be re-applied.

ExecutableSetting: This represents a generic, non-instrument specific setting, i.e. a setting you can refer to for all instruments.  The Driver maps this setting to a DriverSetting which then removes any concern of naming differences.  E.g. you could refer to a setting Settle Time and on one DMM it might actually be Settling Time and on another DMM it might be Time to Settle.

 

You add Executable Settings to the Executable as you instantiate it.  If you create a Driver, you must also create a set of mappings from ExecutableSetting to DriverSetting; if a setting is not used by a particular driver, use Ignore as the mapped name and that's what the framework will do.

 

The framework is currently very SCPI focussed and settings aren't actually used yet.  As the framework evolves it is envisaged they will become more integrated and the feature finished.

Therefore, currently, you should not use Settings as they are not implemented.

Processing

image

Processing of Executables is performed through ExecutableDirector instances and an ExecutableProcessor instance.

 

  • ExecutableDirector: The ExecutableDirector controls the processing of one or more Executables. Each Executable is processed at least once and depending upon the choice of ExecutableDirector, multiple times.
    • ExecutableDirector: processes each Executable once only.
    • RepeatingDirector: processes each Executable timesRepeat times.

    • ContinuousDirector: processes each Executable continuously until ordered to stop.  Your test application can do this by raising a stop event.  You could abort the running VI but this may leave the instrument in an unknown state (recover with a Reset Executable in the next test run.)
    • TimedDirector: processes each Executable for a minimum period of time.

An ExecutableDirector can hold more than one Executable and each Executable is processed in turn in the order loaded.  A processing run for an ExecutableDirector is 'every Executable', so Stop and Pause orders (via events) are acted on at the end of a run (actually, at the start of the next run if there is one.)  For the TimedDirector, the duration is a minimum amount of time because a processing run will be completed once started; note also that a Pause order does not stop the clock and the duration paused counts towards the overall duration.

waitTime is a duration in milliseconds between processing of each Executable.  So with a wait time of 10ms, and three Executables, processing will be Executable1-wait 10ms-Executable2-wait 10ms-Executable3.  For a TimedDirector, this wait also counts towards the processing duration.

 

  • ExecutableProcessor: This is the framework's main control processor, responsible for processing all ExecutableDirectors.  You only need one instance of this and processing starts by calling member processDirectors().  The ExecutableProcessor listens for Stop, Pause, and Resume events, acting accordingly on the ExecutableDirectors.  Although not a member property, processDirectors() takes a waitTime as a parameter which acts the same way as waitTime on the ExecutableDirector, except the wait is between Directors not Executables.

You select the ExecutableDirector(s) you want and add them to the ExecutableProcessor.  Thus you can mix-and-match the testing you want.  For example, you could load a Reset Executable into a ExecutableDirector, followed by a Measure Executable into a ContinousDirector.  This would then reset the instrument and continuously perform a measurement.

 

You should have no need to create an alternative ExecutableProcessor but you may want a different ExecutableDirector.  Create this as a subclass of ExecutableDirector and implement shouldContinue() (return true if processing of Executables should occur again) and if necessary initialise() if the ExecutableDirector needs any setup (for example, the TimedDirector sets its startMilliseconds property in initialise() so it can determine when the duration has elapsed.)

 

Note that a Pause event will be acted upon but it will timeout after 60 seconds regardless of whether a Resume event is raised. This is to prevent Instruments just 'sitting there' and the pause event is not intended for long term interrupt of Executable Processing.

 

Processing Loop

image

The flow diagram above shows the high-level processing when processDirectors() is called on ExecutableProcessor.  This is all under the control of the framework of course, you just need to instantiate the necessary ExecutableDirectors and Exectubles.  Note that ExecutableDirectors can finish independently of each other and are ignored in any subsequent run through.  For example, in the above image, if ExecDirector1 was a TimedDirector of 1 minute; ExecDirector2 was a ContinuousDirector; and ExecDirector3 was a single-shot Director (ExecutableDirector instance) then:

* All will be processed in the first run through

* In the second run through, ExecDirector3 will return false for shouldContinue() so won't run anymore

* In the third and subsequent run throughs up until 1 elapsed minute, ExecDirector2 and ExecDirector3 will run;

* In runs after 1 minute, only ExecDirector3 will run, and will continue to do so until told to stop.

 

So what happens when an Executable is processed?

 

Write Executable

image

 

  1. Pre Exec Callout: run any Executable specific code before the Driver runs the command.
  2. Update Settings: add any new ExecutableSettings to the Driver, which will map them to DriverSettings
  3. Initialise: tell the Driver to create a session to the Instrument if one doesn't already exist (they are re-used once established)
  4. Commit: send any unprocessed DriverSettings to the Instrument
  5. Execute Write Query: send the command to the Instrument
  6. Post Exec Callout: run any Executable specific code after the Driver runs the command.

 

The Pre-Exec Callout() and Post-Exec Callout() can be overridden in your own Driver if something must be done before/after the query is sent.  For example, in Post-Exec Callout the Reset Executable, tells the Driver to reset all its DriverSettings so they will be reapplied before the next Exectuable runs.

 

Read Executable

image

 

The lead-in is the same as a WriteExecutable and the additional steps are:

  1. Exec Write Read Query: sends the command to the Instrument and reads a result.  Results are issued for the Executable and the Parameters as applicable.  See the Documentation tab on the member for details on how the result is parsed into constituent elements.
  2. Write Result: saves the unformatted Instrument response for later processing
  3. Write Param Vals: saves the unformatted Parameter responses for later processing
  4. Post Result: adds a result message on the Notification Queue with the Executable set as message data.  The test application should read this message and arrange for the result to be processed as required - not forgetting that results may be stored in the parameters if used.

 

Examples

Example usage of the framework is provided so that you can use these as a basis of your own test applications but also get a better idea of how the framework actually works.  All examples are in folder "HAF Examples".

 

The examples are provided in an order of increasing complexity and show different Executables and ExecutableDirectors as well as the use of Events and Notifiers for result handling.  The underlying test application follows the same structure (which could be deemed 'overkill' for the simplest example!) and is a good starting point for your own test applications.

 

They make use of the Drivers found in namespace "Z_Implementation".  If you're lucky enough to have the same instruments as me, then you're good to go; otherwise, to run these with your own instruments you will need to create your own Drivers and make the necessary changes to the example implementations.  In some cases it may be as simple as ensuring that the VI Map To Driver in class ResourceEnumerator is modified and that you have followed the implementation pattern for the existing instruments.

 

1-Instrument Identification

This example enumerates any instruments connected to the PC running LabView NXG and presents the list to the user.  Selecting an instrument, by name, and pressing 'Get Id' will return the instrument identity.

 

This is accomplished using the Driver associated to the selected name, the Identity Executable and an ExecutableDirector (one-time execution.)  Results are provided on the Messages queue for handling and displaying on the UI.

 

If you use a Serial device, e.g. Arduino, a sample sketch is provided that will respond correctly to the commands the framework sends it.

 

2-Take Measurement

This example enumerates all instruments connected to the PC, but the user should select a DMM - Keithley DMM6500 using my instruments - as the example 'measures' a selected function.  The UI allows selection of a function that the DMM knows about, e.g. DC Voltage, AC Voltage, Current, Resistance, Frequency etc.  It also allows the selection of parameters (Buffer Elements for the DMM6500) that are passed along with the command.

 

You should set up a test circuit and connect the DMM to it according to the function that will run.

 

When ready, press 'Measure' and the DMM will attempt to take the correct measurement and display the result, including the results of any parameters also selected.  The DMM identity is also returned.

 

This uses the Identity Executable; the Measure Executable configured with the selected function and parameters; the User Defined Write Executable to create a buffer which the DMM needs (this Executable allows you to provide a hand-crafted SCPI command to be executed); and an ExecutableDirector.  Results are provided on the Messages queue for handling and displaying on the UI.

 

3-Generate Voltage

This example makes use of a PSU instrument to generate a voltage and a DMM instrument to measure that voltage (in the specific case, a Rohde & Schwarz HMC8043 and a Keithley DMM6500).  Select the instruments correctly, enter a Voltage (in mV) and click on Generate.

 

You will need to connect the PSU and DMM to a test circuit for this to work.

 

This uses the Identity Executable; the Voltage Executable; the Measure Executable configured with the Voltage function and no additional parameters; and two ExecutableDirector instances - one for the identities and one for the generation and measure.  Results are provided on the Messages queue for handling and displaying on the UI.

 

4-Waveform Measurement

This example makes use of a DMM instrument to continually take measurements, displaying the results on a Waveform graph.  It will run indefinitely, until 'Stop' is pressed.

 

You will need to connect the DMM to a suitable test circuit for the function you select.  For example, I connected the DMM to a potentiometer to measure the change in resistance as the pot was adjusted.

 

The example responds to the Pause and Resume events.

 

This uses the Identity Executable; the Measure Executable (no parameters); an ExecutableDirector for the identity; and a ContinuousDirector for the measure.  Results are provided through the Results Notifier because the framework will block the main processing loop whilst it does its work - thus the UI cannot be updated via the previously used Messages queue.

 

5-Generate Stepped Voltage

This example makes use of a PSU to generate a voltage and a DMM to measure the voltage.  The PSU is directed to output a voltage in steps, from a start value to an end value in increments.  The DMM measures every step change and the result is displayed on a waveform.

 

You will need to connect the PSU and DMM to a suitable test circuit.  For example, a simple circuit is to provide voltage across a resistor and connect the DMM across the resistor.

 

This example also responds to the Pause and Resume events.

 

This uses the Identity Executable; the Voltage Executable for the voltage generation; the measure Executable configured for Voltage measurement; an ExecutableDirector for the identities and a RepeatingDirector for the generate and measurement.  It demonstrates the use of the Voltage executable with an increment which changes the voltage-to-be-generated to the next value after every execution.  The RepeatingDirector is configured to ensure that it runs the Generate executable until the End Voltage is reached. Results are provided through the Results Notifier because the framework will block the main processing loop whilst it does its work - thus the UI cannot be updated via the previously used Messages queue.

 

Summary

Whilst not particularly complicated, it's reasonably difficult to document clearly what happens so I hope the above is clear enough.  It is highly recommended that you follow through one of the existing examples to see how it works.  These examples also form a template for your own test application so that it deals with events and notifications in a well-controlled and performant manner.

 

I'm open for collaboration on extending the framework, particularly with new Drivers for instruments I don't own.  I can already see there will be benefit in turning some of the example code into framework code for re-use and that is likely to evolve as I create test application for future projects.

 

Any questions or problems, please comment below and I will endeavour to answer.  Happy testing...

 

Links

LabVIEW NXG Community Edition: Post 1 - Review

LabVIEW NXG Community Edition: Post 2 - Hardware Abstraction Framework  (this post)

LabVIEW NXG Community Edition: Post 3 - Unit Testing Framework

  • Sign in to reply

Top Comments

  • genebren
    genebren over 6 years ago +1
    Wow! Very interesting stuff. I have used some of the LabVIEW product is the past (LABwindows - C coding framework) to write test/burn-in programs to exercise consumer based electronic products that I designed…
Parents
  • genebren
    genebren over 6 years ago

    Wow! Very interesting stuff.  I have used some of the LabVIEW product is the past (LABwindows - C coding framework) to write test/burn-in programs to exercise consumer based electronic products that I designed (hardware/software).  This looks so much easier.  At one time I was working on a LabFIEW clone package for my own line of test and measurement equipment.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 6 years ago

    Wow! Very interesting stuff.  I have used some of the LabVIEW product is the past (LABwindows - C coding framework) to write test/burn-in programs to exercise consumer based electronic products that I designed (hardware/software).  This looks so much easier.  At one time I was working on a LabFIEW clone package for my own line of test and measurement equipment.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Andrew J
    Andrew J over 6 years ago in reply to genebren

    Thanks Gene, I'm hoping it's going to be useful for testing and characterisation particularly as data can be exported and compared.