Test & Tools
  • Technologies
  • More
Test & Tools
Blog Low-cost Vector Network Analyzer: NanoVNA-H4 Unboxing
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 22 Jun 2024 9:36 PM Date Created
  • Views 9405 views
  • Likes 12 likes
  • Comments 9 comments
  • NanoVNA-H4
  • VNA calibration standards
  • nanovna
  • vector network analyzer
  • NanoVNA H4
  • vna
Related
Recommended

Low-cost Vector Network Analyzer: NanoVNA-H4 Unboxing

shabaz
shabaz
22 Jun 2024


I recently needed a VNA, and went with one called NanoVNA-H4. This short blog merely contains an un-boxing.

If you’re interested in finding out what VNAs are used for, check out the earlier blog post:  Vector Network Analyzer (VNA): A Practical Getting-Started Guide for the General Reader  

There are several versions of NanoVNA. The version I went for isn’t the best, it just happens to be the one I wanted to use for particular needs, and is pretty low-cost (about £45). Although it is stated for operation up to 1.5 GHz, really it only operates in its sweet-spot below 300 MHz. If you need a VNA for a higher frequency range than 300 MHz, this product is probably not worth getting, because apparently its performance is not very good at all beyond 300 MHz. This is fine for my needs as mentioned; I have a higher-frequency VNA. One VNA probably isn’t enough, since all the low-cost ones have various compromises.

It comes in a sturdy box. The packaging internally is almost as nice as high-end smartphone packaging.

image

There’s lots in the box. There are a couple of USB cables and an instruction sheet containing the details of the menu system (there are a lot of menu pages!), and a wrist-strap with a guitar pick that is extremely useful for tapping on the screen to configure the instrument. As well as a couple of low-cost SMA cables, there is also an SMA Male calibration kit. To be honest, most of the accessories are not worthwhile, apart from the wrist-strap. The SMA calibration kit is OK, but you’ll want to upgrade that at some point. Same with the SMA cables.

The USB cables are junk; I could not plug them in, they felt incorrectly tight. It’s best to throw them away and use your own USB-C cable.

As for the instrument itself; I was surprised that the screen is of quite decent quality. It is visible from most angles, which I had not expected.

image

The case is plastic, held together with four screws on the underside. It’s a little basic, but the device is so low-cost, it is to be expected.

The photo here shows the two SMA connectors (it’s a two-port VNA), and the USB-C socket at the bottom.

image

The top edge contains the wrist-strap hole, and a left/right jog-wheel which is pushed inward to enter the menu and to click on items, and a slide-switch for power (there is an internal rechargeable battery).

image

Some info on the rear panel:

image

As mentioned, the display is surprisingly good. Not top quality, but better than expected for the price. It’s also of a decent size. I had expected to need to use a PC application to drive the instrument, but the NanoVNA-H4 is actually fairly usable directly from the built-in display, even without teenager-grade eyesight.

This default display is a little busy; not a fan of the multiple overlaid charts! I intend on switching off everything and defaulting to just a Smith Chart display if I can.

image

I had been dreading that the user menu (menu structure PDF downloadable below) would be very awkward to control with the jog-wheel method, but it’s not bad at all. Plus, bonus, the guitar-pick on the display makes everything very quick to select if you don’t wish to use the jog-wheel.

image

As optional extras, I purchased two better-quality cables (about £7 each from the same store) because a VNA requires that. Also, I purchased a ‘test kit’ which consists of a PCB, some mounting hardware, two 50-ohm surface-mount resistors, four SMA connectors and two strips of pin sockets. I think the aim of this test kit is to be able to solder in a load of the pin sockets, and then you can push in components like capacitors, inductors etc.

image

The top side of the test board is hard to follow, but that’s not a big deal because it will be covered with pin headers anyway.

image

Fortunately it’s clear to consult the layout from the underside.

image

I have not used the NanoVNA-H4 yet, so I can’t comment on how good/bad it is.

Thanks for reading!

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 2 years ago +1
    A nice review. I was impressed with my Nano VNA - an earlier model I think. To be honest the variations of NanoVNA are a bit confusing! Does your R&S FPC1500 not outperform this at all frequency ranges…
  • shabaz
    shabaz over 2 years ago in reply to aswinvenu +1
    That would be good to see! The LibreVNA is in that unfortunate space where it's too pricey for being a beginner VNA, and probably not mature enough to be purchased by orgs. It looks great but I think mainly…
Parents
  • shabaz
    shabaz over 2 years ago

    Looks like there are (at least) two different software sources which can be used!

    One is in a github repo owned by a user hugen79, and the other is in a repo owned by user DiSlord.

    It's actually very hard to tell which of these two are installed on the device. I had to search the source code!

    In the NanoVNA device, tapping on Device->Version will display some info. 

    Mine contained the text:

    Copyright NanoVNA.com 
    based on  @DiSlord @edy555 ...source
    Licensed under GPL.

    According to a search of the source code, that's firmware built from the hugen79 repo content.

    If it were from the DiSlord repo, then I ought to see the following text:

    Copyright @DiSlord (based on @edy555 source)
    Licensed under GPL.

    So, similar-ish messages but subtly different! Anyway, I've concluded that the device came with hugen79 firmware, and in my case it's already at the current latest version.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 2 years ago

    Looks like there are (at least) two different software sources which can be used!

    One is in a github repo owned by a user hugen79, and the other is in a repo owned by user DiSlord.

    It's actually very hard to tell which of these two are installed on the device. I had to search the source code!

    In the NanoVNA device, tapping on Device->Version will display some info. 

    Mine contained the text:

    Copyright NanoVNA.com 
    based on  @DiSlord @edy555 ...source
    Licensed under GPL.

    According to a search of the source code, that's firmware built from the hugen79 repo content.

    If it were from the DiSlord repo, then I ought to see the following text:

    Copyright @DiSlord (based on @edy555 source)
    Licensed under GPL.

    So, similar-ish messages but subtly different! Anyway, I've concluded that the device came with hugen79 firmware, and in my case it's already at the current latest version.