Test & Tools
  • Technologies
  • More
Test & Tools
Blog mini project: PICO-PI programmable Lab Switch - 1a: understand UART and Interrupts
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 16 Oct 2022 6:44 PM Date Created
  • Views 3234 views
  • Likes 9 likes
  • Comments 0 comments
  • pico_freertos_smp
  • pico_freertos_scpi_switch
  • pico
Related
Recommended

mini project: PICO-PI programmable Lab Switch - 1a: understand UART and Interrupts

Jan Cumps
Jan Cumps
16 Oct 2022

In this series, I design a programmable lab switch based on RP2040, that can turn a set of signals or supplies on or off. Over USB. SCPI compatible.
In this post: understand RP2040 UART with interrupts.

image
image source: a similar exercise on the Infinion PSoC 6.

Understand RP2040 UART and Interrupts

The RP2040 FreeRTOS port doesn't include wrappers for the peripherals. It's not uncommon - a port is good if it supports running the RTOS. Making the peripherals RTOS aware isn't needed. We can do that ourselves.
A few things to consider:

  • protect UART resources from multi-task access, where needed
  • write tasks for receiving data and incoming traffic interrupt handling. Maybe for sending data?

To do this, I first need to understand how the UARTs of the RP2040 work. There's an excellent example: uart_advanced. The example uses interrupts for both receive and send, but I'm looking for receive only.

Review pico-examples UART interrupt example

Enable RX Interrupt

This is straightforward:

    // Turn off FIFO's - we want to do this character by character
    uart_set_fifo_enabled(UART_ID, false);

    // Set up a RX interrupt
    // We need to set up the handler first
    // Select correct interrupt for the UART we are using
    int UART_IRQ = UART_ID == uart0 ? UART0_IRQ : UART1_IRQ;

    // And set up and enable the interrupt handlers
    irq_set_exclusive_handler(UART_IRQ, on_uart_rx);
    irq_set_enabled(UART_IRQ, true);

    // Now enable the UART to send interrupts - RX only
    uart_set_irq_enables(UART_ID, true, false);

    // OK, all set up.

Single-char is set, and that matches what I'll want to do: I want to shoot each character to the SCPI library later.
Then, the interrupt is registered and activated.

Handle RX Interrupt

Again simple:

// RX interrupt handler
void on_uart_rx() {
    while (uart_is_readable(UART_ID)) {
        uint8_t ch = uart_getc(UART_ID);
        // TODO: handle
    }
}

The handle retrieves any available character from the UART. I haven't reviewed RP2040 SDK in depth, but it seems you don't have to clear the interrupt ...

Port to FreeRTOS

This will not be hard to translate to RTOS:

  • make the "UART read task" wait on a direct task message
  • in the "UART RX interrupt handler", notify the read task, so that it wakes up.
  • in the "UART read task", get the character from UART, send it to the business logic (SCPI parser),
  • go back to start

In the next blog, I'll implement most of this. The business logic will not be there yet. I'll toggle the LED whenever you type a 'b' character ...

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Show all blog posts