Test & Tools
  • Technologies
  • More
Test & Tools
Blog Mitutoyo 530-122 Vernier Caliper
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: javagoza
  • Date Created: 8 Mar 2022 10:58 PM Date Created
  • Views 4849 views
  • Likes 14 likes
  • Comments 8 comments
  • vernier caliper
  • bluebot
  • caliper
Related
Recommended

Mitutoyo 530-122 Vernier Caliper

javagoza
javagoza
8 Mar 2022
Mitutoyo 530-122 Vernier Caliper

I was selected as one of the winners for the giveaway in the Industrial Robotics quiz community.element14.com/.../industrial-robotics-quiz

The giveaway is a Vernier Caliper and it arrived at my office today. As soon as I got home I started trying it out.

It is a Mitutoyo 530-122 Vernier Caliper. It is a high accuracy model: ±0.03mm. It has metric scale

Unboxing

It comes inside a cardboard box.

image

With a plastic cover and instructions for use. Use cases and how to read the measurements with the maximum precision of the tool

image

Can measure outside and inside diameter (OD and ID), depth, and steps. Range 0 - 150mm

image

Roadtest

I'm testing it by making a 3D model of the blue boogie bot from element14 although I don't need that much precision for this task. It's really comfortable.
It is not a light caliber, the weight is noticeable and it is appreciated when having it in your hand. It is very well balanced and handles very well with the right hand.

It is very simple, easy to read, I can do the readings well without the need for close-up glasses or a magnifying glass.

The numbers and lines have very good definition, are very easy to read and have a sensational contrast. The ruled surface is glare-free and looks good from any angle.

It has a metric scale which is what I am used to using. It also has a very useful clamping screw for forgetful people like me.

image

image

Thank you for this excellent gift, it will always be close at hand on the desk.

  • Sign in to reply
Parents
  • shabaz
    shabaz over 4 years ago

    Hi Enrique,

    You were an engineer before, but now you're visibly an engineer to even strangers who see it on your desk!

    Very nice instrument. 

    By coincidence, I bought this a few days ago.. it's only a toy, it's actually tiny, the length of a pen, with perhaps 1/4 mm accuracy if I stare at the lines really hard : ) and the depth end of it is totally bent and unusable : ) but it was less than £1 - I'll use it to teach some young family members how to read the vernier marking, it will be a very interesting concept to them I think.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 4 years ago in reply to shabaz

    I also have one of those cheap plastic ones. It is impossible to use it with one hand or even with two, but it has an imperial scale, which is something that is good for me to have on hand to get a visual idea of the sizes.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • javagoza
    javagoza over 4 years ago in reply to shabaz

    I also have one of those cheap plastic ones. It is impossible to use it with one hand or even with two, but it has an imperial scale, which is something that is good for me to have on hand to get a visual idea of the sizes.