Test & Tools
  • Technologies
  • More
Test & Tools
Blog MXO 4 New Feature: Log Frequency Axis Spectrum Analysis!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 11 Aug 2023 8:35 PM Date Created
  • Views 1807 views
  • Likes 13 likes
  • Comments 7 comments
  • spectrum_analyser
  • MXO4
  • MXO 4
  • spectrum analyzer
  • spectrum_analysis
  • rohde & schwarz
  • mxo 4 oscilloscope
  • r&s
  • spectrum_analyzer
  • rohde&schwarz
Related
Recommended

MXO 4 New Feature: Log Frequency Axis Spectrum Analysis!

shabaz
shabaz
11 Aug 2023

Table of Contents

  • Introduction
  • What is it?
  • What does it look like?
  • EMC Pre-Compliance Testing
  • Noise Measurements
  • Notch Filter
  • Band Pass Filter
  • Summary

Introduction

Due to customer requests, the MXO 4 now supports a fully log-log spectrum output display! I was keen to try it out. This ultra-short blog post shows some example screenshots! Or just check out the equally brief (4-minute) video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

What is it?

Most spectrum analyzers display the spectrum with a logarithmic vertical axis (indicating power, or occasionally amplitude), but the horizontal frequency axis is normally linear. While that’s fine for many use-cases, sometimes it is either highly desirable, or required, for that axis to be in log format. One ‘required’ example is for EMC pre-compliance testing.

Some ‘highly desirable’ examples involve audio testing. When examining frequency response, it can be quicker, and more intuitive, to be using a log axis. The MXO 4’s high resolution ADC and integrated high-resolution waveform generator makes it extremely attractive for audio work, and now the log-log spectrum further solidifies such use-cases.

What does it look like?

The screenshot below shows a 1-100 MHz span, and a 10 MHz signal of interest. Normally it would be squashed up on the left, but now it’s in the center. Often detail is squashed at the low frequency end of spectrum traces, but now all the low-frequency content is easier to visually resolve.
High frequency content is sometimes spaced too far apart for easy visualization, so again the log frequency feature comes to the rescue here.

image

EMC Pre-Compliance Testing

Check out the full written review, or the video review, for more detail. Now, the MXO 4 is getting to be great for this use-case. It still cannot perform limit lines, but there is a workaround; it is possible to graphically annotate lines and then save that as a configuration that can be recalled whenever particular EMC tests are needed.

image

Noise Measurements

Some output is way easier to recognize on a log axis. An example is pink noise, which should look like a straight line on such an axis. The noise incidentally was generated using the MXO 4’s in-built waveform generator.

image

Notch Filter

Here’s a use-case where not only would the signal of interest normally be squashed on the left side in a normal 20 Hz to 20 kHz span trace, but it would also be very hard to spot without spectrum analysis capabilities. The screenshot shows a low-level (just a few millivolts) 500 Hz tone in green. It goes into a DSP, and egresses as shown in the yellow trace. It is very low-level but clearly visible on the spectrum chart. The DSP happens to implement a notch filter, set to 480 Hz which is extremely close to the tone. The notch is extremely sharp, and therefore the signal passes with little attenuation. The video above shows the effect when the notch filter is tuned to precisely 500 Hz.

This is a scenario that would be impossible to see with most dedicated spectrum analyzer instruments, because of the extremely low frequency. The MXO 4 works great for audio applications, and the video shows that the output is still fast even at the 10 Hz resolution bandwidth that was used.

image

Band Pass Filter

I wanted to build a very sharp speech filter for 300 Hz to 3 kHz. Ordinarily such a filter could be partially tested with a frequency response analyzer (FRA), but out of curiosity I wanted to see if some of the testing could be speeded up with a frequency chirp that was not linearly changing with frequency, but logarithmically. MATLAB was used to create the waveform, and then it was stored into the MXO 4, for recalling whenever such audio testing is desired. It sweeps across 20 Hz to 20 kHz, in 6 seconds, and then repeats indefinitely.

From my perspective the screenshot below revealed a lot, and showed me the shortcomings with the filter. The video contains some more information.

image

Summary

I was really happy to see the Logarithmic Frequency Axis feature arrive in an MXO software update, since I was missing this on other test tools. The feature appears to work well and I’m keen to make a lot more use of it, in particular for some filtering projects for audio and RF purposes.

Thanks for reading/watching.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 3 years ago in reply to michaelkellett +1
    Hi Michael, Glad all is OK, I hope you're back to 100% very soon! It is pretty amazing how much adjustment was needed for the ultra-precise filters! I can imagine BT could afford it! A lot of old…
  • shabaz
    shabaz over 3 years ago in reply to DAB

    Hi DAB,

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 3 years ago

    Very informative, well done.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to michaelkellett

    Hi Michael,

    Glad all is OK, I hope you're back to 100% very soon!

    It is pretty amazing how much adjustment was needed for the ultra-precise filters! I can imagine BT could afford it! 

    A lot of old radio equipment also used very high-end filters where the LC stages were mechanical analogies, these were used at frequencies of 455 kHz or 1.4 MHz were popular, and with a bandwidth of just a few kHz (speech) or hundreds of Hz (i.e. morse).

    image(image source rfcafe)

    Nowadays they can cost £50+ on ebay since occasionally some radios built even in the early 2000's used them, although mostly DSP had already overtaken at that time for the IF frequency).  This one is listed at £150 on ebay and the seller has already sold one (possibly at that price!):

    image (image source: ebay)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 3 years ago

    Hello Shabaz, Thanks for the update.

    I'm currently stuck at home resting after having my knee replaced.but much looking forward to playing with the MXO4  log spectrum analysis. Maybe next week.

    Your audio bandpass filter brings back horrible memories of a piece of test equipment we made for BT along while ago. It had a 2kHz 20Hz wide bandpass filter implemeneted by a cascade of 8th order elipptical high pass and low pas filters. Each filter used two quad op amps arranged as pot tuneable gyrator"LC" stages. 16 adjustments in all. When you got good at it you could tune one in under an hour ! But no fancy tools, just sig gen, True RMS meter with digitial read out (Fluke 8050 I think). I might well have traded a leg for an MXO4 at that time.

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to shabaz

    Yes and no. This weekend I'm attending DEF CON. Then when I get back, I have several overdue projects I need to finish. (I don't like doing software updates on instruments mid-project, unless it's to fix a known issue.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>