Test & Tools
  • Technologies
  • More
Test & Tools
Blog OpAmp as Schmitt-trigger
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 25 Jan 2025 6:29 PM Date Created
  • Views 9925 views
  • Likes 16 likes
  • Comments 23 comments
  • art of electronics
  • opamp
  • schmitt-trigger
Related
Recommended

OpAmp as Schmitt-trigger

Jan Cumps
Jan Cumps
25 Jan 2025

A Schmitt-trigger is a circuit that turns a non-perfect digital signal into a clean one. It has 2 main functions:

  • recreate a good fast ramp for signals that have lost their oomph (or never had clean fast edges). 
  • provide a bit of hysteresis, so that signals with significant noise can be restored to proper high and low

There was a recent design of shabaz that uses Schmitt-triggers:  Brush and Large-Area Multi-Meter Probes for PCB Reverse-Engineering: A DIY Approach! . The Art of Electronics (AOE) happens to explain that very circuit. A good excuse to check it out.

image
image source: The Art of Electronics 3rd edition p. 237 - fair use

Schmitt-triggers have a set level where they consider a signal high or low. The main difference with a comparator circuit, is that they also introduce hysteresis. Output will switch when the input reaches a particular level, but it will not switch again until the input has dropped below a different, lower, input level. An engineer will define the two levels so, that the noise on the input will never cause a state flip.

image

image source: TI Application Brief Understanding Schmitt Triggers - fair use

For this post, I'm recreating the AOE design based on an OpAmp (identical to Shabaz', just with different levels and operating voltage), The only change I made is the desired voltage level. I brought that down from  5 V to approx. 3.3 V, because that's in the range of my signal generator. I use the very common UA741 in this design, because I have a through-hole one. In a real design, you'd probably use a more modern one that can work on lower voltages, and can drive its output to the rails. And is faster (see jc2048 ' comment).

This is an inverting design. The output drives low when the input is high.

The circuit

It's virtually the same as the AOE design. But R1 is 20K instead of 10K, OpAmp voltage 10 V. 

image


image
images: the actual circuit that I set up on a breadboard.

Results

Test with an input that is noisy, and migrates to both upper and lower levels multiple times:

image
image source: the design successfully cleans up a noisy test signal from my waveform generator

The yellow trace is the input. I have chosen a signal that is noisy on both low and high level. I've set it so that it has glitches on both sides of the hysteresis range. The magenta trace is the output. It's a nice "digital" signal, with fast edges and little noise. Because I used the imperfect UA741, signal does not reach ground or VCC. The Blue trace is the set point. You can clearly see that the output level influences the comparison point.

Operation: this is an OpAmp with positive feedback. R3 feeds the output back to the + input. That "escalates" the OpAmp. When the input crosses the set point, it immediately goes to the rail voltage (or as close as it can get to it).

R3 also has another effect: It influences the set point, because it is either connected to the positive or ground rail. When output is low, R3 will pull the set point down a little. When output is high, it will pull it up somewhat. That's what generates the hysteresis. Set point and hysteresis width are function of the 3 resistors values (and by how close the OpAmps can drive to the rails).

  • Sign in to reply
Parents
  • jc2048
    jc2048 over 1 year ago

    I've never owned a copy of tAoE. Perhaps e14 could offer one or two as a prize in a P14 competition.

    Good blog, but...

    "it immediately goes to the rail voltage"

    not with a 741 it doesn't. The slew rate is less than a volt per microsecond, and that's slower than the recommended input transition rate even for a slow logic like HCT. In practice it would probably happily work anyway (for a personal project), but there's a danger the input might oscillate during the transition.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to jc2048

    Yes, it's too slow for real world applications:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to jc2048

    I thought this was interesting: I tried to reverse-engineer an old circuit (1980's) and noticed an unusual application of op-amp comparators: being used for RS-232! As you say, this was HC logic interfacing era. 

    I didn't fully trace out the circuit since I didn't need the full detail, so not sure if they had added hysteresis. Plus I'm not too sure about that chain of diodes and resistors, I could have made a mistake. I only reverse-engineered just enough to realize that they were using them for digital level conversion for the RS-232 outputs. I was thinking why, but then realized chips like MAX202 were probably way too new back then. Plus, the particular customers would have wanted second-sourced parts to be available, which would have been easier with these op-amps.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 1 year ago in reply to shabaz

    Not seen that before. MC1488 and MC1489 were the standard IC parts for RS232 line driver/receiver back then, until Maxim came up with the one with the switched-capacitor converters to derive the line voltages on-chip from the +5V.

    The 4049 input is using the static protection as a clamp to each rail, which isn't really good practice, but would work ok with a 10k current-limiting resistor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 1 year ago in reply to jc2048

    Hehe I think the MAX202 in PDIP package was amongst the first ICs I ever used (well, amongst the first dozen perhaps; 741 or 555 must have been the actual first IC I used). I made myself a 68HC11 dev-board, and used MAX202 for the comms. 

    Regarding the 4049, I believe the circuit is doing things like wake-on-RS-232-activity and needed to conserve power (this is portable equipment) so that may have driven them to using it on the input side.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to jc2048

    change of plan. I set up the circuit with the 741 anyway . My last LM324 is defect.

    1: Falling edge

    image

    2: Rising edge

    image

    3: recovery from negative rail: I didn't find a good way to do that (edit: see next comment below). Looks like it doesn't struggle with that. Most likely either my technique or understanding is off:

    image

    4: it definitely looses the plot with fast cross-overs. This signal spans the hysteresis at each edge:

    image

    5: maximum frequency where a triangle is correctly processed: around 10 kHz

    image

    I tried to place that triangle so that it results in a 50% duty cycle. Faster than that, and there's no flat area in the output left. At 23 - 24 kHz it loses the tracking completely.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Jan Cumps

     jc2048 is this the recovery you are referring to?

    Negative rail:

    image

    Positive rail:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Jan Cumps

     jc2048 is this the recovery you are referring to?

    Negative rail:

    image

    Positive rail:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jc2048
    jc2048 over 1 year ago in reply to Jan Cumps

    "... is this the recovery you are referring to?"

    Yes. Worse than just the delay, which may not matter too much given how pedestrian the 741 output is, is that it's unbalanced - it behaves differently coming away from the +ve rail to the other one. That will be common with bipolar op amps because of the way the output stages were designed. As you've already discovered, that then messes up (wrt the mark/space ratio) slicing a fast waveform.

    If you look at the datasheet for an old, bipolar, commodity comparator like a LM393, the outputs move after about 250ns (depends on the amount of overdrive at the input), balanced either way, and the transition is much faster, even though the level translation to the logic is o/c and a pull-up.