Test & Tools
  • Technologies
  • More
Test & Tools
Blog Pomona Insulation Piercing Clips
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 28 Jul 2019 11:32 PM Date Created
  • Views 3984 views
  • Likes 12 likes
  • Comments 16 comments
  • piercing_clip_connector
  • insulation piercing
  • banana plug
  • wire_piercing
  • pomona
Related
Recommended

Pomona Insulation Piercing Clips

shabaz
shabaz
28 Jul 2019

A friend gave me a couple of Pomona Insulation Piercing ClipsPomona Insulation Piercing Clips which I thought were pretty neat. Apparently they are quite popular with the automotive repair/test crowd.

The clips were something I had not seen before, so thought maybe it would be good to share some pics/video if anyone else has not seen these before either.

 

In brief, they can connect to banana plugs (there is also a version of clip compatible with multimeter test leadsversion of clip compatible with multimeter test leads) and then the other end can be hooked over an insulated wire, and by turning the red or black end of the clip, a sharp needle pierces the insulation for making contact with the conductor.

 

The damage is fairly minimal, and the repair depends of course on the industry/application and environment. It may need a small insulation repair, since the insulation it is compromised.

 

image

 

Here's a close-up showing the insulation being pierced:

image

They feel well-made, and I like the ergonomics too. The pointy nose is nice too for pushing into a nest of wires. I get the feeling it would be very easy to use this one-handed, by using the thumb and index finger to push back on the lever, while pushing into the wires, and hooking it on. After that, the lever can be released and then the black or red end of the clip needs screwing in (possible one-handed, but depends on if it will disturb the wire or not - you may want to do that part two-handed).

 

Here's a 7-minute video showing me using it with a few wires (the clip is designed for 14-22AWG wires, but it seems fine with thinner wires too).

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

There are versions for long-distance probing/poking image (up to 24 inch!):

image

Thanks for reading!

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 7 years ago in reply to jw0752 +7
    Aliexpress to the rescue ! https://www.aliexpress.com/wholesale?catId=0&initiative_id=AS_20190729000340&SearchText=insulation+piercing+test+clip MK
  • jw0752
    jw0752 over 7 years ago +6
    Hi Shabaz, They looked really useful until I saw the price. I think my application will need to be a bit more profitable before I invest. John
  • shabaz
    shabaz over 7 years ago in reply to jw0752 +6
    Hi John! Most Pomona stuff is pricey here, but this one looks expensive universally. I just noticed Fluke have the identical product on their price-book too, at an even more unmentionable price!
Parents
  • balearicdynamics
    balearicdynamics over 7 years ago

    Hey Shabaz! This is something new for me too. I never saw this kind of probes-connectors. Seems almost complex to build but also seems very efficient. The piercing approach of these probes resembles me the 80's network coaxial cables. It was possible to connect computer converters like network to centronics or serial using the tap-drill method. But I never saw something like this for decades.

     

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to balearicdynamics

    Hi Enrico!

    Very interesting.. I've never seen these vampire taps for networks before, but had heard of them. You're right, this probe seems a similar idea!

    The first place I worked had a ton of serial interfaced terminals (like VT100) but I don't know how the connection got to the desks. They were phasing it all out for PCs, but lots of work was still done on the terminals (like inventory, etc).

    The serial terminals went to a VAX machine. I remember using a word processor called Lex.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    Lex is a famous editor Shabaz! I remember it too. These vampires are really Jurassic IT. These were used with the 1-inch diameter IBM coax cable. I saw them on AS400 and in the first data center where I worked but whey was using IBM360 10 base 5 networks, data tapes and punched cards to schedule the jobs with JCL (The IBM Job Control Language).In that period terminals was Hazeltine and VT100 arrived some year later, with the 3200Kb modems and BBS, at least in Italy. This system was very efficient because it was possible to make a connection everywhere there was one of these main cables around.

     

    Some more details can be found hereç https://en.wikipedia.org/wiki/10BASE5

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to shabaz

    Lex is a famous editor Shabaz! I remember it too. These vampires are really Jurassic IT. These were used with the 1-inch diameter IBM coax cable. I saw them on AS400 and in the first data center where I worked but whey was using IBM360 10 base 5 networks, data tapes and punched cards to schedule the jobs with JCL (The IBM Job Control Language).In that period terminals was Hazeltine and VT100 arrived some year later, with the 3200Kb modems and BBS, at least in Italy. This system was very efficient because it was possible to make a connection everywhere there was one of these main cables around.

     

    Some more details can be found hereç https://en.wikipedia.org/wiki/10BASE5

    • Cancel
    • Vote Up +4 Vote Down