• Products and Partners
    Products and Partners
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
Test & Tools
  • Technologies
  • More
Test & Tools
Blog Programmable Electronic Load - LCD Display
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 23 Mar 2018 1:05 PM Date Created
  • Views 1726 views
  • Likes 6 likes
  • Comments 4 comments
  • metrology
  • lcd
  • boosterpack
  • rtos
  • msp432
  • ti_rtos
  • launchpad
  • laboratory
  • instrument
Related
Recommended

Programmable Electronic Load - LCD Display

Jan Cumps
Jan Cumps
23 Mar 2018

This blog focuses on the LCD for the electronic load that Robert Peter Oakes, jc2048 and Jan Cumps are designing.

 

image

The post shows what's displayed on the screen and how that info is retrieved..

 

The Layout

 

The LCD shows the mode, status, set and measured values.

image

 

 

 

The Display

 

The optional display is a boosterpack, Product LinkProduct Link. The load doesn’t need the display to operate.

It was added for two reasons: it served as a debug tool at the beginning of the project when the SCPI commands weren,t implemented.

And it’s a test case to ensure that presentation layer is independent of instrument code.

Both SCPI module and display use the load’s api to control and query the app.

 

The boosterpack has a monochrome 96 x 96 graphic LCD with reflective back plane.

That display was used on early Nokia mobile phones and is made by SHARP.

 

 

 

 

image

 

The Firmware

 

The firmware uses the drivers that come with  SimpleLink TI-RTOS. The eload uses standard functionality only.


The code to manage the screen is very easy. A single RTOS task initialises the LCD, then refreshes all the content once per second.

That’s it.

 

Initialise

This code runs at the startup of the device. It initialises the display and shows a welcome message

 

void *threadDisplay(void *arg0);
#define THREAD_PRIORITY_DISPLAY 10
#define THREAD_SLEEP_DISPLAY 1
#define THREAD_STACK_DISPLAY 2048

 

 

    priParam.sched_priority = THREAD_PRIORITY_DISPLAY;
    pthread_attr_setschedparam(&attrs, &priParam);
    retc |= pthread_attr_setstacksize(&attrs, THREAD_STACK_DISPLAY);
    if (retc != 0) {
        /* pthread_attr_setstacksize() failed */
        while (1);
    }
    retc = pthread_create(&thread, &attrs, threadDisplay, NULL);
    if (retc != 0) {
        /* pthread_create() failed */
        while (1);
    }

 

 

void *threadDisplay(void *arg0)
{
    uint32_t i;
    char formatString[12];
    Display_init();
    /* Initialize display and try to open LCD type of display. */
    Display_Params params;
    Display_Params_init(&params);
    params.lineClearMode = DISPLAY_CLEAR_BOTH;
//    Display_Handle hLcd = Display_open(Display_Type_LCD | Display_Type_GRLIB, &params);
    Display_Handle hLcd = Display_open(Display_Type_LCD, &params);
    if (!hLcd) {
        return NULL; // we didn't get a display handle. Check if the following is defined: BOARD_DISPLAY_USE_LCD
    }
    Graphics_Context *context = DisplayExt_getGraphicsContext(hLcd);
    GrContextForegroundSet(context, ClrBlack);
    GrContextBackgroundSet(context, ClrWhite);


    GrClearDisplay(context);
    GrContextFontSet(context, &g_sFontCmss12);




    GrStringDraw(context, "The Breadboard", -1, 10, 15, 0);
    GrStringDraw(context, "Electronic Load", -1, 15, 30, 0);
    GrStringDraw(context, "Copyright Free", -1, 13, 45, 0);
    GrStringDraw(context, "Version 0", -1, 22, 60, 0);


    GrFlush(context);
    int8_t cMode;


    float fVoltage = 0.0f;
    float fCurrent = 0.0f;

 

Main Schedule

The loop is run once per second. It displays the constant mode, the current, voltage, power and resistance.

 

    while (1) {
        sleep(THREAD_SLEEP_DISPLAY);
        cMode = eloadGetChar();
        fVoltage = eloadGetVoltageDC();
        fCurrent = eloadGetCurrentDC();
        GrClearDisplay(context);
        GrContextFontSet(context, &g_sFontCmss12);

        sprintf(formatString, "mode: %c %02.4f\0", cMode, eloadGetSetpoint());
        GrContextFontSet(context, &g_sFontFixed6x8);
        GrStringDraw(context, (int8_t *)formatString, -1, 4, 0, 0);

        i = 0;
        sprintf(formatString, "I: %02.4f\0", fCurrent);
        GrContextFontSet(context, &g_sFontFixed6x8);
        GrStringDraw(context, (int8_t *)formatString, -1, 4, (15 + 12*i), 0);

        i = 1;
        sprintf(formatString, "V: %02.4f\0", fVoltage);
        GrContextFontSet(context, &g_sFontFixed6x8);
        GrStringDraw(context, (int8_t *)formatString, -1, 4, (15 + 12*i), 0);

        i = 2;
        sprintf(formatString, "P: %02.4f\0", fVoltage * fCurrent);
        GrContextFontSet(context, &g_sFontFixed6x8);
        GrStringDraw(context, (int8_t *)formatString, -1, 4, (15 + 12*i), 0);

        i = 3;
        if (fCurrent> 0.0f) {
            sprintf(formatString, "R: %02.4f\0", fVoltage / fCurrent);
        } else {
            sprintf( formatString, "R: --.--");
        }
        GrContextFontSet(context, &g_sFontFixed6x8);
        GrStringDraw(context, (int8_t *)formatString, -1, 4, (15 + 12*i), 0);

        i = 4;
        sprintf(formatString, "Input: O%s\0", eloadInputEnabled()? "n " : "ff");
        GrContextFontSet(context, &g_sFontFixed6x8);
        GrStringDraw(context, (int8_t *)formatString, -1, 4, (15 + 12*i), 0);


        GrFlush(context);


    }
}

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +2
    Very nice update on the project. From the LCD display, it looks like you are getting some pretty good results with your load. Keep up the good work! Gene
  • Jan Cumps
    Jan Cumps over 8 years ago +2
    Blog adapted to SimpleLink RTOS. There's no functional changes, just using the new idioms and POSIX API
  • Jan Cumps
    Jan Cumps over 7 years ago +1
    I'm changing the LCD display used in the load. The current one is a 96 x 96 Pixels LCD that's no longer available for purchase. Sharp doesn't produce the LCD anymore. I purchased the boosterpack with the…
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    Blog adapted to SimpleLink RTOS. There's no functional changes, just using the new idioms and POSIX API

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago

    Blog adapted to SimpleLink RTOS. There's no functional changes, just using the new idioms and POSIX API