• Products and Partners
    Products and Partners
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
Test & Tools
  • Technologies
  • More
Test & Tools
Blog Programmable Electronic Load - Measurements Part 1: Control Circuit
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 19 May 2018 11:29 AM Date Created
  • Views 3902 views
  • Likes 5 likes
  • Comments 6 comments
  • opamp
  • control_theory
  • feedback
  • integrator
  • dc_load
Related
Recommended

Programmable Electronic Load - Measurements Part 1: Control Circuit

Jan Cumps
Jan Cumps
19 May 2018

Analog Time !

I've prepared the DC Load to measure the behaviour of the circuit. In this blog series I'll show dynamic aspects of the instrument.

image

The first blog shows the points of interest and some initial teaser measurements. If you want a particular measurement to be done, ask in the comments.

 

 

Test Points

 

I've wired the main points of the control circuit - an opamp integrator:

  • the inputs of the integrator (set point and measured feedback)
  • the output of the integrator
  • the gate of the power mossfet.

image

 

 

This should be enough to get a view into the dynamics of the circuit. In hindsight I could have also captured the inverting input of the integrator but I didn't.

 

First Setup: Square Wave input signal.

 

jc2048 has documented the behaviour using a simulator. One of the exercises was the reaction of the controller circuit on a square wave input.

Programmable Electronic Load: Dynamic Behaviour: Part 1 Overview

 

I've replicated this by passing a pulsed 0.6 V signal to the dc load and try to keep the current to 200 mA.

On the captures below, the

  • yellow signal is the square wave 0.6 V 20 Hz input voltage to the dc load.  It isn't a perfect square because there is output capacitance on supply.
    (I don't have a square wave generator that can be loaded, so I used the TI SWIFTTm Power Module EVM module from the RoadTest I did a while ago and pulsed the output via the EN signal)
  • purple is the TTL 20 Hz signal that I used to pulse that voltage.
  • light blue is the gate voltage to of the mosfet.
  • dark blue is the measured current, taken after the opamp. Inverted because the opamp has a negative gain.

 

image

 

The first capture shows a complete cycle:

image

 

The next one is triggered on the rising edge:

image

 

The last one is triggered on the falling edge:

image

 

That's it for this blog. It's more food for thought than actually analyzing what's happening. I think it shows enough info to start a discussion though.

  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 8 years ago +1
    This is confusing because there is more than one thing that can be considered as an input. That first dynamic-behaviour blog was on the effect of changing the set-point input (ie the current being demanded…
  • Jan Cumps
    Jan Cumps over 8 years ago +1
    Things you do to improve probing:
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    The following is a scenario where current is set to 1.5 A, then the input is turned on:

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago

    The following is a scenario where current is set to 1.5 A, then the input is turned on: