Test & Tools
  • Technologies
  • More
Test & Tools
Blog Silicon Solder Mat
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 6 Feb 2021 4:39 PM Date Created
  • Views 6246 views
  • Likes 14 likes
  • Comments 47 comments
Related
Recommended

Silicon Solder Mat

Jan Cumps
Jan Cumps
6 Feb 2021

I purchased a silicon solder mat today, when I was in the electronics shop to pick up my order.

 

image

 

I use an antistatic mat as a generic work area, and prefer to keep that tidy. That mat can take an accidental touch of a hot iron, but it's not intended for that.

 

The silicon solder mat (from Velleman - Buy Belgian!) is heat resistant, up to 500° C.

Flexible and can be cleaned in a kitchen sink. It returns back to its original form.

Total size 45 x 30 cm. Work area without covering anything is approx. 40 * 28. It costed 20 €.

 

One of the biggest advantages for me is that it's easy to pick up and stow away. My lab is used as office, diner table and lab bench, depending on the time of day.

I prefer to have a reasonable clean desk. I remove instruments and projects when I use the desk as home office. And vice versa.

I'll report back in a while how the thing behaves in the real world. If I'm happy with the purchase or regret it.

  • Sign in to reply

Top Comments

  • ntewinkel
    ntewinkel over 5 years ago in reply to Jan Cumps +9
    Jan Cumps wrote: Mine has Velleman printed on it and that is better ! These would actually make great element14 swag. It's already the right colour too... just need some orange printing added. Velleman…
  • 14rhb
    14rhb over 5 years ago +7
    Hi Jan Cumps , I've the same mat, as you already ellude to, they are great for keeping the solder 'mess' in one place and I don't think you'll regret your purchase I bought my one to save me the embarassment…
  • ralphjy
    ralphjy over 5 years ago +7
    I use a smaller one - 35 x 25 cm, somewhat thinner (3.5mm) and without magnets. It works really well and is the perfect size for the type of soldering that I do. It was $8 from Amazon.
Parents
  • ntewinkel
    ntewinkel over 5 years ago

    Those mats are super useful. I didn't find out about those until just a few years ago, and got a not-as-fancy one from the land of online things:

    image

     

    I'm not sure where the tiny mat came from... It might have been a kitchen-aisle item or a dollar store find. It's super thin.

     

    I do also have a letter (A4?) sized one that came with a glue gun.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to ntewinkel

    Mine has Velleman printed on it and that is better !

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tariq.ahmad
    tariq.ahmad over 5 years ago in reply to ntewinkel

    image

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 5 years ago in reply to ntewinkel

    Y'know, I saw these mats and initially thought it may have been simply a gimmick. I guess not?

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to cstanton

    I think that some of the embellishments are a bit of a gimmick, yes.

    The mat itself is useful. Because it protects the work surface, it's easy to clean, keeps dirt and flux / isoprophyl flows contained, and easy to stow away.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 5 years ago in reply to Jan Cumps

    Jan Cumps  wrote:

     

    I think that some of the embellishments are a bit of a gimmick, yes.

    The mat itself is useful. Because it protects the work surface, it's easy to clean, keeps dirt and flux / isoprophyl flows contained, and easy to stow away.

     

    I agree with all of what Jan said!

     

    I don't use the little "screw organizer grid" at all, but the top sections are handy for tossing clipped bits into, and for holding some small parts.

    And the edge keeps things from rolling off the worktop.

     

    Also, the surface texture is very nice - it's just the right amount of grippy.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 5 years ago in reply to cstanton

    Obviously some people find them very useful.

    They wouldn't fit well in any of my workflows, except possibly final assembly, but I doubt I would actually use one. I don't use the red mat I showed above - bought it for a different purpose.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 5 years ago in reply to cstanton

    Obviously some people find them very useful.

    They wouldn't fit well in any of my workflows, except possibly final assembly, but I doubt I would actually use one. I don't use the red mat I showed above - bought it for a different purpose.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ntewinkel
    ntewinkel over 5 years ago in reply to dougw

    dougw  wrote:

     

    Obviously some people find them very useful.

     

    It's one of those things I didn't know I was missing until I got it image

    I was using flattened file folders to protect my desk before I knew about the silicon mats.

    I bought it mainly just to replace the ugly file folders image

     

    I only use it for soldering, but I can see it also being handy for fixing things like cell phones with little screws. It might be a little too small for other projects.

     

    The silicon does seem to be properly heat resistant - I've had the tip directly on it on numerous occasions to pick up a melted blob of solder with the iron. It's also much thicker than the flimsy dollar-store one I got first, which is now just under the soldering iron stand to catch stray bits.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 5 years ago in reply to ntewinkel

    I have several different vises I use to hold things I am soldering. The fine-work card-vise (which is flat and heavy) sits under a stereo microscope and needs to slide smoothly around so I can position the work properly under the microscope. The microscope is suspended from a cantilever so no part of it touches the bench surface, but it does not move. Additionally, I have brace pads for my wrists to keep them steady - those braces need to slide as well. A mat wouldn't make sense for that workflow.

    I do have the inklings of a card holder design that allows easy positioning of work under a microscope, but that is still in the daydreaming project bucket.

    • Cancel
    • Vote Up +3 Vote Down