Test & Tools
  • Technologies
  • More
Test & Tools
Blog Silicon Solder Mat
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 6 Feb 2021 4:39 PM Date Created
  • Views 6100 views
  • Likes 14 likes
  • Comments 47 comments
Related
Recommended

Silicon Solder Mat

Jan Cumps
Jan Cumps
6 Feb 2021

I purchased a silicon solder mat today, when I was in the electronics shop to pick up my order.

 

image

 

I use an antistatic mat as a generic work area, and prefer to keep that tidy. That mat can take an accidental touch of a hot iron, but it's not intended for that.

 

The silicon solder mat (from Velleman - Buy Belgian!) is heat resistant, up to 500° C.

Flexible and can be cleaned in a kitchen sink. It returns back to its original form.

Total size 45 x 30 cm. Work area without covering anything is approx. 40 * 28. It costed 20 €.

 

One of the biggest advantages for me is that it's easy to pick up and stow away. My lab is used as office, diner table and lab bench, depending on the time of day.

I prefer to have a reasonable clean desk. I remove instruments and projects when I use the desk as home office. And vice versa.

I'll report back in a while how the thing behaves in the real world. If I'm happy with the purchase or regret it.

  • Sign in to reply

Top Comments

  • ntewinkel
    ntewinkel over 5 years ago in reply to Jan Cumps +9
    Jan Cumps wrote: Mine has Velleman printed on it and that is better ! These would actually make great element14 swag. It's already the right colour too... just need some orange printing added. Velleman…
  • 14rhb
    14rhb over 5 years ago +7
    Hi Jan Cumps , I've the same mat, as you already ellude to, they are great for keeping the solder 'mess' in one place and I don't think you'll regret your purchase I bought my one to save me the embarassment…
  • ralphjy
    ralphjy over 5 years ago +7
    I use a smaller one - 35 x 25 cm, somewhat thinner (3.5mm) and without magnets. It works really well and is the perfect size for the type of soldering that I do. It was $8 from Amazon.
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to geralds

    I've only used it once, today, just to try it out.

    I am going to try and address your questions separately:

     

    But the silicone rubber is a little wobbly, isn't it?

    No, the mat is not wobbly when it lays down. It's flat on the bench. It's wobbly when you lift it up.

     

    To me, I think the elastic edge for my arms is a bit high, don't it?

    Only the back side is high. The sides and front have a ridge, but it is low and does not feel uncomfortable.

     

    the small components could be catapulted away if you suddenly move the mat.

    It does not move or shake once it is on the bench. It has a natural grip.

     

    like the control panel of Starship Enterprise

    Yes image I think that the designer was not selected for the stylistic skills.

     

    If you don't need the ridges and pockets (and I think they aren't essential), then a flat mat (or a flat one with a little ridge to keep flux from flowing off) would be certainly as good. And cheaper.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • geralds
    geralds over 5 years ago

    Hi Jan Jan Cumps

     

    image

    It's a nice mat.

    Yes, I am also looking for such a mat.

    But the silicone rubber is a little wobbly, isn't it?

    To me, I think the elastic edge for my arms is a bit high, don't it?

    When working on a SMD board, I need a very flat desk and plenty of room for my arms so that I can work smoothly and gently.

    Trembling hands are not practical when working with SMD, for example when the elbow presses on an edge, such as the edge of the silicone rubber.

    Shaky is not good either, otherwise the small components could be catapulted away if you suddenly move the mat.

    image

     

    But it looks good ... like the control panel of Starship Enterprise. image

     

    An other think I have about the magnets. How strong they are?

    There are a lot of magnets on the mat.

    So hm .. a magnetically sensitive component, like a bank card, your personal data can be erased rapidly, or not?

     

    Best Regards

    Gerald

    ---

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 5 years ago

    I like it.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to 14rhb

    Great idea.. Giant waffle mould is an innovation I for one have been missing in my life : )

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to dougw

    I presume it is not conductive?

    It's ESD safe. Enough conductive to not build op charge.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>