Test & Tools
  • Technologies
  • More
Test & Tools
Blog Soldering Iron Thermometer QUICK 191AD Review
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 19 Sep 2021 8:52 PM Date Created
  • Views 5011 views
  • Likes 10 likes
  • Comments 3 comments
  • 191ad
  • quick
  • soldering_tools
Related
Recommended

Soldering Iron Thermometer QUICK 191AD Review

shabaz
shabaz
19 Sep 2021

I recently bought a QUICK 191AD soldering iron thermometer, here's a 3-minute review : )

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This instrument costs about £100 in the UK (a couple of resellers in the UK stock it). It comes with a pack of ten sensors, there is a spring peg to hold it taut. It's a type-K thermocouple basically.

image

I cannot say it is the most useful tool in the world, I'm unlikely to use it often just to check soldering iron tip temperature. I may get a bit more use out of the tool simply because it has a connector for a normal external thermocouple probe too. One is supplied with the tool.

image

Functionality is pretty basic; all it does is display the temperature in degrees C (1 degree C granularity) between -13 and 973 degrees C, there is a Fahrenheit button, plus a useful Max-Hold capability, and the power-off time is configurable. The internals show that the design is quite ancient:

image

There's lots of spray coating on the board, and I couldn't read off any IC part numbers, unfortunately.

The instrument comes with calibration, and it is accurate (I tested with a thermocouple simulator/calibrator tool) across the entire range. My soldering iron was measured by the instrument to within 5 degrees C of the set temperature.

 

To summarize, the instrument is quite basic, but since it comes with calibration, is accurate, and can be used with an external thermocouple, I think that goes some way toward making the tool more useful.

 

Thanks for reading!

  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 5 years ago +1
    Thanks for posting the video. Today I learned I have been using my meter wrong. I had been putting pressure on the sensor. For example, basically resting the iron tip on it. I was, at least, already using…
Parents
  • rsjawale24
    rsjawale24 over 5 years ago

    I recently bought a soldering iron thermometer from an online Indian store on sale just for INR 213 ~ 2.86 USD. Waiting for it to arrive. It looks like a rip off version of Hakko FG-100. Not sure about it's accuracy though. Will test it and post a short blog.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to rsjawale24

    Hi Rushiraj,

     

    That's a much better price!

    Actually, even if it were inaccurate, it is worth it just for the mechanical portion alone, because that could be wired up to (say) a multimeter that has thermocouple input. But probably it will be fine as-is, since precise accuracy isn't needed, and besides sometimes it's useful just for comparison purposes (e.g. comparing one iron or tip with another).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 5 years ago in reply to rsjawale24

    Hi Rushiraj,

     

    That's a much better price!

    Actually, even if it were inaccurate, it is worth it just for the mechanical portion alone, because that could be wired up to (say) a multimeter that has thermocouple input. But probably it will be fine as-is, since precise accuracy isn't needed, and besides sometimes it's useful just for comparison purposes (e.g. comparing one iron or tip with another).