Test & Tools
  • Technologies
  • More
Test & Tools
Blog Tektronix - MDO3000 - 6 Instruments in 1 scope
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: patkelly
  • Date Created: 9 Apr 2014 9:55 AM Date Created
  • Views 1827 views
  • Likes 5 likes
  • Comments 6 comments
  • mdo3000
  • scope
  • tektronix
Related
Recommended

Tektronix - MDO3000 - 6 Instruments in 1 scope

patkelly
patkelly
9 Apr 2014

The MDO3000 Mixed Domain Oscilloscope (MDO) SeriesMDO3000 Mixed Domain Oscilloscope (MDO) Series, a 6-in-1 integrated oscilloscope from Tektronix reducing cost and maximising workspace.

 

The MDO3000 MDO3000 includes an integrated spectrum analyzer, arbitrary function generator, logic analyzer, protocol analyzer, and digital voltmeter/counter. Completely customizable the MDO3000MDO3000 allows the user to add instruments and performance as required. Containing an integrated 4-digit digital voltmeter (DVM) and 5-digit frequency counter, any of the analog inputs can be a source for the voltmeter, using the same probes that are already attached for general oscilloscope usage. The display is both numeric and graphical and shows minimum, maximum, and average values of the measurement as well as the range of values measured over the previous five second interval.

 

image

 

A fast waveform capture rate of greater than 280,000 wfm/s with FastAcq facilitates the identification of infrequent problems common in digital systems: runt pulses, glitches, timing issues, and more.

 

Intensity grading is used to indicate how often rare transients are occurring relative to normal signal characteristics with four waveform palettes available in FastAcq acquisition mode.

The MDO3000 MDO3000 is the first oscilloscope in its class to include an integrated spectrum analyzer with a frequency range of 9 kHz up to the analog bandwidth of the instrument which can be upgraded to 3 GHz (option MDO3SA), enabling spectral analysis on most consumer wireless standards.

 

"As designs are becoming integrated, so too should the oscilloscopes used to test them."

 

Chris Godfrey, Global Product Director Test & Tools, Premier Farnell, said: “We are pleased to grow our Tektronix range with the addition of the MDO3000MDO3000.  As designs are becoming integrated, so too should the oscilloscopes used to test them.  Our drive is to support the customer from design right through to production and this product’s great range of features makes it easier for engineers to diagnose problems quickly and efficiently.”

 

image

 

Dave Farrell, general manager, Mainstream Oscilloscopes at Tektronix, said: “There’s a fundamental shift with regard to wireless in embedded systems. With RF technologies so established and affordable, they are becoming as accepted and widely used as serial data was a few years ago.  In addition, with digital signals increasing in speed, the effects of electromagnetic interference (EMI) has become a common problem requiring looking at the RF spectrum of even non-wireless systems.  Just as MSOs have replaced analog-only oscilloscopes, it follows that MDOs are the next logical evolution and are becoming the accepted mainstream industry standard.”

 

Key performance specifications - Technical Datasheet

  • Oscilloscope
    • 2 and 4 analog channel models
    • 1 GHz, 500 MHz, 350 MHz, 200 MHz, 100 MHz bandwidth models
    • Bandwidth is upgradable (up to 1 GHz)
    • Up to 5 GS/s sample rate
    • 10 M record length on all channels
    • >280,000 wfm/s maximum waveform capture rate
    • Standard passive voltage probes with 3.9 pF capacitive loading
    • and 1 GHz, 500 MHz, or 250 MHz analog bandwidth
  • Spectrum Analyzer
    • Frequency range
      • Standard: 9 kHz - oscilloscope bandwidth
      • Optional: 9 kHz - 3 GHz
    • Ultra-wide capture bandwidth up to 3 GHz

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

image

  • Sign in to reply

Top Comments

  • Problemchild
    Problemchild over 12 years ago +2
    Hi Pat certainly a nice bit of kit obviously other folk on other sites have reviewed other members of this series. What I'd really like to see for this and other equipment tests is a full road test were…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Problemchild +1
    Oh John, ask and ye shall recieve, I believe we indeed are set to do a road test - Beginning early May...Please keep an I out for that and sign up...
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor +1
    Coolio I shall keep an I out and several other Vowels it helps
Parents
  • Problemchild
    Problemchild over 12 years ago

    Hi Pat certainly a nice bit of kit obviously other folk on other sites have reviewed other members of this series. What I'd really like to see for this and other equipment tests is a full road test were someone actually uses it to do something not just a list of the key features because these after all are  in the buy me sheet from the vendor. The problem with a bit of equipment  like this is that there is so much going on that many people don't even understand why they would need feature X,Y or Z. I suppose that those in the know have already bought one but it would be great to have a real world reason to drool over a bit of equipmentlike this  image !!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Problemchild

    Oh John, ask and ye shall recieve,

    I believe we indeed are set to do a road test - Beginning early May...Please keep an I out for that and sign up...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor

    Coolio I shall keep an I out and several other Vowels it helps image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor

    Bit early I know but was wondering when the Roadtest for this Scope is starting , would certainly like a go at reviewing it !...Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor

    Bit early I know but was wondering when the Roadtest for this Scope is starting , would certainly like a go at reviewing it !...Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • patkelly
    patkelly over 12 years ago in reply to Problemchild

    You ain't seen me...right! image

     

    http://www.element14.com/community/roadTests/1296