Test & Tools
  • Technologies
  • More
Test & Tools
Forum Diode identification and car radio repair
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 387 subscribers
  • Views 6761 views
  • Users 0 members are here
Related

Diode identification and car radio repair

edumcg
edumcg over 6 years ago

Hello,

 

 

I'm trying to repair my nissan car radio model: Clarion BTS33

 

 

The problem began when the fuel volumen line of my car shortcircuited with 12V.  As soon as that happened my radio turned off and never came back again. I sent the radio with some folks to repair it, they replaced some ICs that were burned out but they couldn't replace one specific diode.

 

 

Right now, when I plug the radio into my car only the screen shows up but it prints nothing. Just a blank orange screen. No audio output no matter what buttons I press.

 

 

I found the cable on Amazon: https://www.amazon.com/20-pin-Subaru-Headunit-Harness-Steering/dp/B01D9K3L44

 

 

I also found the user manual of the radio: https://fccid.io/2ABGYBTS33-CLARION/User-Manual/User-guide-2150158

 

 

The only component that looks burned out is the diode D402. The diode is the same as de diode D403 so I can see the marking is "C308" the 08 is fllipped to the right 90 degress.

 

 

My plan is to replace the diode but I haven't been able to find a datasheet.

 

 

I've attached images of the radio and the circuit board. Any help would be appreciated.

 

 

Thanks!

Attachments:
image
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 6 years ago in reply to MDeGrauw +3
    Well now, would you lookie there. Thanks MdG & JC, I learned something. SOT-23 packaging never existed before my absenteeism from electronics. I noticed the more bright members ignored my comments and…
  • fiddler_in_the_lab
    fiddler_in_the_lab over 6 years ago +2
    I would not have to high hopes that replacing that diode will fix the problem.... but as it is an easy thing to do if you (or a friend) have a multimeter and basic soldering skills. So it sure is worth…
  • msbettyhunt
    msbettyhunt over 6 years ago in reply to fiddler_in_the_lab +2
    It is a good idea of replacing the diode with the general purpose diode. Hope it will work.
Parents
  • edumcg
    edumcg over 6 years ago

    Hi guys,

     

    Well I measured the 3 terminals of the diode and only the 2 that are beside each other resulted with continuity. I also noticed that the continuity is because they are both grounded. Another thing I noticed is that the marking is actually "C30B" I mistaken the B for an 8.



    Sorry for my bad diagram. So I'm not sure if this part is actually a diode at all. But as Fredrik Andersson said maybe is not worth it to replace this irrelevant part and I should be searching for something more specific.

    I think my next step is to identify every IC on the board and then try to find their specific datasheet to figure out if they are doing what they are supposed to.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • edumcg
    edumcg over 6 years ago

    Hi guys,

     

    Well I measured the 3 terminals of the diode and only the 2 that are beside each other resulted with continuity. I also noticed that the continuity is because they are both grounded. Another thing I noticed is that the marking is actually "C30B" I mistaken the B for an 8.



    Sorry for my bad diagram. So I'm not sure if this part is actually a diode at all. But as Fredrik Andersson said maybe is not worth it to replace this irrelevant part and I should be searching for something more specific.

    I think my next step is to identify every IC on the board and then try to find their specific datasheet to figure out if they are doing what they are supposed to.