Test & Tools
  • Technologies
  • More
Test & Tools
Forum Diode identification and car radio repair
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 388 subscribers
  • Views 6700 views
  • Users 0 members are here
Related

Diode identification and car radio repair

edumcg
edumcg over 6 years ago

Hello,

 

 

I'm trying to repair my nissan car radio model: Clarion BTS33

 

 

The problem began when the fuel volumen line of my car shortcircuited with 12V.  As soon as that happened my radio turned off and never came back again. I sent the radio with some folks to repair it, they replaced some ICs that were burned out but they couldn't replace one specific diode.

 

 

Right now, when I plug the radio into my car only the screen shows up but it prints nothing. Just a blank orange screen. No audio output no matter what buttons I press.

 

 

I found the cable on Amazon: https://www.amazon.com/20-pin-Subaru-Headunit-Harness-Steering/dp/B01D9K3L44

 

 

I also found the user manual of the radio: https://fccid.io/2ABGYBTS33-CLARION/User-Manual/User-guide-2150158

 

 

The only component that looks burned out is the diode D402. The diode is the same as de diode D403 so I can see the marking is "C308" the 08 is fllipped to the right 90 degress.

 

 

My plan is to replace the diode but I haven't been able to find a datasheet.

 

 

I've attached images of the radio and the circuit board. Any help would be appreciated.

 

 

Thanks!

Attachments:
image
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 6 years ago in reply to MDeGrauw +3
    Well now, would you lookie there. Thanks MdG & JC, I learned something. SOT-23 packaging never existed before my absenteeism from electronics. I noticed the more bright members ignored my comments and…
  • fiddler_in_the_lab
    fiddler_in_the_lab over 6 years ago +2
    I would not have to high hopes that replacing that diode will fix the problem.... but as it is an easy thing to do if you (or a friend) have a multimeter and basic soldering skills. So it sure is worth…
  • msbettyhunt
    msbettyhunt over 6 years ago in reply to fiddler_in_the_lab +2
    It is a good idea of replacing the diode with the general purpose diode. Hope it will work.
Parents
  • fiddler_in_the_lab
    fiddler_in_the_lab over 6 years ago

    I would not have to high hopes that replacing that diode will fix the problem.... but as it is an easy thing to do if you (or a friend) have a multimeter and basic soldering skills. So it sure is worth to try.

     

    I did not find a perfect match for the marking code. There are a few dual diodes that start with C3 (or C30). The 08 could be a date code. But in this case you are lucky that there are more diodes of the same type mounted on the PCB so you can measure if the diode configuration is either "common cathode" or "serial" with a multimeter that have a diode test.. You could probably measure directly on the PCB, or de-solder it to be safe. The diode test should also show if it is a schottky or silicon diode.

     

    I do think that it is enough to replace the diode with any general purpose diode that have the same configuration and type (eg common cathode schottky in sot-23 package) to see it it works.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • edumcg
    edumcg over 6 years ago in reply to fiddler_in_the_lab

    I did the diode test with a multimeter and these are my results:

    image

    I don't know if the diode marked with a orange  may be faulty since the reading was the same when exchanging the positive and negative probes of my multimeter.

     

    The one marked by a yellow box is surely a common cathode. Both have the same marking code.

    I'm gonna get a general purpose diode with the same characteristic and replace both of them. One at a time.
    Thanks for posting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • edumcg
    edumcg over 6 years ago in reply to fiddler_in_the_lab

    I did the diode test with a multimeter and these are my results:

    image

    I don't know if the diode marked with a orange  may be faulty since the reading was the same when exchanging the positive and negative probes of my multimeter.

     

    The one marked by a yellow box is surely a common cathode. Both have the same marking code.

    I'm gonna get a general purpose diode with the same characteristic and replace both of them. One at a time.
    Thanks for posting.