Test & Tools
  • Technologies
  • More
Test & Tools
Forum Why Are Digital Scopes Noisy (Or what appears to be Noisy)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 387 subscribers
  • Views 3277 views
  • Users 0 members are here
  • test
  • digital
  • tektronix
  • measure
  • oscilloscope
  • and
  • noise
Related

Why Are Digital Scopes Noisy (Or what appears to be Noisy)

Robert Peter Oakes
Robert Peter Oakes over 12 years ago

Dave Jones of EEVBlog and others have gone to great length to show how the noise shown on newer digital scopes is actually because there better at detecting it due to being able to refresh the screens at better rates and of course because of the digital sampling etc, and for that part I totally get it.

https://www.youtube.com/watch?v=Znwp0pK8Tzk

 

Well I do if it where not for the fact that at no time has it been explained where the actual noise is coming from in the first place, If i have a probe or other length of wire on the input, then OK it is an antenna and so you expect it and a nice new high bandwidth scope will show it all

 

but if the input is terminated, shorted out or otherwise not connected surely it should not be there, or certainly not at the levels shown in the videos

 

If I was paying over 10K for a scope, im sure that it showing 100mV of noise or more when the input is terminated, shorted or otherwise connected to a good signal source, I would be a little upset.

 

If I am trying to measure single digit noise on a scope and the scope is generating its own far in excess of this then what gives ?

 

So there you have it, I know we have a Tektronics Expert in our ranks right now, I would be very interested on his/her take on this and of course from anyone else. I for one would love to understand why for my own sake and also to help others understand

 

Let the debate begin and perhaps we can get a great briefing note out of it

 

Peter

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago in reply to Robert Peter Oakes +2
    The thermal noise from a 1k resistor over a 1GHz bandwidth is 127uV, from 1 1M resistor it's about 4mV which are about 0.762mV and 24mV pk-pk respectively. If you are using a x10 probe it is the 1M case…
  • michaelkellett
    michaelkellett over 12 years ago in reply to Robert Peter Oakes +1
    Scope manufacturers are very coy about noise specs. Looking at the 12 bit LeCroy data sheet there is no simple "divisions pk-pk on range x" spec. Instead it says that it has 55dB SNR - thats a ratio of…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    All very good and valid points but still

     

    an oscilloscope with say a 2mV per division range should be able to show a sub 2mV waveform without much noise

     

    take a typical scope with 8 to 10 vertical division, if the noise is 1 division then that's 10% or more of the range, does not this seem excessive for the range

     

    some of the examples I have seen on you-tube  where showing a division of noise even on the 100 - 200mV ranges, that's an awful lot of noise even for a cheap oscilloscope

     

    So yes I get the ADC noise, input front end noise etc etc, but I would never expect it to be more than sub 2% on a low cost scope and probably less than 0.5% on a high end scope

     

    Am i crazy for expecting that ???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to Robert Peter Oakes

    Scope manufacturers are very coy about noise specs.

     

    Looking at the 12 bit LeCroy data sheet there is no simple "divisions pk-pk on range x" spec.

     

    Instead it says that it has 55dB SNR - thats a ratio of 562:1 so at 8 divisions full scale you could expect as little as 1.4% of  a division which would be very nice, despite being well short of 12 bits.

     

    Here's an interesting link:

     

    http://www.evaluationengineering.com/special-reports/201307/instruments/Resolving-Finer-Detail.html

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 12 years ago in reply to Robert Peter Oakes

    Scope manufacturers are very coy about noise specs.

     

    Looking at the 12 bit LeCroy data sheet there is no simple "divisions pk-pk on range x" spec.

     

    Instead it says that it has 55dB SNR - thats a ratio of 562:1 so at 8 divisions full scale you could expect as little as 1.4% of  a division which would be very nice, despite being well short of 12 bits.

     

    Here's an interesting link:

     

    http://www.evaluationengineering.com/special-reports/201307/instruments/Resolving-Finer-Detail.html

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to michaelkellett

    That is a very cool article

     

    Thanks