Test & Tools
  • Technologies
  • More
Test & Tools
Forum Polarity Sense Circuit
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 1 answer
  • Subscribers 387 subscribers
  • Views 7053 views
  • Users 0 members are here
  • reverse_polarity_sensor
Related

Polarity Sense Circuit

jw0752
jw0752 over 11 years ago

In one of my recent builds it was necessary to come up with a circuit that would sense if the inputs were hooked up reverse polarity. I came up with this circuit:

 

image

I have tested this circuit to 100 volts DC on its Test Input terminals. If the Test Inputs are under normal polarity the output is LOW and if the Test Inputs are under reverse polarity the Output is HIGH. Unfortunately the Test Inputs will not sense a reversed polarity below 3.5 Volts. While these limitations were not a problem for my build I am curious if there are other better circuits to test polarity than what I cooked up here. Also if you see problems with the circuit above any critique would be appreciated. R1 limits the forward current through LED1 which acts like a zener and keeps the voltage Gate to Drain from exceeding breakdown limits. D1 is reverse biased under proper polarity. R2 keeps the P CH MOSFET off until there is a Negative Voltage applied at the gate by a reversed Test Input polarity.

 

Thanks John

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 11 years ago +2
    I don't know what your application is for this polarity sense circuit, but if you're worried about DC power inputs being hooked up incorrectly you might consider using a Schottky Diode Bridge for your…
  • shabaz
    shabaz over 11 years ago in reply to jw0752 +2
    Hi John, I once took apart a very old touch tone phone (probably a trimline), it was interesting to see that they used analog tone generation circuitry! using pot core wound transformers for the tone generation…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    without an OP-Amp or other transistor your limited by the Diode voltages and also the VGS Threshold of the FET so without making it much more complex it seems you hae a good solution or what you needed…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    so a few ground rules

     

    No Battery ??

    minimal load on circuit...

     

    any more ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    so a few ground rules

     

    No Battery ??

    minimal load on circuit...

     

    any more ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter,

    There are probably not many applications for this type of circuit or there would be more literature. The need I had in my DC Load Unit has been satisfied and right now I am just experimenting and playing with different ideas. Since I really do not have a pending need the ground rules are a little flexible. My imagination suggests that my goal would be a circuit that had minimal load on the circuit whether it was hooked up proper polarity or reversed. I would want it to cover a range of voltage from say 1 volts to 80 volts and it should be fast enough so that the inputs can be disengaged from the main circuit before any damage is done. Right now I have 4 or 5 new ideas to investigate thanks to you, michaelkellett , D_Hersey , johnbeetem , and mcb1 .

    Thanks John