Test & Tools
  • Technologies
  • More
Test & Tools
Forum Color Convention for Power Wires
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 386 subscribers
  • Views 6226 views
  • Users 0 members are here
  • wire_color_convention
Related

Color Convention for Power Wires

jw0752
jw0752 over 10 years ago

     I am aware of the color convention for Positive and Negative wires in electronics. Red is Positive and Black is Negative. The other day as I was hooking up a small dual supply OpAmp it dawned on me that I did not know what the color convention is for the Zero Volt Ground wire between the two supplies. Does anyone know if there is a Color Convention for this Zero wire and what that color is? Also it would be interesting to know if there are any other standardized color conventions for hookup wires such as signal or output.

 

John

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 10 years ago in reply to Robert Peter Oakes +2
    I take the path of least resistance and follow what PSU manufacturers do: When a supply is asymmetrical, I use red for + and black for -. When I'm dealing with a symmetrical setup, I use the same, but…
  • mcb1
    mcb1 over 10 years ago +1
    Good question. I've tended to use Red and Black as well. If the voltages were mixed I often used Orange for 12v. Mains wiring tends to use Green for Earth or Ground and is a wise choice, but black is also…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1 suggested
    Red is correct for DC Positive but Black is correct for DC 0V by convention, not negative For AC mains in USA/Canada Black is LIVE, WHITE is neutral, UK and other areas Brown is Live and Blue is neutral…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    Red is correct for DC Positive but Black is correct for DC 0V by convention, not negative

     

    For AC mains in USA/Canada Black is LIVE, WHITE is neutral, UK and other areas Brown is Live and Blue is neutral

    LIVE

    Color wire brown.svgColor wire black.svgColor wire red.svgColor wire yellow.svg

    NEUTRAL

    Color wire blue.svgColor wire white.svg

     

    The only real consistent thing for pretty much all countries is Green, Green/Yellow or Bare copper is always GROUND

    Color wire green yellow.svgColor wire green.svgColor wire bare copper.svg

     

     

    Now depending on cores and Voltages this all can change, also older wiring may be different, to be sure check local codes and WIKI https://en.wikipedia.org/wiki/Electrical_wiring seems to also have a reasonable list but verify local codes to be sure

     

    So for DC Low voltages there is a sudo code (I doubt it is official), look to PC wiring etc for what I mean

     

    Red - 5V

    Yellow - 12V

    Black - 0V

    ....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 10 years ago in reply to Robert Peter Oakes

    I take the path of least resistance and follow what PSU manufacturers do:

     

    When a supply is asymmetrical, I use red for + and black for -.

    When I'm dealing with a symmetrical setup, I use the same, but the ground point in the middle is green.

    image

     

    My breadboard uses the same convention:

    image

     

     

    Of course, then there's these image :

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to Jan Cumps

    Please be careful with the assumption that GREEN is the Middle because it is not, it is ground and only ground, it is possible that 0V may be tied to GND but should not be as assumption and with alot of electronics it is undesirable , in all of the above pictures Green is GND and not 0V, the one with Black as Ground goes against ALL convention and should be regarded as wrong or atleast very missleading

     

    In the PSU picture it clearly shows that 0V can go as high as 240V above GND but no more, there will be MOVs etc to prevent it from happening but outside of that, the - and + are isolated from GND

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to Jan Cumps

    Please be careful with the assumption that GREEN is the Middle because it is not, it is ground and only ground, it is possible that 0V may be tied to GND but should not be as assumption and with alot of electronics it is undesirable , in all of the above pictures Green is GND and not 0V, the one with Black as Ground goes against ALL convention and should be regarded as wrong or atleast very missleading

     

    In the PSU picture it clearly shows that 0V can go as high as 240V above GND but no more, there will be MOVs etc to prevent it from happening but outside of that, the - and + are isolated from GND