Test & Tools
  • Technologies
  • More
Test & Tools
Forum Need help measuring 120VAC main
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 371 subscribers
  • Views 2660 views
  • Users 0 members are here
Related

Need help measuring 120VAC main

totalhighspeed
totalhighspeed over 9 years ago

I built a circuit board to measure 120VAC using a Raspberry PI. I have a bridge rectifier and voltage divider. All using surface mount 1206 parts. Everything works well. When I put a voltmeter on the test point it shows 1/100th the line voltage in DC. However, when I actually look at it on a scope, I see that the ripple is 0 to 1.2v, essentially the full rectified voltage. The filter isn't doing hardly anything.

 

I'm trying to keep is all as small as possible so I'd like to stick with 1206 package for the filtering capacitors especially since the PCB has already been manufactured using these. I did use a through hole for the inductor it has 5mm lead spacing. Can someone recommend what capacitor and inductor values to use to get a cleaner DC(ish) voltage. The voltage divider is before the filtering so using low voltage capacitors are not a problem.

 

I was using 1000pF on C1 and 2200pF on C2 and 100mH for the Inductor. Below is the layout:

 

>-------- L1 ---------->

      |             |

     C1        C2

      |             |

>----------------------->

 

Any help would be GREATLY appreciated...

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago in reply to totalhighspeed +3 verified
    First I must give you the quick lecture on mains safety: USE AN ISOLATING TRANSFORMER !!! If your circuit is connected to the mains supply it is not safe. Now to filtering some safe 60Hz AC to measure…
  • D_Hersey
    D_Hersey over 9 years ago +2
    Listen to the nice, smart and pretty folks on this thread and USE A T-FORMER!
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    please provide the full schematic, there is no rectifier in this diagram nor the values of the components

     

    We will be better able to help if you provide the full diagram with details

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • totalhighspeed
    0 totalhighspeed over 9 years ago in reply to Robert Peter Oakes

    image

    As requested....

     

    The zener (ZD6) is just a 3.3v to keep the Pi's GPIO's safe.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to totalhighspeed

    First I must give you the quick lecture on mains safety:

     

    USE AN ISOLATING TRANSFORMER !!!

     

    If your circuit is connected to the mains supply it is not safe.

     

    Now to filtering some safe 60Hz AC to measure it:

    You don't really need a bridge rectifier - a single diode will do.

    Use LTSpice to simulate this kind of stuff - it's free and easy to use.

     

    This is about what you've got but I'm running AC into it just to see the response of the filter - as you can see its not really working at the right sort of frequency at all - you need a filter which lets through almost nothing at 60 or 120 Hz (half or full wave rectifier)

    image

     

    The second circuit is a simplification of yours (but remember you shouldn't build this - if the 1M resistor fails you DIE !!)

    I think this is what you are seeing on your design the problem is that there is almost no filtering going on.

    image

     

    This third go is with some better component values and some simplification:

    image

     

    Now it works - its taking a while to settle and there is some ripple. If you were to use a small transformer to give you a nice safe 10V to work with you could have this design where we can reduce some impedances without risk of death !

     

    image

     

    You can get a faster response at the expense of ripple by reducing the capacitor values or the resistor values. The input impedance of the ADC must be high (> 100k). If  you use  a transformer you may live to improve it.

     

    Have fun, use simulation.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 9 years ago

    As Micheal points out - be mindful of safety.

    There are many calculators and simulators on-line:

    RC Low-pass Filter Design Tool

    Low Pass Filter Calculator

    RC pad corner frequency upper and lower cutoff frequency calculation filter calculate time constant tau RC voltage power…

    etc.

    I have seen people use capacitive dividers instead of resistive dividers to get the voltage down.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • peterjcs23
    0 peterjcs23 over 9 years ago

    You could step down the voltage with a transformer to make the voltage safe to handle on a PCB.

     

    77DB-06-09. IDEAL POWER, AC/AC Power Supply, UK, 240 V, 10 W, 9 VAC, 670 mA | Farnell element14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • totalhighspeed
    0 totalhighspeed over 9 years ago

    Michael,

    I appreciate the safety warning and will take it into account.

     

    Everyone,

    Thank you for the input and the assistance.

     

    As for safety, there will be no current load, this device isn't powering -anything- it will just be for measuring the voltage of the AC main. It will be encased in plastic and there will be a breaker in line so that power can be disconnected for any maintenance that might be required. The PCB is also clearly marked to indicate the presence of high voltage.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 9 years ago

    Listen to the nice, smart and pretty folks on this thread and USE A T-FORMER!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to D_Hersey

    Wow, thanks Don, Iv'e been called 'smart' once before and 'nice' a few time - be this is the very first 'pretty' !!

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 9 years ago

    It's all the studying:

     

    Results from this new dating app say reading makes you more attractive | Deseret News

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to michaelkellett

    Totally agree, reminds me of an old proverb image

     

    You can get to do it right a million times, but only get to do it wrong once.

     

    how many people have you heard of that have had near death experiences, how many people who died have you heard from image

     

     

    USE A TRANSFORMER, SET AN EXAMPLE TO THE NEW ONES AND DO IT SAFELY ESPECIALLY AS PEOPLE CAN AND DO COPY WITH FAR LESS KNOWLEGE THAN YOU.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>