Test & Tools
  • Technologies
  • More
Test & Tools
Forum The opposite of a ten turn potentiometer?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 387 subscribers
  • Views 2491 views
  • Users 0 members are here
Related

The opposite of a ten turn potentiometer?

supper_slash
supper_slash over 9 years ago

I need a solution for a potentiometer that goes from 0-100 in an eight of a turn.

Think of a lever that is testing the thickness of something.  And every second or so the reading is taken and logged into an Arduino.

 

I have used an Arduino to read pot's before,but I have never only had to read from(12 o'clock, to 2 o'clock) before with high sensitivity.

I was thinking of using a GEAR amplification to make a regular pot work if I must, but it would take a very large amount of space, so I am trying to think of another solution.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 9 years ago

    Depending on the application you might get away with this, it's more usual to use a different kind of sensor for measuring small displacements.

     

    You can use strain gauges on a springy metal arm or LVDT sensors, or perhaps a rotational sensor designed to work over small angles.

     

    If you tell us what you are trying to measure it would be possible to advise you better.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • supper_slash
    0 supper_slash over 9 years ago in reply to michaelkellett

    I have 2 projects in the works for this application.

    1. A volume pedal type device that the pot will need to be mounted at the pivot point. {As it is now I am not happy with my design that uses a vertical runner to turn a gear on a standard POT.}Strip Gear.
      The above image shows the parts used in the current designs in the foot pedals that I am looking to replace. I am hoping to simply place a POT AT the pivot point in this design.
      Pedal design

    2. A gauging system for my filament on my 3-D printer. The Idea is to have a lever with a roller at the end of it amplify the thickness of the pinched filament to a mounted POT. That pot will send the readings every 10 seconds or so to a Microcontroller for data logging.
      lever
      POT on the left, roller and filament on the right. So small changes in the filament  effect large changes in the POT.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • supper_slash
    0 supper_slash over 9 years ago in reply to michaelkellett

    I have 2 projects in the works for this application.

    1. A volume pedal type device that the pot will need to be mounted at the pivot point. {As it is now I am not happy with my design that uses a vertical runner to turn a gear on a standard POT.}Strip Gear.
      The above image shows the parts used in the current designs in the foot pedals that I am looking to replace. I am hoping to simply place a POT AT the pivot point in this design.
      Pedal design

    2. A gauging system for my filament on my 3-D printer. The Idea is to have a lever with a roller at the end of it amplify the thickness of the pinched filament to a mounted POT. That pot will send the readings every 10 seconds or so to a Microcontroller for data logging.
      lever
      POT on the left, roller and filament on the right. So small changes in the filament  effect large changes in the POT.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to supper_slash

    You won't do better than the pot with rack and pinion for the foot pedal, at least not without a lot of complication.

     

    For the filament thickness there are loads of options - how much are prepared to spend and how much time can you put into messing about.

     

    Look here for some ideas:

     

    https://www.aliexpress.com/wholesale?SearchText=displacement+sensor&initiative_id=RS_20160930091159

     

    good range of prices - from about £10 to over £1000

     

    MK