Test & Tools
  • Technologies
  • More
Test & Tools
Forum Reverse polarity protection circuit & output backward flow control
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 7 answers
  • Subscribers 387 subscribers
  • Views 6144 views
  • Users 0 members are here
  • reverse polarity protection
Related

Reverse polarity protection circuit & output backward flow control

tim687
tim687 over 9 years ago

I am building my own (2 channel) lab bench. This is the conversion board I'm using to convert 12V (input) to 1-24V (one for each channel).

 

In the product description they say

Input reverse connect protection: No (If necessary, please input series schottky diode)
Output control flow backward: No (If used for battery charging or load is bring electricity load, please on the output side series schottky diode)

This does mean that there is no reverse polarity input protection (that is not needed anyways), but does this mean that there is reverse polarity output protection?

In the datasheet of the LTC3780 I found the following pin descriptions in the pinout:

 

SENSE+ (Pin 3/Pin 1):

The + Input to the Current Sense

and Reverse Current Detect Comparators. The ITH

pin voltage and built-in offsets between SENSE– and SENSE+ pins,

in conjunction with RSENSE, set the current trip threshold.

SENSE– (Pin 4/Pin 2):

The (–) Input to the Current Sense

and Reverse Current Detect Comparators.

 

Is this the reverse polarity protection feature and output backward flow control I'm looking for?

 

If yes, I don't have to design the circuitry to protect the output, if no, could you provide a solution which can accept variable voltages?

This is one solution I found very interesting due to the indicator LED and the 'no power loss' (claim).

Due to inefficiency of a schottky diode I am only going to use it if necessary.

 

Thanks in advance for helping me out!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago +1 suggested
    This board will make a truly dreadful bench supply - unless you only want it to work light bulbs or heaters then please think again. I recently helped a customer trouble shoot a new design where they had…
  • rachaelp
    rachaelp over 9 years ago in reply to michaelkellett +1 suggested
    Michael Kellett wrote: For a general purpose bench supply you can't beat a decent linear design - just learn to live with the size, weight and heat MK You can also do a hybrid design to try and get the…
  • michaelkellett
    michaelkellett over 9 years ago in reply to tim687 +1 suggested
    Hello Tim, The noise is un-fixable by any reasonable means - it consists of bursts of very large amplitude 50-130 MHz decaying sine bursts as the power devices switch. We put at least 160 hours of engineering…
Parents
  • jw0752
    0 jw0752 over 9 years ago

    Hi Tim,

     

    While the LTC3780 may support some protections the advertising indicates that there is no protection. Schottky diodes are relatively inexpensive and if you feel that there is any danger of reverse voltages being applied it won't hurt to put a diode in parallel for the input and in series for the output. You will only loose 0.4 volts on the output. There is no loss for the use of the polarity protection diode in parallel on the input.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 9 years ago

    Hi Tim,

     

    While the LTC3780 may support some protections the advertising indicates that there is no protection. Schottky diodes are relatively inexpensive and if you feel that there is any danger of reverse voltages being applied it won't hurt to put a diode in parallel for the input and in series for the output. You will only loose 0.4 volts on the output. There is no loss for the use of the polarity protection diode in parallel on the input.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • tim687
    0 tim687 over 9 years ago in reply to jw0752

    Hi John,

     

    At 10 Amps that is 4 Watt of power, I am not concerned about the power loss, but more of the heat. I want the lab bench to be very reliable and putting the diodes to handle this load is not making me very confident about the lab bench.

    There is no relay circuit for variable voltages?

     

    The input of the DC-DC converter will be the right way around at all times, so no protection is needed there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago in reply to tim687

    Hi Tim,

     

    I'm not saying this is the correct diode, but it is similar to what I would use in your application. Search Newark for a diode that has twice your expected output voltage and as low a junction voltage as possible. This one will handle 16 Amps. Of course you will have to heat sink it to get this amount of power through it. Another possibility might be to use a P Channel MOSFET as a switch but I will have to investigate how that would work. P Channel Power MOSFET can have very low impedance at saturation.

     

    http://www.newark.com/ixys-semiconductor/dss16-01a/diode-schottky-16a-to220ac/dp/96K8814

     

    John