Test & Tools
  • Technologies
  • More
Test & Tools
Forum Reverse polarity protection circuit & output backward flow control
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 7 answers
  • Subscribers 387 subscribers
  • Views 6015 views
  • Users 0 members are here
  • reverse polarity protection
Related

Reverse polarity protection circuit & output backward flow control

tim687
tim687 over 9 years ago

I am building my own (2 channel) lab bench. This is the conversion board I'm using to convert 12V (input) to 1-24V (one for each channel).

 

In the product description they say

Input reverse connect protection: No (If necessary, please input series schottky diode)
Output control flow backward: No (If used for battery charging or load is bring electricity load, please on the output side series schottky diode)

This does mean that there is no reverse polarity input protection (that is not needed anyways), but does this mean that there is reverse polarity output protection?

In the datasheet of the LTC3780 I found the following pin descriptions in the pinout:

 

SENSE+ (Pin 3/Pin 1):

The + Input to the Current Sense

and Reverse Current Detect Comparators. The ITH

pin voltage and built-in offsets between SENSE– and SENSE+ pins,

in conjunction with RSENSE, set the current trip threshold.

SENSE– (Pin 4/Pin 2):

The (–) Input to the Current Sense

and Reverse Current Detect Comparators.

 

Is this the reverse polarity protection feature and output backward flow control I'm looking for?

 

If yes, I don't have to design the circuitry to protect the output, if no, could you provide a solution which can accept variable voltages?

This is one solution I found very interesting due to the indicator LED and the 'no power loss' (claim).

Due to inefficiency of a schottky diode I am only going to use it if necessary.

 

Thanks in advance for helping me out!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago +1 suggested
    This board will make a truly dreadful bench supply - unless you only want it to work light bulbs or heaters then please think again. I recently helped a customer trouble shoot a new design where they had…
  • rachaelp
    rachaelp over 9 years ago in reply to michaelkellett +1 suggested
    Michael Kellett wrote: For a general purpose bench supply you can't beat a decent linear design - just learn to live with the size, weight and heat MK You can also do a hybrid design to try and get the…
  • michaelkellett
    michaelkellett over 9 years ago in reply to tim687 +1 suggested
    Hello Tim, The noise is un-fixable by any reasonable means - it consists of bursts of very large amplitude 50-130 MHz decaying sine bursts as the power devices switch. We put at least 160 hours of engineering…
Parents
  • tim687
    0 tim687 over 9 years ago

    But back to the question; are the protection circuits I've posted earlier today any good?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago in reply to tim687

    Hi Tim,

    The circuits that you posted are designed to protect what ever you are hooking up from you accidentally hooking the power supply up to that circuit with the polarity reversed. (Just like installing the batteries backwards). The circuits that you posted will work for that purpose but I got the impression that what you were looking for was a method that would keep voltage from an outside source creating a back flow current into your power supply. While this is not a common worry the best way and so far the only way I can find to do this is to use a diode in series with your output.

     

    I built a bench supply a while back and blogged about it. I don't know if it will give you any new ideas but in case you want to check it out here is the link.

     

    https://www.element14.com/community/people/jw0752/blog/2017/02/11/oh-no-not-another-power-supply

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tim687
    0 tim687 over 9 years ago in reply to jw0752

    Hi John,

    It was both actually. But for now I'll just go with the reverse polarity protection.

    Is there any circuit that fits best?

     

    Thanks,

     

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 9 years ago in reply to tim687

    The reverse polarity circuits are not designed to protect your bench supply. They are intended to protect what ever equipment you are hooking up to the bench supply. If accidentally you hook the positive and negative of the bench supply up to the incorrect terminals of a piece of equipment without polarity protection you may damage it. With polarity protection the piece of equipment would be OK. The polarity protection is part of the circuit or equipment you are experimenting with and not part of the bench supply.

     

    Here are the three simplest I could find.

     

    https://provideyourown.com/2012/reverse-polarity-protection-circuits/

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 9 years ago in reply to tim687

    The reverse polarity circuits are not designed to protect your bench supply. They are intended to protect what ever equipment you are hooking up to the bench supply. If accidentally you hook the positive and negative of the bench supply up to the incorrect terminals of a piece of equipment without polarity protection you may damage it. With polarity protection the piece of equipment would be OK. The polarity protection is part of the circuit or equipment you are experimenting with and not part of the bench supply.

     

    Here are the three simplest I could find.

     

    https://provideyourown.com/2012/reverse-polarity-protection-circuits/

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer