Test & Tools
  • Technologies
  • More
Test & Tools
Forum Reverse polarity protection circuit & output backward flow control
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 7 answers
  • Subscribers 387 subscribers
  • Views 6134 views
  • Users 0 members are here
  • reverse polarity protection
Related

Reverse polarity protection circuit & output backward flow control

tim687
tim687 over 9 years ago

I am building my own (2 channel) lab bench. This is the conversion board I'm using to convert 12V (input) to 1-24V (one for each channel).

 

In the product description they say

Input reverse connect protection: No (If necessary, please input series schottky diode)
Output control flow backward: No (If used for battery charging or load is bring electricity load, please on the output side series schottky diode)

This does mean that there is no reverse polarity input protection (that is not needed anyways), but does this mean that there is reverse polarity output protection?

In the datasheet of the LTC3780 I found the following pin descriptions in the pinout:

 

SENSE+ (Pin 3/Pin 1):

The + Input to the Current Sense

and Reverse Current Detect Comparators. The ITH

pin voltage and built-in offsets between SENSE– and SENSE+ pins,

in conjunction with RSENSE, set the current trip threshold.

SENSE– (Pin 4/Pin 2):

The (–) Input to the Current Sense

and Reverse Current Detect Comparators.

 

Is this the reverse polarity protection feature and output backward flow control I'm looking for?

 

If yes, I don't have to design the circuitry to protect the output, if no, could you provide a solution which can accept variable voltages?

This is one solution I found very interesting due to the indicator LED and the 'no power loss' (claim).

Due to inefficiency of a schottky diode I am only going to use it if necessary.

 

Thanks in advance for helping me out!

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 9 years ago +1 suggested
    This board will make a truly dreadful bench supply - unless you only want it to work light bulbs or heaters then please think again. I recently helped a customer trouble shoot a new design where they had…
  • rachaelp
    rachaelp over 9 years ago in reply to michaelkellett +1 suggested
    Michael Kellett wrote: For a general purpose bench supply you can't beat a decent linear design - just learn to live with the size, weight and heat MK You can also do a hybrid design to try and get the…
  • michaelkellett
    michaelkellett over 9 years ago in reply to tim687 +1 suggested
    Hello Tim, The noise is un-fixable by any reasonable means - it consists of bursts of very large amplitude 50-130 MHz decaying sine bursts as the power devices switch. We put at least 160 hours of engineering…
Parents
  • michaelkellett
    0 michaelkellett over 9 years ago

    This board will make a truly dreadful bench supply - unless you only want it to work light bulbs or heaters then please think again.

     

    I recently helped  a customer trouble shoot a new design where they had used the LTC3780 - the network connections would not work dues to power supply noise.

     

    I made two different versions of test boards, bought  a board  a bit like yours from Amazon and also tested the Linear Technology demo board - all of the boards were still very very noisy - quite unusable for a general purpose bench supply.

     

    The conversion efficiency that can be achieved with this chip is great - but the noise is a huge issue.

     

    We moved over to using buck only switchers on the original board (since we didn't have to have the LTC3780's boost capability) and this worked much better.

     

    For  a general purpose bench supply you can't beat a decent linear design - just learn to live with the size, weight and heat image

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

    For a general purpose bench supply you can't beat a decent linear design - just learn to live with the size, weight and heat

     

    MK

    You can also do a hybrid design to try and get the best of both worlds (with a little compromise). If you use a switcher to get the voltage to a few volts above your desired output and then use a linear regulator to step down to your desired output voltage, you get a reduction in switching noise because the power supply rejection ratio (PSRR) of the linear regulator is high without too much heat in the linear regulator as the switcher reduces the voltage drop across it.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • tim687
    0 tim687 over 9 years ago in reply to rachaelp

    The voltage is variable so I'm not sure how I'd make such a circuit with regulators. I only have a few 5V linear regulators available currently.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to tim687

    You basically cascade the regulators so you have Vin -> Switching Regulator -> Linear Regulator -> Vout and then you take your feedback from Vout and generate appropriate control voltages to the two regulators to ensure the switcher output remains a few volts above the final output voltage.

     

    I think it's unlikely that you'll get a clean enough output for your supply by just trying to filter the output with adding capacitors. You could try to create an LC filter on your output to suppress the noise but really, if you are trying the create a nice clean supply the best way is to have a linear power supply design.

     

    The board you are planning to use supports up to 10A or 7A for long term use but what current do you really need?

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • tim687
    0 tim687 over 9 years ago in reply to rachaelp

    Not sure what current I need. I'm not building it for a specific purpose, just to test electronics without blowing anything up. (as I often did with a computer power supply in the past)

     

     

    You basically cascade the regulators so you have Vin -> Switching Regulator -> Linear Regulator -> Vout and then you take your feedback from Vout and generate appropriate control voltages to the two regulators to ensure the switcher output remains a few volts above the final output voltage.

    Does this apply to a pre-made pcb as well? I am imagining that a 12V rails of a server grade power supply is not that noisy.

     

    Thanks,

     

    Tim

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tim687
    0 tim687 over 9 years ago in reply to rachaelp

    Not sure what current I need. I'm not building it for a specific purpose, just to test electronics without blowing anything up. (as I often did with a computer power supply in the past)

     

     

    You basically cascade the regulators so you have Vin -> Switching Regulator -> Linear Regulator -> Vout and then you take your feedback from Vout and generate appropriate control voltages to the two regulators to ensure the switcher output remains a few volts above the final output voltage.

    Does this apply to a pre-made pcb as well? I am imagining that a 12V rails of a server grade power supply is not that noisy.

     

    Thanks,

     

    Tim