Test & Tools
  • Technologies
  • More
Test & Tools
Forum Cheap XR2206 Function Generator Overheating...
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 23 replies
  • Answers 7 answers
  • Subscribers 387 subscribers
  • Views 5580 views
  • Users 0 members are here
Related

Cheap XR2206 Function Generator Overheating...

kas.lewis
kas.lewis over 9 years ago

Hello All,

 

I've been working to learn more about analog circuitry, for this purpose I decided I would try a XR2206 bases function generator cheap yes, but hopefully a place to start. When I first received the unit I tested it (can't give a positive rating on eBay unless it works) and I was able to see the three waveforms. They had soem jitter and other issues but overall it worked.

 

Today I decided to get start really working with it and noticed that the XR2206 IC started to get very warm. As I was not 100% I had connected it the right way, I tried connecting it in reverse (probably not the smartest idea thinking back). The IC was still getting pretty warm and this was not even with the voltage at the recommended level (using 5V instead of 9V, I always start from zero and turn up the supply). I then disconnected the GND from the oscilloscope and the IC started to cool off, connecting it again and it heats up. I have now tried this with two scopes (TBS 120B-EDU and DS)X1120G) and the same thing happens with both of them. I do know that the plug all my equipment is connected to is not grounded (old wiring, looking to rectify this just not sure how at the moment).

 

If anyone has some ideas as to why connecting the scope would cause the IC to heat up I would be very interested in then and exploring this issue further.

 

Thanks

Kas

 

P.s I'm not sure that this is the right group to post this in but, I'm not sure where else this should go.

  • Sign in to reply
  • Cancel

Top Replies

  • ewinter2112
    ewinter2112 over 9 years ago +4 suggested
    I purchased one of these as a project for my grandson because it was inexpensive. And you get what you pay for but still well worth the money. I cant speak to you specific issue but ................. To…
  • michaelkellett
    michaelkellett over 9 years ago in reply to kas.lewis +2 suggested
    If it's drawing 220mA then the chip will get hot (3W at 14V makes for a very hot chip) . Almost certainly the chip is blown. It's a very long time since I used one of these and I can't remember how easy…
  • the-dubster
    the-dubster over 9 years ago +1
    Out of interest, what current is the circuit drawing with the load (O'Scope) connected and not connected? I may be wide of the mark here but the XR2206P has a minimum supply of 10V (Max 26V) - and a typical…
Parents
  • the-dubster
    0 the-dubster over 9 years ago

    Out of interest, what current is the circuit drawing with the load (O'Scope) connected and not connected?

     

    I may be wide of the mark here but the XR2206P has a minimum supply of 10V (Max 26V) - and a typical current draw of 12mA (Max 20mA)  -  XR22106CPD is 14-20mA.

     

    Possibly driving it with a reduced voltage may cause it to draw more current to meet it's power requirements?

     

    Also, output impedance could possibly be an issue, RH Electronics list a kit with an output impedance of 600 ohms - again, could too low an impedance cause excessive current draw?

    (Incidentally, the RH kit has a supply of 12V and between 12-20mA supply current requirements . . . . . . ).

     

     

     

     

    Or I may be talking total cack! image

     

     

     

    Specs and test cct taken from Sparkfun Website

     

     

    (I have no affiliation to the websites listed - they just popped up using a 'popular' search engine!!) image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 9 years ago in reply to the-dubster

    the-dubster,

     

    From what I can see it's consuming 0.22A with a supply of 14V. After disconnecting the scope it's still drawing the same current. Maybe it was an illusion that it was only over heating when connected to the scope. (Its also fun doubting yourself after the fact image).

     

    Kas

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to kas.lewis

    If it's drawing 220mA then the chip will get hot (3W at 14V makes for a very hot chip) .

     

    Almost certainly the chip is blown.

     

    It's a very long time since I used one of these and I can't remember how easy they were to blow up.

     

    I realise that you want to learn about analogue circuits - do you want to make a signal generator or was playing with it a end in itself. If you want  a signal generator I can make some other suggestions that are not based on obsolete parts and might be more forgiving.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • the-dubster
    0 the-dubster over 9 years ago in reply to michaelkellett

    See my last post below - I misread as 22mA and not 220mA - away too high, supply range is 10 (or 14) to 26V - Current is 14-22mA.  That gives a max power dissipation of 520mW - absolute max rating I think was about 750mW. As michaelkellett stated, you're dragging in excess of 3W through this.

     

    That isn't good whichever way you paint it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kas.lewis
    0 kas.lewis over 9 years ago in reply to michaelkellett

    michaelkellett,

     

    I am looking to learn more about analog circuits, so the signal generator was an inexpensive way to get something to play with. I'm not really in a position to spend a lot on a generator at the moment.

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kas.lewis
    0 kas.lewis over 9 years ago in reply to michaelkellett

    michaelkellett,

     

    I am looking to learn more about analog circuits, so the signal generator was an inexpensive way to get something to play with. I'm not really in a position to spend a lot on a generator at the moment.

     

    Kas