Test & Tools
  • Technologies
  • More
Test & Tools
Forum I2C switch / output expander with Open Drain
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 29 replies
  • Answers 7 answers
  • Subscribers 386 subscribers
  • Views 6158 views
  • Users 0 members are here
Related

I2C switch / output expander with Open Drain

Jan Cumps
Jan Cumps over 9 years ago

I'm looking for an I2C expander or switch that can put output to open drain.

 

Should be

- 5V tolerant

- at least one output that can be driven low and high-Z

- if possible SOIC package

- no isolation needed

- a few mA is enough.

- does not need to be bidirectional. Output only would be ok.

 

Is there a good candidate?

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 9 years ago +5 verified
    I've used TI port expanders from the PCA95xx range in the past and they seem quite good. How about this one? http://www.ti.com/lit/ds/symlink/pca9557.pdf P0 is open drain, P1 through P7 are push-pull.…
  • jc2048
    jc2048 over 9 years ago +3
    Philips fan? Here's my all-time favourite databook cover (that's from 1991)
  • rachaelp
    rachaelp over 9 years ago in reply to Jan Cumps +2 suggested
    Or the NXP equivalent from here? PCA9557D NXP, I/O Expander, 8bit, 400 kHz, I2C, SMBus, 2.3 V, 5.5 V, SOIC | Farnell element14
Parents
  • jc2048
    0 jc2048 over 9 years ago

    Erm, what's this for exactly? If you're pulling down the gate of the output MOSFET, it needs to tolerate more than 5V. The nice power MOSFETs that Peter found and wants to use are not logic-level devices and the gate will be working up at 6 or 7V.

     

    A small MOSFET controlled by one of the regular outputs of your expander would be better.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to jc2048

    image

     

    to provide the ~enable signal. Pull the node to 0V to switch off the load.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to Jan Cumps

    jc2048, do you think that an open collector PCA9557DPCA9557Dwon't do in this case

    It only has to keep the signal at approx 0V when engaged, should be masked from what happens at left side of diode when high-Z (would it suffer from 7V minus a diode drop in High-Z config ? maybe yes ...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to Jan Cumps

    jc2048, do you think that an open collector PCA9557DPCA9557Dwon't do in this case

    It only has to keep the signal at approx 0V when engaged, should be masked from what happens at left side of diode when high-Z (would it suffer from 7V minus a diode drop in High-Z config ? maybe yes ...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jc2048
    0 jc2048 over 9 years ago in reply to Jan Cumps

    If there's ESD protection just above the 5V level, then that will catch the diode and limit the diode OR node to maybe 6.5V or something like that (not high enough for the operation we want, though it would do if you built a version with a logic-level power MOSFET on the output). If there's no ESD protection, then you lift the output until it starts to breakdown - not a disaster because of the 10k limiting the current so much, but it still catches the voltage, only we don't know where (that's hackery, not Real Design(tm)).