Test & Tools
  • Technologies
  • More
Test & Tools
Forum I2C switch / output expander with Open Drain
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 29 replies
  • Answers 7 answers
  • Subscribers 386 subscribers
  • Views 6065 views
  • Users 0 members are here
Related

I2C switch / output expander with Open Drain

Jan Cumps
Jan Cumps over 9 years ago

I'm looking for an I2C expander or switch that can put output to open drain.

 

Should be

- 5V tolerant

- at least one output that can be driven low and high-Z

- if possible SOIC package

- no isolation needed

- a few mA is enough.

- does not need to be bidirectional. Output only would be ok.

 

Is there a good candidate?

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 9 years ago +5 verified
    I've used TI port expanders from the PCA95xx range in the past and they seem quite good. How about this one? http://www.ti.com/lit/ds/symlink/pca9557.pdf P0 is open drain, P1 through P7 are push-pull.…
  • jc2048
    jc2048 over 9 years ago +3
    Philips fan? Here's my all-time favourite databook cover (that's from 1991)
  • rachaelp
    rachaelp over 9 years ago in reply to Jan Cumps +2 suggested
    Or the NXP equivalent from here? PCA9557D NXP, I/O Expander, 8bit, 400 kHz, I2C, SMBus, 2.3 V, 5.5 V, SOIC | Farnell element14
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to jc2048

    .... another thought. In this set-up, would it make sense to not use the open collector P0 of the extender (there's only one - we may have a better use for it later) and use one of the push-pulls?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to Jan Cumps

    btw, just simply leaving it disconnected will allow the system to work, it won't drive the output on if either of the other two connections are still low

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to jc2048

    It was not transients in my little mishap, it was a gross overloading of the FET that then cause the shunt resistor to fail (A rather expensive one I might add image ) and consiquently feeding the source voltage right into the OPAMP inputs, grossly exceeding their input protection limits.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago in reply to Jan Cumps

    image, its great to win a contest and upgrade your lab, then sell the old stuff to add even more coolness to the bench image

     

    You definitely deserved to win that one btw...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to Robert Peter Oakes

    I sold my previous soldering station last week - a decent one but a few steps down from the one I won (it was also several steps down in $$).

    The great thing is that both me as the seller and the person who bought it were delighted with the deal. And it gets me some budget to throw towards the DC load.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jc2048
    0 jc2048 over 8 years ago in reply to Jan Cumps

    Yes, use one of the push-pull outputs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jc2048
    0 jc2048 over 8 years ago in reply to Robert Peter Oakes

    OK, understood. But the question was do you need Jan to add anything for protection purposes that can't be dealt with just by the processor shutting the MOSFET down? If not, Jan can have a go at a first draft of the board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 8 years ago in reply to jc2048

    Jon Clift wrote:

    ...

     

    Love that PSU. Why aren't you using it?

    Also: this was the first supply that I had that was able to run in constant current mode. The other ones I had either blew a fuse or (the self-modded one based on an Oppermann kit in 1982 or 3? and my first commercial supply) switch off at over current.

    I like the maximum current future more than the ones that just switch off. Even worse, I have a commercial one that goes to -0.7 V when current exceeds the set point. That's Not Funny.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago in reply to jc2048

    I dont think anything more than we already have, all the op-amps have suitably high resistors to protect them and a diode off board should be across the sense resistor, maybe two could be there (Back to back), the FET already has one and as already suggested, a fuse should also help. we just dont want too much in the power path in order to still handle high currents with low voltage

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<